Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
Related Pages
Here is a list of all related documentation pages:
[detail level 12]
oLicenseCopyright (c) 2017-2018 Microchip Technology Inc
oExtra Information for TC Driver
oExamples for TC DriverThis is a list of the available Quick Start guides (QSGs) and example applications for SAM Timer/Counter (TC) Driver
oDocument Revision History
oQuick start guide for USB host Communication Device Class module (UHI CDC)This is the quick start guide for the USB host Communication Device Class module (UHI CDC) with step-by-step instructions on how to configure and use the modules in a selection of use cases
oQuick Start Guide for the SAM AT30TSE75X Temperature Sensor DriverIn this use case we will interface the temperature sensor, set a resolution and read the temperature
oLicenseCopyright (c) 2014-2018 Microchip Technology Inc
oExtra Information for ADC Driver
oExamples for ADC DriverThis is a list of the available Quick Start guides (QSGs) and example applications for SAM Analog-to-Digital Converter (ADC) Driver
oDocument Revision History
oExtra Information for PORT Driver
oExamples for PORT DriverThis is a list of the available Quick Start guides (QSGs) and example applications for SAM Port (PORT) Driver
oDocument Revision History
oOverviewThis unit test carries out tests for the External Interrupt driver
oSAM EXTINT Unit TestOverview:
oExtra Information for RTC (CAL) Driver
oExamples for RTC CAL DriverThis is a list of the available Quick Start guides (QSGs) and example applications for SAM RTC Calendar (RTC CAL) Driver
oDocument Revision History
oQuick start guide for USB Device Vendor module (UDI Vendor)This is the quick start guide for the USB device interface Vendor module (UDI Vendor) with step-by-step instructions on how to configure and use the modules in a selection of use cases
oQuick start guide for USB device mouse module (UDI mouse)This is the quick start guide for the USB device mouse module (UDI mouse) with step-by-step instructions on how to configure and use the modules in a selection of use cases
oQuick Start Guide for SERCOM I2C Master - CallbackIn this use case, the I2C will used and set up as follows:
oQuick Start Guide for SERCOM I2C Master - BasicIn this use case, the I2C will used and set up as follows:
oQuick Start Guide for Using DMA with SERCOM I2C MasterThe supported board list:
oExtra Information for SERCOM I2C Driver
oExamples for SERCOM I2C DriverThis is a list of the available Quick Start guides (QSGs) and example applications for Asfdoc_sam0_sercom_i2c_group
oDocument Revision History
oExtra Information for TCC Driver
oExamples for TCC DriverThis is a list of the available Quick Start guides (QSGs) and example applications for SAM Timer Counter for Control Applications (TCC) Driver
oDocument Revision History
oQuick Start Guide for SERCOM I2C Slave - BasicIn this use case, the I2C will used and set up as follows:
oQuick Start Guide for Using DMA with SERCOM I2C SlaveThe supported board list:
oExtra Information for SERCOM USART Driver
oExamples for SERCOM USART DriverThis is a list of the available Quick Start guides (QSGs) and example applications for SAM Serial USART (SERCOM USART) Driver
oSERCOM USART MUX SettingsThe following lists the possible internal SERCOM module pad function assignments, for the four SERCOM pads when in USART mode
oDocument Revision History
oExtra Information for SYSTEM INTERRUPT Driver
oExamples for SYSTEM INTERRUPT DriverThis is a list of the available Quick Start guides (QSGs) and example applications for SAM System Interrupt (SYSTEM INTERRUPT) Driver
oDocument Revision History
oQuick start guide for USB device Mass Storage module (UDI MSC)This is the quick start guide for the USB device interface MSC module (UDI MSC) with step-by-step instructions on how to configure and use the modules in a selection of use cases
oQuick start guide for Serial Interface serviceThis is the quick start guide for the Serial Interface module, with step-by-step instructions on how to configure and use the serial in a selection of use cases
oExtra Information for EXTINT Driver
oExamples for EXTINT DriverThis is a list of the available Quick Start guides (QSGs) and example applications for SAM External Interrupt (EXTINT) Driver
oDocument Revision History
oExtra Information for RTC COUNT Driver
oExamples for RTC (COUNT) DriverThis is a list of the available Quick Start guides (QSGs) and example applications for SAM RTC Count (RTC COUNT) Driver
oDocument Revision History
oExtra Information
oExamples for Emulated EEPROM ServiceThis is a list of the available Quick Start guides (QSGs) and example applications for SAM EEPROM Emulator (EEPROM) Service
oDocument Revision History
oExtra Information for SYSTEM Driver
oDocument Revision History
oQuick Start Guide for EVENTS - Interrupt HooksIn this use case, the EVENT module is configured for:
oExtra Information for SERCOM SPI Driver
oExamples for SERCOM SPI DriverThis is a list of the available Quick Start guides (QSGs) and example applications for SAM Serial Peripheral Interface (SERCOM SPI) Driver
oMUX SettingsThe following lists the possible internal SERCOM module pad function assignments for the four SERCOM pads in both SPI Master and SPI Slave modes
oDocument Revision History
oExamples for GFX Mono LibraryThis is a list of the available Quick Start guides (QSGs) and example applications for Monochrome graphical display system
oQuick start guide for USB device multi-touch module (UDI Multi-touch)
oQuick start guide for USB host mass-storage module (UHI MSC)This is the quick start guide for the USB host mass-storage module (UHI MSC) with step-by-step instructions on how to configure and use the modules in a selection of use cases
oQuick start guide for USB device Communication Class Device module (UDI CDC)This is the quick start guide for the USB device interface CDC module (UDI CDC) with step-by-step instructions on how to configure and use the modules in a selection of use cases
oExtra Information for PAC Driver
oExamples for PAC DriverThis is a list of the available Quick Start guides (QSGs) and example applications for SAM Peripheral Access Controller (PAC) Driver
oList of Non-Write Protected RegistersLook in device datasheet peripheral's subsection "Register Access Protection" to see which is actually available for your device
oDocument Revision History
oasfdoc_sam0_iso7816_qsDriver for smart card via ISO7816
oExtra Information for WDT Driver
oExamples for WDT DriverThis is a list of the available Quick Start guides (QSGs) and example applications for SAM Watchdog (WDT) Driver
oDocument Revision History
oQuick start guide for USB host mouse module (UHI mouse)This is the quick start guide for the USB host mouse module (UHI mouse) with step-by-step instructions on how to configure and use the modules in a selection of use cases
oExtra Information for SERCOM SPI Master Driver w/ Vectored I/O
oExamples for SERCOM SPI Master Driver w/ Vectored I/OThis is a list of the available Quick Start guides (QSGs) and example applications for SAM Serial Peripheral Interface Master Driver w/ Vectored I/O (SERCOM SPI)
oDocument Revision History
oQuick start guide for USB device keyboard module (UDI keyboard)This is the quick start guide for the USB device keyboard module (UDI keyboard) with step-by-step instructions on how to configure and use the modules in a selection of use cases
oExtra Information for CRC32
oExamples for CRC32This is a list of the available Quick Start Guides (QSGs) and example applications for SAM 32-bit cyclic redundancy check (CRC32) Driver
oDocument Revision History
oExtra Information for AC Driver
oExamples for AC DriverThis is a list of the available Quick Start guides (QSGs) and example applications for SAM Analog Comparator (AC) Driver
oDocument Revision History
oxTaskHandleTask
otaskYIELDTask
otaskENTER_CRITICALTask
otaskEXIT_CRITICALTask
otaskDISABLE_INTERRUPTSTask
otaskENABLE_INTERRUPTSTask
oxTaskGetTickCountTask
ouxTaskGetNumberOfTasksTask
opcTaskGetTaskNameTask
ovTaskListTask
ovTaskGetRunTimeStatsTask
ovSemaphoreDeleteSemphr
ouxQueueMessagesWaitingQueue
ovQueueDeleteQueue
oconf_clock.h examples with USB supportContent of XMEGA conf_clock.h:
oExtra Information for SYSTEM PINMUX Driver
oExamples for SYSTEM PINMUX DriverThis is a list of the available Quick Start guides (QSGs) and example applications for SAM System Pin Multiplexer (SYSTEM PINMUX) Driver
oDocument Revision History
oQuick start guide for USB host vendor module (UHI vendor)This is the quick start guide for the USB host vendor module (UHI vendor) with step-by-step instructions on how to configure and use the modules in a selection of use cases
oExtra Information for SYSTEM CLOCK Driver
oExamples for System Clock DriverThis is a list of the available Quick Start guides (QSGs) and example applications for SAM System Clock Management (SYSTEM CLOCK) Driver
oDocument Revision History
oExtra Information for DMAC Driver
oExamples for DMAC DriverThis is a list of the available Quick Start Guides (QSGs) and example applications for SAM Direct Memory Access Controller (DMAC) Driver
oDocument Revision History
oQuick Start Guide for CRC-32To use this service, the user must supply a container variable for the CRC and call crc32_calculate() with the parameters for the first block in the dataset
oExtra Information for CCL Driver
oExamples for CCL DriverThis is a list of the available Quick Start guides (QSGs) and example applications for SAM Configurable Custom Logic (CCL) Driver
oDocument Revision History
oExtra Information for NVM Driver
oExamples for NVM DriverThis is a list of the available Quick Start guides (QSGs) and example applications for SAM Non-Volatile Memory (NVM) Driver
oDocument Revision History
oExtra Information
oExamples for Emulated RWW EEPROM ServiceThis is a list of the available Quick Start guides (QSGs) and example applications for SAM Read While Write EEPROM (RWW EEPROM) Emulator Service
oDocument Revision History
oSAM Tic-Tac-Toe ExampleOverview:
oconf_clock.h examples with USB supportContent of conf_clock.h for AT32UC3A0, AT32UC3A1, AT32UC3B devices (USBB):
oQuick Start Guide for SERCOM I2C Slave - CallbackIn this use case, the I2C will used and set up as follows:
oQuick start guide for USB device generic module (UDI generic)This is the quick start guide for the USB device generic module (UDI generic) with step-by-step instructions on how to configure and use the modules in a selection of use cases
oExtra Information for BOD Driver
oExamples for BOD DriverThis is a list of the available Quick Start guides (QSGs) and example applications for SAM Brown Out Detector (BOD) Driver
oDocument Revision History
oExtra Information for AT25DFx SerialFlash Driver
oExamples for AT25DFx SerialFlash DriverThis is a list of the available Quick Start guides (QSGs) and example applications for AT25DFx SerialFlash Driver
oDocument Revision History
\Todo List