FreeRTOS configuration.
Copyright (c) 2012-2018 Microchip Technology Inc. and its subsidiaries.
Functions | |
int | main (void) |
Main function. Execution starts here. More... | |
static void | main_memories_trans_task (void *pvParameters) |
void | main_msc_disable (void) |
Called by MSC interface Callback running when USB Host disable MSC interface. More... | |
bool | main_msc_enable (void) |
Called by MSC interface Callback running when USB Host enable MSC interface. More... | |
void | main_msc_notify_trans (void) |
Called when a data transfer on MSC must be executed Thus, the udi_msc_process_trans() function must be called. More... | |
void | main_resume_action (void) |
Turn on a led to notify active mode Called when the USB line is resumed from the suspend state. More... | |
void | main_sof_action (void) |
Manages the leds behaviors Called when a start of frame is received on USB line each 1ms. More... | |
void | main_suspend_action (void) |
Enters the application in low power mode Callback called when USB host sets USB line in suspend state. More... | |
void | vApplicationIdleHook (void) |
Variables | |
static volatile bool | main_b_msc_enable = false |
static xSemaphoreHandle | main_trans_semphr = NULL |
Handle to the semaphore protecting memories transfer. More... | |
int main | ( | void | ) |
Main function. Execution starts here.
References Assert, board_init(), cpu_irq_enable, irq_initialize_vectors, main_memories_trans_task(), memories_initialization(), NULL, sleepmgr_init(), sysclk_init(), tskIDLE_PRIORITY, udc_start(), ui_init(), ui_powerdown(), vSemaphoreCreateBinary, vTaskStartScheduler(), and xTaskCreate.
|
static |
References pdTRUE, udi_msc_process_trans(), UNUSED, and xSemaphoreTake.
Referenced by main().
void main_msc_disable | ( | void | ) |
Called by MSC interface Callback running when USB Host disable MSC interface.
bool main_msc_enable | ( | void | ) |
Called by MSC interface Callback running when USB Host enable MSC interface.
true | if MSC startup is ok |
void main_msc_notify_trans | ( | void | ) |
Called when a data transfer on MSC must be executed Thus, the udi_msc_process_trans() function must be called.
References pdFALSE, and xSemaphoreGiveFromISR.
void main_resume_action | ( | void | ) |
Turn on a led to notify active mode Called when the USB line is resumed from the suspend state.
Called by UDD when the USB line exit of suspend state.
References ui_wakeup().
void main_sof_action | ( | void | ) |
Manages the leds behaviors Called when a start of frame is received on USB line each 1ms.
Called when a start of frame is received on USB line.
References main_b_msc_enable, udd_get_frame_number(), and ui_process().
void main_suspend_action | ( | void | ) |
Enters the application in low power mode Callback called when USB host sets USB line in suspend state.
Called by UDD when a suspend is received Callback running when USB Host set USB line in suspend state.
References ui_powerdown().
void vApplicationIdleHook | ( | void | ) |
Referenced by main_msc_disable(), main_msc_enable(), and main_sof_action().
|
static |
Handle to the semaphore protecting memories transfer.