#include "ble/le_device_db.h"
#include "ble/core.h"
#include <stdio.h>
#include <string.h>
#include "btstack_debug.h"
Data Structures | |
struct | le_device_memory_db |
Macros | |
#define | __BTSTACK_FILE__ "le_device_db_memory.c" |
#define | INVALID_ENTRY_ADDR_TYPE 0xff |
Typedefs | |
typedef struct le_device_memory_db | le_device_memory_db_t |
Functions | |
int | le_device_db_add (int addr_type, bd_addr_t addr, sm_key_t irk) |
add device to db More... | |
int | le_device_db_count (void) |
get number of devices in db for enumeration More... | |
void | le_device_db_dump (void) |
void | le_device_db_encryption_get (int index, uint16_t *ediv, uint8_t rand[8], sm_key_t ltk, int *key_size, int *authenticated, int *authorized) |
get remote encryption info More... | |
void | le_device_db_encryption_set (int index, uint16_t ediv, uint8_t rand[8], sm_key_t ltk, int key_size, int authenticated, int authorized) |
set remote encryption info More... | |
void | le_device_db_info (int index, int *addr_type, bd_addr_t addr, sm_key_t irk) |
get device information: addr type and address needed to identify device More... | |
void | le_device_db_init (void) |
Note: LE Device DB for pure LE Peripherals is not required if only LE Legacy Pairing without signed writes is used. More... | |
void | le_device_db_remove (int index) |
free device More... | |
void | le_device_db_set_local_bd_addr (bd_addr_t bd_addr) |
sets local bd addr. More... | |
Variables | |
static le_device_memory_db_t | le_devices [MAX_NR_LE_DEVICE_DB_ENTRIES] |
#define __BTSTACK_FILE__ "le_device_db_memory.c" |
#define INVALID_ENTRY_ADDR_TYPE 0xff |
Referenced by le_device_db_add(), le_device_db_count(), le_device_db_dump(), and le_device_db_remove().
typedef struct le_device_memory_db le_device_memory_db_t |
add device to db
addr_type,address | of the device |
irk | of the device |
References le_device_memory_db::addr_type, bd_addr_to_str(), INVALID_ENTRY_ADDR_TYPE, log_info, and log_info_key().
Referenced by sm_key_distribution_handle_all_received().
int le_device_db_count | ( | void | ) |
get number of devices in db for enumeration
References counter, and INVALID_ENTRY_ADDR_TYPE.
Referenced by le_device_db_dump(), sm_key_distribution_handle_all_received(), and sm_run().
void le_device_db_dump | ( | void | ) |
References bd_addr_to_str(), INVALID_ENTRY_ADDR_TYPE, le_device_db_count(), log_info, and log_info_key().
void le_device_db_encryption_get | ( | int | index, |
uint16_t * | ediv, | ||
uint8_t | rand[8], | ||
sm_key_t | ltk, | ||
int * | key_size, | ||
int * | authenticated, | ||
int * | authorized | ||
) |
get remote encryption info
index ediv rand ltk key size authenticated authorized
References le_device_memory_db::authenticated, le_device_memory_db::authorized, le_device_memory_db::ediv, le_device_memory_db::key_size, log_info, le_device_memory_db::ltk, and le_device_memory_db::rand.
Referenced by sm_address_resolution_handle_event(), sm_pdu_handler(), and sm_request_pairing().
void le_device_db_encryption_set | ( | int | index, |
uint16_t | ediv, | ||
uint8_t | rand[8], | ||
sm_key_t | ltk, | ||
int | key_size, | ||
int | authenticated, | ||
int | authorized | ||
) |
set remote encryption info
index ediv rand ltk key size authenticated authorized
References le_device_memory_db::authenticated, le_device_memory_db::authorized, le_device_memory_db::ediv, le_device_memory_db::key_size, log_info, le_device_memory_db::ltk, and le_device_memory_db::rand.
Referenced by sm_key_distribution_handle_all_received().
get device information: addr type and address needed to identify device
index | |
addr_type,address | of the device as output |
irk | of the device |
References le_device_memory_db::addr_type.
Referenced by sm_key_distribution_handle_all_received(), sm_notify_client_index(), and sm_run().
void le_device_db_init | ( | void | ) |
Note: LE Device DB for pure LE Peripherals is not required if only LE Legacy Pairing without signed writes is used.
Per bonded device:
References le_device_db_remove().
Referenced by le_counter_setup(), le_prov_app_setup(), and tss_app_setup().
void le_device_db_remove | ( | int | index | ) |
free device
index |
References le_device_memory_db::addr_type, and INVALID_ENTRY_ADDR_TYPE.
Referenced by le_device_db_init(), and sm_event_packet_handler().
void le_device_db_set_local_bd_addr | ( | bd_addr_t | bd_addr | ) |
sets local bd addr.
allows for db per Bluetooth controller
bd_addr |
Referenced by sm_event_packet_handler().
|
static |