Microchip® Advanced Software Framework

os_hook.h File Reference

Copyright (c) 2016-2018 Microchip Technology Inc.

and its subsidiaries.

#include "compiler.h"

Data Structures

struct  hif_msg_t
 
struct  params_dispatch
 

Macros

#define MSG_CMD   5
 
#define MSG_QUIT   4
 
#define MSG_RX   1
 
#define MSG_START   6
 
#define MSG_TX_AP   3
 
#define MSG_TX_STA   2
 

Typedefs

typedef void(* wifi_task_cb )(void *arg)
 

Functions

void os_hook_deinit (void)
 
uint8_t os_hook_dispatch_no_wait (wifi_task_cb handler, void *p)
 Run handler function in the netif thread context and return immediately. More...
 
void os_hook_dispatch_wait (wifi_task_cb handler, struct params_dispatch *p, void *pv)
 Run handler function in the netif thread context and wait for function return. More...
 
void os_hook_init (void)
 Initialize netif thread. More...
 
void os_hook_isr (void)
 Put interrupt request in netif queue for later processing. More...
 
void os_hook_notify (void)
 Release lock to notify calling thread that netif job is done. More...
 
void os_hook_send_start (wifi_task_cb handler, struct params_dispatch *p, void *pv)
 Start WiFi in the netif thread context and wait for function return. More...
 
void os_hook_send_stop (wifi_task_cb handler, struct params_dispatch *p, void *pv)
 
void os_hook_set_handle (void *task)
 

#define MSG_CMD   5
#define MSG_QUIT   4
#define MSG_RX   1

Referenced by os_hif_task(), and os_hook_isr().

#define MSG_START   6

Referenced by os_hif_task(), and os_hook_send_start().

#define MSG_TX_AP   3

Referenced by os_hif_task(), and wilc_netif_tx().

#define MSG_TX_STA   2

typedef void(* wifi_task_cb)(void *arg)

void os_hook_deinit ( void  )
uint8_t os_hook_dispatch_no_wait ( wifi_task_cb  handler,
void *  p 
)

Run handler function in the netif thread context and return immediately.

References hif_msg_t::handler, hif_thread, hif_msg_t::id, msg, MSG_CMD, hif_msg_t::priv, xQueueSend, and xTaskGetCurrentTaskHandle().

void os_hook_dispatch_wait ( wifi_task_cb  handler,
struct params_dispatch p,
void *  pv 
)

Run handler function in the netif thread context and wait for function return.

References hif_msg_t::handler, hif_thread, hif_msg_t::id, msg, MSG_CMD, hif_msg_t::priv, params_dispatch::signal_semaphore, xQueueSend, xSemaphoreTake, and xTaskGetCurrentTaskHandle().

void os_hook_init ( void  )
void os_hook_isr ( void  )

Put interrupt request in netif queue for later processing.

References hif_msg_t::id, msg, MSG_RX, NULL, osprintf(), hif_msg_t::payload, hif_msg_t::payload_size, hif_msg_t::pbuf, pdFALSE, pdTRUE, and xQueueSendFromISR.

void os_hook_notify ( void  )

Release lock to notify calling thread that netif job is done.

References xSemaphoreGive.

Referenced by os_m2m_wifi_connect_imp(), os_m2m_wifi_enable_ap_imp(), os_m2m_wifi_init_imp(), and os_m2m_wifi_set_max_tx_rate_imp().

void os_hook_send_start ( wifi_task_cb  handler,
struct params_dispatch p,
void *  pv 
)

Start WiFi in the netif thread context and wait for function return.

References hif_msg_t::handler, hif_msg_t::id, msg, MSG_START, hif_msg_t::priv, params_dispatch::signal_semaphore, xQueueSend, and xSemaphoreTake.

Referenced by os_m2m_wifi_init().

void os_hook_send_stop ( wifi_task_cb  handler,
struct params_dispatch p,
void *  pv 
)
void os_hook_set_handle ( void *  task)

References hif_thread.

Referenced by os_m2m_wifi_init_imp().