semphr.
h
vSemaphoreCreateBinary( xSemaphoreHandle xSemaphore )
Macro that implements a semaphore by using the existing queue mechanism. The queue length is 1 as this is a binary semaphore. The data size is 0 as we don't want to actually store any data - we just want to know if the queue is empty or full.
This type of semaphore can be used for pure synchronisation between tasks or between an interrupt and a task. The semaphore need not be given back once obtained, so one task/interrupt can continuously 'give' the semaphore while another continuously 'takes' the semaphore. For this reason this type of semaphore does not use a priority inheritance mechanism. For an alternative that does use priority inheritance see xSemaphoreCreateMutex().
xSemaphore | Handle to the created semaphore. Should be of type xSemaphoreHandle. |
Example usage:
xSemaphoreHandle xSemaphore;
void vATask( void * pvParameters ) { Semaphore cannot be used before a call to vSemaphoreCreateBinary (). This is a macro so pass the variable in directly. vSemaphoreCreateBinary( xSemaphore );
if( xSemaphore != NULL ) { The semaphore was created successfully. The semaphore can now be used. } }