Includes IEEE Constant Definitions.
Macros | |
#define | aBaseSlotDuration (60) |
The number of symbols forming a superframe slot when the superframe order is equal to 0. More... | |
#define | aBaseSuperframeDuration |
The number of symbols forming a superframe when the superframe order is equal to 0. More... | |
#define | ACK_PAYLOAD_LEN (0x03) |
Length (in octets) of ACK payload. More... | |
#define | aGTSDescPersistenceTime (4) |
The number of superframes in which a GTS descriptor exists in the beacon frame of a PAN coordinator. More... | |
#define | aMaxBeaconOverhead (75) |
The maximum number of octets added by the MAC sublayer to the payload of its beacon frame. More... | |
#define | aMaxBeaconPayloadLength (aMaxPHYPacketSize - aMaxBeaconOverhead) |
The maximum size, in octets, of a beacon payload. More... | |
#define | aMaxLostBeacons (4) |
The number of consecutive lost beacons that will cause the MAC sublayer of a receiving device to declare a loss of synchronization. More... | |
#define | aMaxMACPayloadSize (aMaxPHYPacketSize - aMinMPDUOverhead) |
The maximum number of octets that can be transmitted in the MAC Payload field. More... | |
#define | aMaxMACSafePayloadSize |
The maximum number of octets that can be transmitted in the MAC Payload field of an unsecured MAC frame that will be guaranteed not to exceed aMaxPHYPacketSize. More... | |
#define | aMaxMPDUUnsecuredOverhead (25) |
The maximum number of octets added by the MAC sublayer to the PSDU without security. More... | |
#define | aMaxPHYPacketSize (127) |
Maximum size of PHY packet. More... | |
#define | aMaxSIFSFrameSize (18) |
The maximum size of an MPDU, in octets, that can be followed by a SIFS period. More... | |
#define | aMinCAPLength (440) |
The minimum number of symbols forming the CAP. More... | |
#define | aMinMPDUOverhead (9) |
The minimum number of octets added by the MAC sublayer to the PSDU. More... | |
#define | aNumSuperframeSlots (16) |
The number of slots contained in any superframe. More... | |
#define | ASSOC_PERMIT_BIT_POS (15) |
Association permit bit position. More... | |
#define | ASSOCIATION_RESERVED (3) |
Association status code value (see wpan_mlme_associate_resp()). More... | |
#define | ASSOCIATION_SUCCESSFUL (0) |
Association status code value (see wpan_mlme_associate_resp()). More... | |
#define | aTurnaroundTime (12) |
Maximum turnaround Time of the radio to switch from Rx to Tx or Tx to Rx in symbols. More... | |
#define | aUnitBackoffPeriod (20) |
The number of symbols forming the basic time period used by the CSMA-CA algorithm. More... | |
#define | BATT_LIFE_EXT_BIT_POS (12) |
Battery life extention bit position. More... | |
#define | BROADCAST (0xFFFF) |
Generic 16 bit broadcast address. More... | |
#define | CLEAR_ADDR_64 (0ULL) |
Unused EUI-64 address. More... | |
#define | CONV_DBM_TO_phyTransmitPower(dbm_value) |
Converts a dBm value to a phyTransmitPower value. More... | |
#define | CONV_phyTransmitPower_TO_DBM(phyTransmitPower_value) |
Converts a phyTransmitPower value to a dBm value. More... | |
#define | ED_VAL_LEN (1) |
Length of the ED value parameter number field. More... | |
#define | EXT_ADDR_LEN (8) |
Length (in octets) of extended address. More... | |
#define | FCF1_FV_2003 (0) |
The mask for a IEEE 802.15.4-2003 compatible frame in the frame version subfield fcf1. More... | |
#define | FCF1_FV_2006 (1) |
The mask for a IEEE 802.15.4-2006 compatible frame in the frame version subfield fcf1. More... | |
#define | FCF1_FV_2012 (2) |
The mask for a IEEE 802.15.4e-2012 compatible frame in the frame version subfield fcf1. More... | |
#define | FCF1_FV_MASK (3 << FCF1_FV_SHIFT) |
The mask for the frame version subfield fcf1. More... | |
#define | FCF1_FV_SHIFT (4) |
Shift value for the frame version subfield fcf1. More... | |
#define | FCF_2_DEST_ADDR_OFFSET (2) |
Offset of Destination Addressing Mode of octet two of MHR. More... | |
#define | FCF_2_SOURCE_ADDR_OFFSET (6) |
Offset of Source Addressing Mode of octet two of MHR. More... | |
#define | FCF_ACK_REQUEST (1 << 5) |
The mask for the ACK request bit of the FCF. More... | |
#define | FCF_DEST_ADDR_OFFSET (10) |
Defines the offset of the destination address. More... | |
#define | FCF_FRAME_PENDING (1 << 4) |
The mask for the frame pending bit of the FCF. More... | |
#define | FCF_FRAME_VERSION_2003 (0 << 12) |
The mask for a IEEE 802.15.4-2003 compatible frame in the frame version subfield. More... | |
#define | FCF_FRAME_VERSION_2006 (1 << 12) |
The mask for a IEEE 802.15.4-2006 compatible frame in the frame version subfield. More... | |
#define | FCF_FRAME_VERSION_2012 (2 << 12) |
The mask for a IEEE 802.15.4e-2012 compatible frame in the frame version subfield. More... | |
#define | FCF_FRAMETYPE_ACK (0x02) |
Define the ACK frame type. More... | |
#define | FCF_FRAMETYPE_BEACON (0x00) |
Defines the beacon frame type. More... | |
#define | FCF_FRAMETYPE_DATA (0x01) |
Define the data frame type. More... | |
#define | FCF_FRAMETYPE_LLDN (0x04) |
Define the LLDN frame type. More... | |
#define | FCF_FRAMETYPE_MAC_CMD (0x03) |
Define the command frame type. More... | |
#define | FCF_FRAMETYPE_MASK (0x07) |
Defines a mask for the frame type. More... | |
#define | FCF_FRAMETYPE_MP (0x05) |
Define the multipurpose frame type. More... | |
#define | FCF_GET_FRAMETYPE(x) ((x) & FCF_FRAMETYPE_MASK) |
Macro to get the frame type. More... | |
#define | FCF_LEN (2) |
Length (in octets) of FCF. More... | |
#define | FCF_LONG_ADDR (0x03) |
Address Mode: LONG. More... | |
#define | FCF_NO_ADDR (0x00) |
Address Mode: NO ADDRESS. More... | |
#define | FCF_PAN_ID_COMPRESSION (1 << 6) |
The mask for the PAN ID compression bit of the FCF. More... | |
#define | FCF_RESERVED_ADDR (0x01) |
Address Mode: RESERVED. More... | |
#define | FCF_SECURITY_ENABLED (1 << 3) |
The mask for the security enable bit of the FCF. More... | |
#define | FCF_SET_DEST_ADDR_MODE(x) |
Macro to set the destination address mode. More... | |
#define | FCF_SET_FRAMETYPE(x) (x) |
A macro to set the frame type. More... | |
#define | FCF_SET_SOURCE_ADDR_MODE(x) |
Macro to set the source address mode. More... | |
#define | FCF_SHORT_ADDR (0x02) |
Address Mode: SHORT. More... | |
#define | FCF_SOURCE_ADDR_OFFSET (14) |
Defines the offset of the source address. More... | |
#define | FCS_LEN (2) |
Length (in octets) of FCS. More... | |
#define | GTS_ALLOCATE (1) |
#define | GTS_DEALLOCATE (0) |
#define | GTS_RX_SLOT (1) |
#define | GTS_SLOT_LENGTH_1 (0x01) |
#define | GTS_SLOT_LENGTH_10 (0x0A) |
#define | GTS_SLOT_LENGTH_11 (0x0B) |
#define | GTS_SLOT_LENGTH_12 (0x0C) |
#define | GTS_SLOT_LENGTH_13 (0x0D) |
#define | GTS_SLOT_LENGTH_14 (0x0E) |
#define | GTS_SLOT_LENGTH_15 (0x0F) |
#define | GTS_SLOT_LENGTH_2 (0x02) |
#define | GTS_SLOT_LENGTH_3 (0x03) |
#define | GTS_SLOT_LENGTH_4 (0x04) |
#define | GTS_SLOT_LENGTH_5 (0x05) |
#define | GTS_SLOT_LENGTH_6 (0x06) |
#define | GTS_SLOT_LENGTH_7 (0x07) |
#define | GTS_SLOT_LENGTH_8 (0x08) |
#define | GTS_SLOT_LENGTH_9 (0x09) |
#define | GTS_TX_SLOT (0) |
#define | INVALID_SHORT_ADDRESS (0xFFFF) |
Invalid short address. More... | |
#define | INVERSE_CHANNEL_MASK (~VALID_CHANNEL_MASK) |
Inverse channel masks for scanning. More... | |
#define | LENGTH_FIELD_LEN (1) |
Size of the length parameter. More... | |
#define | LQI_LEN (1) |
Length of the LQI number field. More... | |
#define | MAC_NO_SHORT_ADDR_VALUE (0xFFFE) |
MAC is using long address (by now). More... | |
#define | macAckWaitDuration (0x40) |
The maximum number of symbols to wait for an acknowledgment frame to arrive following a transmitted data frame. More... | |
#define | macAssociatedPANCoord (0x56) |
Indication of whether the device is associated to the PAN through the PAN coordinator. More... | |
#define | macAssociatedPANCoord_def (false) |
Default value for PIB macAssociatedPANCoord. More... | |
#define | macAssociationPermit (0x41) |
Indication of whether a coordinator is currently allowing association. More... | |
#define | macAssociationPermit_def (false) |
Default value for PIB macAssociationPermit. More... | |
#define | macAutoRequest (0x42) |
Indication of whether a device automatically sends a data request command if its address is listed in the beacon frame. More... | |
#define | macAutoRequest_def (true) |
Default value for PIB macAutoRequest. More... | |
#define | macBattLifeExt (0x43) |
Indication of whether battery life extension, by reduction of coordinator receiver operation time during the CAP, is enabled. More... | |
#define | macBattLifeExt_def (false) |
Default value for PIB macBattLifeExt. More... | |
#define | macBattLifeExtPeriods (0x44) |
The number of backoff periods during which the receiver is enabled following a beacon in battery life extension mode. More... | |
#define | macBattLifeExtPeriods_def (6) |
Default value for PIB macBattLifeExtPeriods. More... | |
#define | macBeaconOrder (0x47) |
Specification of how often the coordinator transmits a beacon. More... | |
#define | macBeaconOrder_def (15) |
Default value for PIB macBeaconOrder. More... | |
#define | macBeaconPayload (0x45) |
The contents of the beacon payload. More... | |
#define | macBeaconPayloadLength (0x46) |
The length, in octets, of the beacon payload. More... | |
#define | macBeaconPayloadLength_def (0) |
Default value for PIB macBeaconPayloadLength. More... | |
#define | macBeaconTxTime (0x48) |
The time that the device transmitted its last beacon frame, in symbol periods. More... | |
#define | macBeaconTxTime_def (0x000000) |
Default value for PIB macBeaconTxTime. More... | |
#define | macBSN (0x49) |
The sequence number added to the transmitted beacon frame. More... | |
#define | macCoordExtendedAddress (0x4A) |
The 64 bit address of the coordinator with which the device is associated. More... | |
#define | macCoordShortAddress (0x4B) |
The 16 bit short address assigned to the coordinator with which the device is associated. More... | |
#define | macCoordShortAddress_def (0xFFFF) |
Default value for PIB macCoordShortAddress. More... | |
#define | macDSN (0x4C) |
The sequence number added to the transmitted data or MAC command frame. More... | |
#define | macGTSPermit (0x4D) |
macGTSPermit is true if the PAN coordinator is to accept GTS requests, false otherwise. More... | |
#define | macGTSPermit_def (true) |
Default value for PIB macGTSPermit. More... | |
#define | macIeeeAddress (0xF0) |
Private MAC PIB attribute to allow setting the MAC address in test mode. More... | |
#define | macMaxBE (0x57) |
The maximum value of the backoff exponent, BE, in the CSMA-CA algorithm. More... | |
#define | macMaxCSMABackoffs (0x4E) |
The maximum number of backoffs the CSMA-CA algorithm will attempt before declaring a channel access failure. More... | |
#define | macMaxCSMABackoffs_def (4) |
Default value for PIB macMaxCSMABackoffs. More... | |
#define | macMaxFrameRetries (0x59) |
The maximum number of retries allowed after a transmission failure. More... | |
#define | macMaxFrameTotalWaitTime (0x58) |
The maximum number of CAP symbols in a beaconenabled PAN, or symbols in a nonbeacon-enabled PAN, to wait either for a frame intended as a response to a data request frame or for a broadcast frame following a beacon with the Frame Pending subfield set to one. More... | |
#define | macMaxNumRxFramesDuringBackoff (0x7F) |
Private MAC PIB attribute to control the CSMA algorithm. More... | |
#define | macMinBE (0x4F) |
The minimum value of the backoff exponent in the CSMA-CA algorithm. More... | |
#define | macMinLIFSPeriod (0x5E) |
The minimum number of symbols forming a LIFS period. More... | |
#define | macMinLIFSPeriod_def (40) |
Default value for PIB macMinLIFSPeriod. More... | |
#define | macMinSIFSPeriod (0x5F) |
The minimum number of symbols forming a SIFS period. More... | |
#define | macMinSIFSPeriod_def (12) |
Default value for PIB macMinSIFSPeriod. More... | |
#define | macPANCoordExtendedAddress (0x7D) |
The 64-bit address of the PAN coordinator. More... | |
#define | macPANCoordShortAddress (0x7E) |
The 16-bit short address assinged to the PAN coordinator. More... | |
#define | macPANId (0x50) |
The 16 bit identifier of the PAN on which the device is operating. More... | |
#define | macPANId_def (0xFFFF) |
Default value for PIB macPANId. More... | |
#define | macPromiscuousMode (0x51) |
This indicates whether the MAC sublayer is in a promiscuous (receive all) mode. More... | |
#define | macResponseWaitTime (0x5A) |
The maximum time, in multiples of aBaseSuperframeDuration, a device shall wait for a response command frame to be available following a request command frame. More... | |
#define | macResponseWaitTime_def (32 * aBaseSuperframeDuration) |
Default value for PIB macResponseWaitTime. More... | |
#define | macRxOnWhenIdle (0x52) |
This indicates whether the MAC sublayer is to enable its receiver during idle periods. More... | |
#define | macRxOnWhenIdle_def (false) |
Default value for PIB macRxOnWhenIdle. More... | |
#define | macSecurityEnabled (0x5D) |
Indication of whether the MAC sublayer has security enabled. More... | |
#define | macSecurityEnabled_def (false) |
Default value for PIB macSecurityEnabled. More... | |
#define | macShortAddress (0x53) |
The 16 bit address that the device uses to communicate in the PAN. More... | |
#define | macShortAddress_def (0xFFFF) |
Default value for PIB macShortAddress. More... | |
#define | macSuperframeOrder (0x54) |
This specifies the length of the active portion of the superframe, including the beacon frame. More... | |
#define | macSuperframeOrder_def (15) |
Default value for PIB macSuperframeOrder. More... | |
#define | macSyncSymbolOffset (0x5B) |
The offset, measured in symbols, between the symbol boundary at which the MLME captures the timestamp of each transmitted or received frame, and the onset of the first symbol past the SFD, namely, the first symbol of the Length field. More... | |
#define | macTimestampSupported (0x5C) |
Indication of whether the MAC sublayer supports the optional timestamping feature for incoming and outgoing data frames. More... | |
#define | macTransactionPersistenceTime (0x55) |
The maximum time (in superframe periods) that a transaction is stored by a coordinator and indicated in its beacon. More... | |
#define | macTransactionPersistenceTime_def (0x01F4) |
Default value for PIB macTransactionPersistenceTime. More... | |
#define | MAX_KEY_ID_FIELD_LEN (9) |
Maximum length of the key id field. More... | |
#define | MAX_MGMT_FRAME_LENGTH (30) |
Maximum size of the management frame(Association Response frame) More... | |
#define | MIN_FRAME_LENGTH (8) |
Minimum size of a valid frame other than an Ack frame. More... | |
#define | MLME_SCAN_TYPE_ACTIVE (0x01) |
Active scan (see wpan_mlme_scan_req()) More... | |
#define | MLME_SCAN_TYPE_ED (0x00) |
Energy scan (see wpan_mlme_scan_req()) More... | |
#define | MLME_SCAN_TYPE_ORPHAN (0x03) |
Orphan scan (see wpan_mlme_scan_req()) More... | |
#define | MLME_SCAN_TYPE_PASSIVE (0x02) |
Passive scan (see wpan_mlme_scan_req()) More... | |
#define | NO_PIB_INDEX (0) |
#define | NON_BEACON_NWK (0x0F) |
BO value for nonbeacon-enabled network. More... | |
#define | NUM_LONG_PEND_ADDR(x) (((x) & 0x70) >> 4) |
Mask for the number of long addresses pending. More... | |
#define | NUM_SHORT_PEND_ADDR(x) ((x) & 0x07) |
Mask for the number of short addresses pending. More... | |
#define | PAN_ACCESS_DENIED (2) |
Association status code value (see wpan_mlme_associate_resp()). More... | |
#define | PAN_AT_CAPACITY (1) |
Association status code value (see wpan_mlme_associate_resp()). More... | |
#define | PAN_COORD_BIT_POS (14) |
PAN coordinator bit position. More... | |
#define | PAN_ID_LEN (2) |
Length (in octets) of PAN ID. More... | |
#define | PL_POS_DST_ADDR_START (6) |
Octet start position of Destination Address field within payload array of frame_info_t. More... | |
#define | PL_POS_DST_PAN_ID_START (4) |
Octet start position of Destination PAN-Id field within payload array of frame_info_t. More... | |
#define | PL_POS_FCF_1 (1) |
Octet position of FCF octet one within payload array of frame_info_t. More... | |
#define | PL_POS_FCF_2 (2) |
Octet position of FCF octet two within payload array of frame_info_t. More... | |
#define | PL_POS_SEQ_NUM (3) |
Octet position of Sequence Number octet within payload array of frame_info_t. More... | |
#define | SEQ_NUM_LEN (1) |
Length of the sequence number field. More... | |
#define | SHORT_ADDR_LEN (2) |
Length (in octets) of short address. More... | |
#define | WPAN_TXOPT_ACK (0x01) |
Value for TxOptions parameter in wpan_mcps_data_req(). More... | |
#define | WPAN_TXOPT_GTS (0x02) |
Value for TxOptions parameter in wpan_mcps_data_req(). More... | |
#define | WPAN_TXOPT_GTS_ACK (0x03) |
Value for TxOptions parameter in wpan_mcps_data_req(). More... | |
#define | WPAN_TXOPT_INDIRECT (0x04) |
Value for TxOptions parameter in wpan_mcps_data_req(). More... | |
#define | WPAN_TXOPT_INDIRECT_ACK (0x05) |
Value for TxOptions parameter in wpan_mcps_data_req(). More... | |
#define | WPAN_TXOPT_OFF (0x00) |
Value for TxOptions parameter in wpan_mcps_data_req(). More... | |
Typedefs | |
typedef enum cca_mode_tag | cca_mode_t |
CCA mode enumeration. More... | |
typedef enum ch_pg_tag | ch_pg_t |
typedef enum trx_cca_mode_tag | trx_cca_mode_t |
CCA Modes of the transceiver. More... | |
Enumerations | |
enum | cca_mode_tag { CCA_MODE_0_CS_OR_ED = 0, CCA_MODE_1_ED = 1, CCA_MODE_2_CS, CCA_MODE_3_CS_ED, CCA_MODE_4_ALOHA } |
CCA mode enumeration. More... | |
enum | ch_pg_tag { CH_PG_2003 = 0, CH_PG_2006 = 2, CH_PG_CHINA = 5, CH_PG_JAPAN = 6, CH_PG_MSK = 7, CH_PG_LRP_UWB = 8, CH_PG_SUN = 9, CH_PG_GENERIC_PHY = 10, CH_PG_16 = 16, CH_PG_18 = 18, CH_PG_INVALID = 0xFF } |
enum | trx_cca_mode_tag { TRX_CCA_MODE0 = 0, TRX_CCA_MODE1 = 1, TRX_CCA_MODE2 = 2, TRX_CCA_MODE3 = 3 } |
#define | phyCurrentChannel (0x00) |
The RF channel to use for all following transmissions and receptions. More... | |
#define | phyChannelsSupported (0x01) |
The 5 most significant bits (MSBs) (b27, ..., b31) of phyChannelsSupported shall be reserved and set to 0, and the 27 LSBs (b0, b1, ..., b26) shall indicate the status (1 = available, 0 = unavailable) for each of the 27 valid channels (bk shall indicate the status of channel k). More... | |
#define | phyTransmitPower (0x02) |
The 2 MSBs represent the tolerance on the transmit power: 00 = 1 dB 01 = 3 dB 10 = 6 dB The 6 LSBs represent a signed integer in twos-complement format, corresponding to the nominal transmit power of the device in decibels relative to 1 mW. More... | |
#define | phyCCAMode (0x03) |
The CCA mode. More... | |
#define | phyCurrentPage (0x04) |
This is the current PHY channel page. More... | |
#define | phyMaxFrameDuration (0x05) |
The maximum number of symbols in a frame: = phySHRDuration + ceiling([aMaxPHYPacketSize + 1] x phySymbolsPerOctet) More... | |
#define | phySHRDuration (0x06) |
The duration of the synchronization header (SHR) in symbols for the current PHY. More... | |
#define | phySymbolsPerOctet (0x07) |
The number of symbols per octet for the current PHY. More... | |
#define | PHY_OVERHEAD (5) |
Number of octets added by the PHY: 4 sync octets + SFD octet. More... | |
enum | phy_enum_tag { PHY_BUSY = (0x00), PHY_BUSY_RX = (0x01), PHY_BUSY_TX = (0x02), PHY_FORCE_TRX_OFF = (0x03), PHY_IDLE = (0x04), PHY_INVALID_PARAMETER = (0x05), PHY_RX_ON = (0x06), PHY_SUCCESS = (0x07), PHY_TRX_OFF = (0x08), PHY_TX_ON = (0x09), PHY_UNSUPPORTED_ATTRIBUTE = (0x0A), PHY_READ_ONLY = (0x0B) } |
typedef enum phy_enum_tag | phy_enum_t |
#define | PHY_SUCCESS_DATA_PENDING (0x10) |
PHY_SUCCESS in phyAutoCSMACA when received ACK frame had the pending bit set. More... | |
#define | ED_SAMPLE_DURATION_SYM (8) |
ED scan/sampling duration. More... | |
#define aBaseSlotDuration (60) |
The number of symbols forming a superframe slot when the superframe order is equal to 0.
#define aBaseSuperframeDuration |
The number of symbols forming a superframe when the superframe order is equal to 0.
#define ACK_PAYLOAD_LEN (0x03) |
Length (in octets) of ACK payload.
Referenced by tx_done_handling().
#define aGTSDescPersistenceTime (4) |
The number of superframes in which a GTS descriptor exists in the beacon frame of a PAN coordinator.
Referenced by mlme_gts_request().
#define aMaxBeaconOverhead (75) |
The maximum number of octets added by the MAC sublayer to the payload of its beacon frame.
#define aMaxBeaconPayloadLength (aMaxPHYPacketSize - aMaxBeaconOverhead) |
The maximum size, in octets, of a beacon payload.
Referenced by mlme_set().
#define aMaxLostBeacons (4) |
The number of consecutive lost beacons that will cause the MAC sublayer of a receiving device to declare a loss of synchronization.
Referenced by check_beacon_reception(), mac_start_missed_beacon_timer(), and start_beacon_loss_timer().
#define aMaxMACPayloadSize (aMaxPHYPacketSize - aMinMPDUOverhead) |
The maximum number of octets that can be transmitted in the MAC Payload field.
Referenced by parse_mpdu(), and wpan_mcps_data_req().
#define aMaxMACSafePayloadSize |
The maximum number of octets that can be transmitted in the MAC Payload field of an unsecured MAC frame that will be guaranteed not to exceed aMaxPHYPacketSize.
Referenced by build_data_frame().
#define aMaxMPDUUnsecuredOverhead (25) |
The maximum number of octets added by the MAC sublayer to the PSDU without security.
#define aMaxPHYPacketSize (127) |
Maximum size of PHY packet.
Referenced by build_data_frame(), and stb_ccm_secure().
#define aMaxSIFSFrameSize (18) |
The maximum size of an MPDU, in octets, that can be followed by a SIFS period.
Referenced by calc_frame_transmit_duration(), calculate_transaction_duration(), mac_process_beacon_frame(), and send_frame().
#define aMinCAPLength (440) |
The minimum number of symbols forming the CAP.
This ensures that MAC commands can still be transferred to devices when GTSs are being used. An exception to this minimum shall be allowed for the accommodation of the temporary increase in the beacon frame length needed to perform GTS maintenance (see 7.2.2.1.3).
#define aMinMPDUOverhead (9) |
The minimum number of octets added by the MAC sublayer to the PSDU.
#define aNumSuperframeSlots (16) |
The number of slots contained in any superframe.
#define ASSOC_PERMIT_BIT_POS (15) |
Association permit bit position.
Referenced by usr_mlme_scan_conf().
#define ASSOCIATION_RESERVED (3) |
Association status code value (see wpan_mlme_associate_resp()).
#define ASSOCIATION_SUCCESSFUL (0) |
Association status code value (see wpan_mlme_associate_resp()).
Referenced by mac_process_associate_response().
#define aTurnaroundTime (12) |
Maximum turnaround Time of the radio to switch from Rx to Tx or Tx to Rx in symbols.
Referenced by calc_frame_transmit_duration(), calculate_transaction_duration(), and tx_done_handling().
#define aUnitBackoffPeriod (20) |
The number of symbols forming the basic time period used by the CSMA-CA algorithm.
Referenced by calc_frame_transmit_duration(), calculate_transaction_duration(), csma_backoff_calculation(), mac_process_beacon_frame(), perform_cca_twice(), recalc_macMaxFrameTotalWaitTime(), and tal_tx_frame().
#define BATT_LIFE_EXT_BIT_POS (12) |
Battery life extention bit position.
#define BROADCAST (0xFFFF) |
Generic 16 bit broadcast address.
Referenced by mac_awake_scan(), mac_build_and_tx_data_req(), mac_prep_disassoc_conf(), mac_process_coord_realign(), mac_process_orphan_realign(), mac_process_tal_tx_status(), mac_t_assocresponsetime_cb(), mcps_data_request(), mlme_associate_request(), mlme_start_request(), send_scan_cmd(), and usr_mcps_data_ind().
#define CLEAR_ADDR_64 (0ULL) |
Unused EUI-64 address.
#define CONV_DBM_TO_phyTransmitPower | ( | dbm_value | ) |
Converts a dBm value to a phyTransmitPower value.
dbm_value | dBm value |
Referenced by limit_tx_pwr(), and tal_set_tx_pwr().
#define CONV_phyTransmitPower_TO_DBM | ( | phyTransmitPower_value | ) |
Converts a phyTransmitPower value to a dBm value.
phyTransmitPower_value | phyTransmitPower value |
Referenced by convert_phyTransmitPower_to_reg_value(), and limit_tx_pwr().
#define ED_SAMPLE_DURATION_SYM (8) |
ED scan/sampling duration.
#define ED_VAL_LEN (1) |
Length of the ED value parameter number field.
Referenced by handle_received_frame_irq().
#define EXT_ADDR_LEN (8) |
Length (in octets) of extended address.
Referenced by mac_extract_mhr_addr_info().
#define FCF1_FV_2003 (0) |
The mask for a IEEE 802.15.4-2003 compatible frame in the frame version subfield fcf1.
#define FCF1_FV_2006 (1) |
The mask for a IEEE 802.15.4-2006 compatible frame in the frame version subfield fcf1.
#define FCF1_FV_2012 (2) |
The mask for a IEEE 802.15.4e-2012 compatible frame in the frame version subfield fcf1.
#define FCF1_FV_MASK (3 << FCF1_FV_SHIFT) |
The mask for the frame version subfield fcf1.
#define FCF1_FV_SHIFT (4) |
Shift value for the frame version subfield fcf1.
#define FCF_2_DEST_ADDR_OFFSET (2) |
Offset of Destination Addressing Mode of octet two of MHR.
Referenced by mac_prep_disassoc_conf().
#define FCF_2_SOURCE_ADDR_OFFSET (6) |
Offset of Source Addressing Mode of octet two of MHR.
#define FCF_ACK_REQUEST (1 << 5) |
The mask for the ACK request bit of the FCF.
Referenced by build_data_frame(), calc_frame_transmit_duration(), calculate_transaction_duration(), mac_build_and_tx_data_req(), mlme_associate_request(), mlme_disassociate_request(), mlme_gts_request(), tx_done_handling(), and tx_pan_id_conf_notif().
#define FCF_DEST_ADDR_OFFSET (10) |
Defines the offset of the destination address.
Referenced by mac_extract_mhr_addr_info().
#define FCF_FRAME_PENDING (1 << 4) |
The mask for the frame pending bit of the FCF.
Referenced by mac_process_beacon_frame(), and mac_process_data_frame().
#define FCF_FRAME_VERSION_2003 (0 << 12) |
The mask for a IEEE 802.15.4-2003 compatible frame in the frame version subfield.
#define FCF_FRAME_VERSION_2006 (1 << 12) |
The mask for a IEEE 802.15.4-2006 compatible frame in the frame version subfield.
Referenced by build_data_frame(), mac_process_coord_realign(), mac_process_orphan_realign(), and parse_mpdu().
#define FCF_FRAME_VERSION_2012 (2 << 12) |
The mask for a IEEE 802.15.4e-2012 compatible frame in the frame version subfield.
#define FCF_FRAMETYPE_ACK (0x02) |
Define the ACK frame type.
(Table 65 IEEE 802.15.4 Specification)
#define FCF_FRAMETYPE_BEACON (0x00) |
Defines the beacon frame type.
(Table 65 IEEE 802.15.4 Specification)
Referenced by mac_process_data_response(), parse_mpdu(), process_data_ind_not_transient(), process_data_ind_scanning(), and process_incoming_frame().
#define FCF_FRAMETYPE_DATA (0x01) |
Define the data frame type.
(Table 65 IEEE 802.15.4 Specification)
Referenced by build_data_frame(), mac_process_data_response(), mac_process_tal_data_ind(), parse_mpdu(), and process_data_ind_not_transient().
#define FCF_FRAMETYPE_LLDN (0x04) |
Define the LLDN frame type.
See 802.15.4e-2012
#define FCF_FRAMETYPE_MAC_CMD (0x03) |
Define the command frame type.
(Table 65 IEEE 802.15.4 Specification)
Referenced by mac_build_and_tx_data_req(), mac_process_tal_data_ind(), mlme_associate_request(), mlme_disassociate_request(), mlme_gts_request(), parse_mpdu(), process_data_ind_not_transient(), process_data_ind_scanning(), send_scan_cmd(), and tx_pan_id_conf_notif().
#define FCF_FRAMETYPE_MASK (0x07) |
Defines a mask for the frame type.
(Table 65 IEEE 802.15.4 Specification)
Referenced by process_incoming_frame().
#define FCF_FRAMETYPE_MP (0x05) |
Define the multipurpose frame type.
See 802.15.4e-2012
#define FCF_GET_FRAMETYPE | ( | x | ) | ((x) & FCF_FRAMETYPE_MASK) |
Macro to get the frame type.
Referenced by parse_mpdu().
#define FCF_LEN (2) |
Length (in octets) of FCF.
Referenced by mac_extract_mhr_addr_info().
#define FCF_LONG_ADDR (0x03) |
Address Mode: LONG.
Referenced by build_data_frame(), mac_build_and_tx_data_req(), mac_extract_mhr_addr_info(), mac_prep_disassoc_conf(), mac_process_data_frame(), mlme_associate_request(), mlme_disassociate_request(), mlme_poll_request(), process_data_ind_not_transient(), send_scan_cmd(), and tx_pan_id_conf_notif().
#define FCF_NO_ADDR (0x00) |
Address Mode: NO ADDRESS.
Referenced by build_data_frame(), mac_build_and_tx_data_req(), mcps_data_request(), and send_scan_cmd().
#define FCF_PAN_ID_COMPRESSION (1 << 6) |
The mask for the PAN ID compression bit of the FCF.
Referenced by build_data_frame(), mac_build_and_tx_data_req(), mac_extract_mhr_addr_info(), mlme_disassociate_request(), mlme_gts_request(), send_scan_cmd(), and tx_pan_id_conf_notif().
#define FCF_RESERVED_ADDR (0x01) |
Address Mode: RESERVED.
Referenced by mcps_data_request().
#define FCF_SECURITY_ENABLED (1 << 3) |
The mask for the security enable bit of the FCF.
Referenced by build_data_frame(), mac_tx_gts_data(), mcps_data_request(), and parse_mpdu().
#define FCF_SET_DEST_ADDR_MODE | ( | x | ) |
Macro to set the destination address mode.
Referenced by build_data_frame(), mac_build_and_tx_data_req(), mlme_associate_request(), mlme_disassociate_request(), mlme_gts_request(), send_scan_cmd(), and tx_pan_id_conf_notif().
#define FCF_SET_FRAMETYPE | ( | x | ) | (x) |
A macro to set the frame type.
Referenced by build_data_frame(), mac_build_and_tx_data_req(), mlme_associate_request(), mlme_disassociate_request(), mlme_gts_request(), send_scan_cmd(), and tx_pan_id_conf_notif().
#define FCF_SET_SOURCE_ADDR_MODE | ( | x | ) |
Macro to set the source address mode.
Referenced by build_data_frame(), mac_build_and_tx_data_req(), mlme_associate_request(), mlme_disassociate_request(), mlme_gts_request(), send_scan_cmd(), and tx_pan_id_conf_notif().
#define FCF_SHORT_ADDR (0x02) |
Address Mode: SHORT.
Referenced by build_data_frame(), mac_build_and_tx_data_req(), mac_extract_mhr_addr_info(), mac_gen_mlme_disassociate_conf(), mac_prep_disassoc_conf(), mac_process_beacon_frame(), mac_process_data_frame(), mcps_data_request(), mlme_associate_request(), mlme_disassociate_request(), mlme_gts_request(), mlme_poll_request(), process_data_ind_not_transient(), and send_scan_cmd().
#define FCF_SOURCE_ADDR_OFFSET (14) |
Defines the offset of the source address.
Referenced by mac_extract_mhr_addr_info().
#define FCS_LEN (2) |
Length (in octets) of FCS.
Referenced by mac_extract_mhr_addr_info(), tx_done_handling(), and wpan_mcps_data_req().
#define GTS_ALLOCATE (1) |
Referenced by mac_parse_bcn_gts_info(), mac_process_beacon_frame(), mlme_gts_request(), and usr_mlme_associate_conf().
#define GTS_DEALLOCATE (0) |
Referenced by handle_gts_sync_loss(), mac_parse_bcn_gts_info(), and mlme_gts_request().
#define GTS_RX_SLOT (1) |
Referenced by handle_gts_data_req(), and usr_mlme_associate_conf().
#define GTS_SLOT_LENGTH_1 (0x01) |
#define GTS_SLOT_LENGTH_10 (0x0A) |
#define GTS_SLOT_LENGTH_11 (0x0B) |
#define GTS_SLOT_LENGTH_12 (0x0C) |
#define GTS_SLOT_LENGTH_13 (0x0D) |
#define GTS_SLOT_LENGTH_14 (0x0E) |
#define GTS_SLOT_LENGTH_15 (0x0F) |
#define GTS_SLOT_LENGTH_2 (0x02) |
#define GTS_SLOT_LENGTH_3 (0x03) |
#define GTS_SLOT_LENGTH_4 (0x04) |
#define GTS_SLOT_LENGTH_5 (0x05) |
#define GTS_SLOT_LENGTH_6 (0x06) |
#define GTS_SLOT_LENGTH_7 (0x07) |
#define GTS_SLOT_LENGTH_8 (0x08) |
#define GTS_SLOT_LENGTH_9 (0x09) |
#define GTS_TX_SLOT (0) |
Referenced by mac_process_data_frame().
#define INVALID_SHORT_ADDRESS (0xFFFF) |
Invalid short address.
Referenced by mac_process_associate_response(), mac_process_disassociate_notification(), mac_t_response_wait_cb(), and mlme_associate_request().
#define INVERSE_CHANNEL_MASK (~VALID_CHANNEL_MASK) |
Inverse channel masks for scanning.
Referenced by mlme_scan_request().
#define LENGTH_FIELD_LEN (1) |
Size of the length parameter.
Referenced by handle_received_frame_irq(), and tx_done_handling().
#define LQI_LEN (1) |
Length of the LQI number field.
Referenced by handle_received_frame_irq(), mac_process_tal_data_ind(), and process_incoming_frame().
#define MAC_NO_SHORT_ADDR_VALUE (0xFFFE) |
MAC is using long address (by now).
Referenced by mac_build_and_tx_data_req(), mac_prep_disassoc_conf(), mlme_associate_request(), and mlme_gts_request().
#define macAckWaitDuration (0x40) |
The maximum number of symbols to wait for an acknowledgment frame to arrive following a transmitted data frame.
This value is dependent on the currently selected logical channel. For 0 <= phyCurrentChannel <= 10, this value is equal to 120. For 11 <= phyCurrentChannel <= 26, this value is equal to 54.
Referenced by mlme_set(), and tal_pib_set().
#define macAssociatedPANCoord (0x56) |
Indication of whether the device is associated to the PAN through the PAN coordinator.
A value of TRUE indicates the device has associated through the PAN coordinator. Otherwise, the value is set to FALSE.
Referenced by mlme_get(), and mlme_set().
#define macAssociatedPANCoord_def (false) |
Default value for PIB macAssociatedPANCoord.
Referenced by do_init_pib().
#define macAssociationPermit (0x41) |
Indication of whether a coordinator is currently allowing association.
A value of true indicates that association is permitted.
Referenced by mlme_get(), and mlme_set().
#define macAssociationPermit_def (false) |
Default value for PIB macAssociationPermit.
Referenced by do_init_pib().
#define macAutoRequest (0x42) |
Indication of whether a device automatically sends a data request command if its address is listed in the beacon frame.
A value of true indicates that the data request command is automatically sent.
Referenced by mlme_get(), and mlme_set().
#define macAutoRequest_def (true) |
Default value for PIB macAutoRequest.
Referenced by do_init_pib().
#define macBattLifeExt (0x43) |
Indication of whether battery life extension, by reduction of coordinator receiver operation time during the CAP, is enabled.
A value of true indicates that it is enabled.
Referenced by mac_coord_realignment_command_tx_success(), mlme_get(), mlme_set(), mlme_start_request(), and tal_pib_set().
#define macBattLifeExt_def (false) |
Default value for PIB macBattLifeExt.
#define macBattLifeExtPeriods (0x44) |
The number of backoff periods during which the receiver is enabled following a beacon in battery life extension mode.
This value is dependent on the currently selected logical channel. For 0 <= * phyCurrentChannel <= 10, this value is equal to 8. For 11 <= * phyCurrentChannel <= 26, this value is equal to 6.
Referenced by mlme_get(), and mlme_set().
#define macBattLifeExtPeriods_def (6) |
Default value for PIB macBattLifeExtPeriods.
Referenced by do_init_pib().
#define macBeaconOrder (0x47) |
Specification of how often the coordinator transmits a beacon.
The macBeaconOrder, BO, and the beacon interval, BI, are related as follows: for 0 <= BO <= 14, BI = aBaseSuperframeDuration * 2^BO symbols. If BO = 15, the coordinator will not transmit a beacon.
Referenced by mac_coord_realignment_command_tx_success(), mac_process_beacon_frame(), mlme_get(), mlme_set(), mlme_start_request(), and tal_pib_set().
#define macBeaconOrder_def (15) |
Default value for PIB macBeaconOrder.
#define macBeaconPayload (0x45) |
The contents of the beacon payload.
Referenced by mac_get_pib_attribute_size(), mlme_get(), and mlme_set().
#define macBeaconPayloadLength (0x46) |
The length, in octets, of the beacon payload.
Referenced by mlme_get(), and mlme_set().
#define macBeaconPayloadLength_def (0) |
Default value for PIB macBeaconPayloadLength.
Referenced by do_init_pib().
#define macBeaconTxTime (0x48) |
The time that the device transmitted its last beacon frame, in symbol periods.
The measurement shall be taken at the same symbol boundary within every transmitted beacon frame, the location of which is implementation specific. The precision of this value shall be a minimum of 20 bits, with the lowest four bits being the least significant.
Referenced by mlme_get(), process_data_ind_not_transient(), tal_pib_set(), and wpan_mlme_set_req().
#define macBeaconTxTime_def (0x000000) |
Default value for PIB macBeaconTxTime.
#define macBSN (0x49) |
The sequence number added to the transmitted beacon frame.
Referenced by mlme_get(), and mlme_set().
#define macCoordExtendedAddress (0x4A) |
The 64 bit address of the coordinator with which the device is associated.
Referenced by mlme_get(), and mlme_set().
#define macCoordShortAddress (0x4B) |
The 16 bit short address assigned to the coordinator with which the device is associated.
A value of 0xfffe indicates that the coordinator is only using its 64 bit extended address. A value of 0xffff indicates that this value is unknown.
Referenced by mlme_disassociate_request(), mlme_get(), mlme_set(), and usr_mlme_set_conf().
#define macCoordShortAddress_def (0xFFFF) |
Default value for PIB macCoordShortAddress.
Referenced by do_init_pib(), mac_process_associate_response(), and mac_t_assocresponsetime_cb().
#define macDSN (0x4C) |
The sequence number added to the transmitted data or MAC command frame.
Referenced by mlme_get(), and mlme_set().
#define macGTSPermit (0x4D) |
macGTSPermit is true if the PAN coordinator is to accept GTS requests, false otherwise.
Referenced by mlme_set().
#define macGTSPermit_def (true) |
Default value for PIB macGTSPermit.
Referenced by do_init_pib().
#define macIeeeAddress (0xF0) |
Private MAC PIB attribute to allow setting the MAC address in test mode.
Referenced by mlme_get(), mlme_set(), and tal_pib_set().
#define macMaxBE (0x57) |
The maximum value of the backoff exponent, BE, in the CSMA-CA algorithm.
See 7.5.1.4 for a detailed explanation of the backoff exponent.
Referenced by mlme_get(), mlme_set(), and tal_pib_set().
#define macMaxCSMABackoffs (0x4E) |
The maximum number of backoffs the CSMA-CA algorithm will attempt before declaring a channel access failure.
Referenced by mlme_get(), mlme_set(), slotted_csma_state_handling(), and tal_pib_set().
#define macMaxCSMABackoffs_def (4) |
Default value for PIB macMaxCSMABackoffs.
#define macMaxFrameRetries (0x59) |
The maximum number of retries allowed after a transmission failure.
Referenced by mlme_get(), mlme_set(), and tal_pib_set().
#define macMaxFrameTotalWaitTime (0x58) |
The maximum number of CAP symbols in a beaconenabled PAN, or symbols in a nonbeacon-enabled PAN, to wait either for a frame intended as a response to a data request frame or for a broadcast frame following a beacon with the Frame Pending subfield set to one.
This attribute, which shall only be set by the next higher layer, is dependent upon macMinBE, macMaxBE, macMaxCSMABackoffs and the number of symbols per octet. See 7.4.2 for the formula relating the attributes.
Referenced by mlme_get(), mlme_set(), and wpan_mlme_set_req().
#define macMaxNumRxFramesDuringBackoff (0x7F) |
Private MAC PIB attribute to control the CSMA algorithm.
Maximum number of frames that are allowed to be received during CSMA backoff periods for a tx transaction.
#define macMinBE (0x4F) |
The minimum value of the backoff exponent in the CSMA-CA algorithm.
Note that if this value is set to 0, collision avoidance is disabled during the first iteration of the algorithm. Also note that for the slotted version of the CSMACA algorithm with the battery life extension enabled, the minimum value of the backoff exponent will be the lesser of 2 and the value of macMinBE.
Referenced by mlme_get(), mlme_set(), and tal_pib_set().
#define macMinLIFSPeriod (0x5E) |
The minimum number of symbols forming a LIFS period.
#define macMinLIFSPeriod_def (40) |
Default value for PIB macMinLIFSPeriod.
Referenced by calc_frame_transmit_duration(), calculate_transaction_duration(), mac_process_beacon_frame(), and send_frame().
#define macMinSIFSPeriod (0x5F) |
The minimum number of symbols forming a SIFS period.
#define macMinSIFSPeriod_def (12) |
Default value for PIB macMinSIFSPeriod.
Referenced by calc_frame_transmit_duration(), calculate_transaction_duration(), mac_process_beacon_frame(), and send_frame().
#define macPANCoordExtendedAddress (0x7D) |
The 64-bit address of the PAN coordinator.
Referenced by mlme_set().
#define macPANCoordShortAddress (0x7E) |
The 16-bit short address assinged to the PAN coordinator.
Referenced by mlme_set().
#define macPANId (0x50) |
The 16 bit identifier of the PAN on which the device is operating.
If this value is 0xffff, the device is not associated.
Referenced by mac_awake_scan(), mac_coord_realignment_command_tx_success(), mac_idle_trans(), mac_process_associate_response(), mac_process_coord_realign(), mac_process_orphan_realign(), mac_t_assocresponsetime_cb(), mlme_associate_request(), mlme_get(), mlme_set(), mlme_start_request(), scan_proceed(), tal_pib_set(), usr_mlme_scan_conf(), and usr_mlme_set_conf().
#define macPANId_def (0xFFFF) |
Default value for PIB macPANId.
Referenced by mac_idle_trans(), mac_process_associate_response(), and mac_t_assocresponsetime_cb().
#define macPromiscuousMode (0x51) |
This indicates whether the MAC sublayer is in a promiscuous (receive all) mode.
A value of true indicates that the MAC sublayer accepts all frames received from the PHY.
Referenced by mlme_get(), mlme_set(), and tal_pib_set().
#define macResponseWaitTime (0x5A) |
The maximum time, in multiples of aBaseSuperframeDuration, a device shall wait for a response command frame to be available following a request command frame.
Referenced by mlme_get(), mlme_set(), and wpan_mlme_set_req().
#define macResponseWaitTime_def (32 * aBaseSuperframeDuration) |
Default value for PIB macResponseWaitTime.
Referenced by do_init_pib().
#define macRxOnWhenIdle (0x52) |
This indicates whether the MAC sublayer is to enable its receiver during idle periods.
Referenced by mlme_get(), and mlme_set().
#define macRxOnWhenIdle_def (false) |
Default value for PIB macRxOnWhenIdle.
Referenced by do_init_pib().
#define macSecurityEnabled (0x5D) |
Indication of whether the MAC sublayer has security enabled.
A value of TRUE indicates that security is enabled, while a value of FALSE indicates that security is disabled.
Referenced by mlme_get(), and mlme_set().
#define macSecurityEnabled_def (false) |
Default value for PIB macSecurityEnabled.
Referenced by do_init_pib().
#define macShortAddress (0x53) |
The 16 bit address that the device uses to communicate in the PAN.
If the device is a PAN coordinator, this value shall be chosen before a PAN is started. Otherwise, the address is allocated by a coordinator during association. A value of 0xfffe indicates that the device has associated but has not been allocated an address. A value of 0xffff indicates that the device does not have a short address.
Referenced by mac_idle_trans(), mac_process_associate_response(), mac_process_coord_realign(), mac_process_orphan_realign(), mlme_get(), mlme_set(), and tal_pib_set().
#define macShortAddress_def (0xFFFF) |
Default value for PIB macShortAddress.
Referenced by mac_idle_trans().
#define macSuperframeOrder (0x54) |
This specifies the length of the active portion of the superframe, including the beacon frame.
The macSuperframeOrder, SO, and the superframe duration, SD, are related as follows: for 0 <= SO <= BO <= 14, SD = aBaseSuperframeDuration * 2SO symbols. If SO = 15, the superframe will not be active following the beacon.
Referenced by mac_coord_realignment_command_tx_success(), mac_process_beacon_frame(), mlme_get(), mlme_set(), mlme_start_request(), and tal_pib_set().
#define macSuperframeOrder_def (15) |
Default value for PIB macSuperframeOrder.
#define macSyncSymbolOffset (0x5B) |
The offset, measured in symbols, between the symbol boundary at which the MLME captures the timestamp of each transmitted or received frame, and the onset of the first symbol past the SFD, namely, the first symbol of the Length field.
#define macTimestampSupported (0x5C) |
Indication of whether the MAC sublayer supports the optional timestamping feature for incoming and outgoing data frames.
#define macTransactionPersistenceTime (0x55) |
The maximum time (in superframe periods) that a transaction is stored by a coordinator and indicated in its beacon.
Referenced by mlme_get(), mlme_set(), and wpan_mlme_set_req().
#define macTransactionPersistenceTime_def (0x01F4) |
Default value for PIB macTransactionPersistenceTime.
Referenced by do_init_pib().
#define MAX_KEY_ID_FIELD_LEN (9) |
Maximum length of the key id field.
#define MAX_MGMT_FRAME_LENGTH (30) |
Maximum size of the management frame(Association Response frame)
#define MIN_FRAME_LENGTH (8) |
Minimum size of a valid frame other than an Ack frame.
#define MLME_SCAN_TYPE_ACTIVE (0x01) |
Active scan (see wpan_mlme_scan_req())
Referenced by mac_awake_scan(), scan_proceed(), usr_mlme_get_conf(), and usr_mlme_scan_conf().
#define MLME_SCAN_TYPE_ED (0x00) |
Energy scan (see wpan_mlme_scan_req())
Referenced by mac_awake_scan(), mlme_scan_request(), and scan_proceed().
#define MLME_SCAN_TYPE_ORPHAN (0x03) |
Orphan scan (see wpan_mlme_scan_req())
Referenced by mac_awake_scan(), mac_process_orphan_realign(), and scan_proceed().
#define MLME_SCAN_TYPE_PASSIVE (0x02) |
Passive scan (see wpan_mlme_scan_req())
Referenced by mac_awake_scan(), scan_proceed(), and scan_set_complete().
#define NO_PIB_INDEX (0) |
Referenced by usr_mlme_associate_conf(), usr_mlme_get_conf(), usr_mlme_reset_conf(), and usr_mlme_scan_conf().
#define NON_BEACON_NWK (0x0F) |
BO value for nonbeacon-enabled network.
Referenced by check_start_parameter(), mac_awake_disassociate(), mac_build_and_tx_data_req(), mac_coord_realignment_command_tx_success(), mac_process_beacon_frame(), mac_sleep_trans(), mac_start_missed_beacon_timer(), mcps_data_request(), mlme_rx_enable_request(), mlme_start_request(), process_data_ind_not_transient(), tal_tx_frame(), and tx_pan_id_conf_notif().
#define NUM_LONG_PEND_ADDR | ( | x | ) | (((x) & 0x70) >> 4) |
Mask for the number of long addresses pending.
Referenced by mac_process_beacon_frame(), and parse_mpdu().
#define NUM_SHORT_PEND_ADDR | ( | x | ) | ((x) & 0x07) |
Mask for the number of short addresses pending.
Referenced by mac_process_beacon_frame(), and parse_mpdu().
#define PAN_ACCESS_DENIED (2) |
Association status code value (see wpan_mlme_associate_resp()).
#define PAN_AT_CAPACITY (1) |
Association status code value (see wpan_mlme_associate_resp()).
#define PAN_COORD_BIT_POS (14) |
PAN coordinator bit position.
#define PAN_ID_LEN (2) |
Length (in octets) of PAN ID.
Referenced by mac_extract_mhr_addr_info().
#define PHY_OVERHEAD (5) |
Number of octets added by the PHY: 4 sync octets + SFD octet.
Referenced by calc_frame_transmit_duration(), calculate_transaction_duration(), mac_process_beacon_frame(), and tx_done_handling().
#define PHY_SUCCESS_DATA_PENDING (0x10) |
PHY_SUCCESS in phyAutoCSMACA when received ACK frame had the pending bit set.
#define phyCCAMode (0x03) |
The CCA mode.
Referenced by mlme_get(), mlme_set(), and tal_pib_set().
#define phyChannelsSupported (0x01) |
The 5 most significant bits (MSBs) (b27, ..., b31) of phyChannelsSupported shall be reserved and set to 0, and the 27 LSBs (b0, b1, ..., b26) shall indicate the status (1 = available, 0 = unavailable) for each of the 27 valid channels (bk shall indicate the status of channel k).
Referenced by mlme_get(), and usr_mlme_get_conf().
#define phyCurrentChannel (0x00) |
The RF channel to use for all following transmissions and receptions.
Referenced by mac_coord_realignment_command_tx_success(), mac_process_coord_realign(), mac_process_orphan_realign(), mlme_associate_request(), mlme_get(), mlme_set(), mlme_start_request(), mlme_sync_request(), scan_clean_up(), scan_proceed(), and tal_pib_set().
#define phyCurrentPage (0x04) |
This is the current PHY channel page.
This is used in conjunction with phyCurrentChannel to uniquely identify the channel currently being used.
Referenced by mac_coord_realignment_command_tx_success(), mac_process_coord_realign(), mac_process_orphan_realign(), mlme_associate_request(), mlme_get(), mlme_set(), mlme_start_request(), mlme_sync_request(), scan_clean_up(), scan_proceed(), tal_pib_set(), usr_mlme_get_conf(), and usr_mlme_reset_conf().
#define phyMaxFrameDuration (0x05) |
The maximum number of symbols in a frame: = phySHRDuration + ceiling([aMaxPHYPacketSize + 1] x phySymbolsPerOctet)
Referenced by mlme_get().
#define phySHRDuration (0x06) |
The duration of the synchronization header (SHR) in symbols for the current PHY.
Referenced by mlme_get().
#define phySymbolsPerOctet (0x07) |
The number of symbols per octet for the current PHY.
Referenced by mlme_get().
#define phyTransmitPower (0x02) |
The 2 MSBs represent the tolerance on the transmit power: 00 = 1 dB 01 = 3 dB 10 = 6 dB The 6 LSBs represent a signed integer in twos-complement format, corresponding to the nominal transmit power of the device in decibels relative to 1 mW.
The lowest value of phyTransmitPower shall be interpreted as less than or equal to 32 dBm.
Referenced by mlme_get(), mlme_set(), tal_pib_set(), and tal_set_tx_pwr().
#define PL_POS_DST_ADDR_START (6) |
Octet start position of Destination Address field within payload array of frame_info_t.
Referenced by mac_prep_disassoc_conf().
#define PL_POS_DST_PAN_ID_START (4) |
Octet start position of Destination PAN-Id field within payload array of frame_info_t.
#define PL_POS_FCF_1 (1) |
Octet position of FCF octet one within payload array of frame_info_t.
Referenced by calc_frame_transmit_duration(), calculate_transaction_duration(), process_incoming_frame(), and tx_done_handling().
#define PL_POS_FCF_2 (2) |
Octet position of FCF octet two within payload array of frame_info_t.
Referenced by mac_prep_disassoc_conf().
#define PL_POS_SEQ_NUM (3) |
Octet position of Sequence Number octet within payload array of frame_info_t.
#define SEQ_NUM_LEN (1) |
Length of the sequence number field.
Referenced by mac_extract_mhr_addr_info().
#define SHORT_ADDR_LEN (2) |
Length (in octets) of short address.
Referenced by mac_extract_mhr_addr_info().
#define WPAN_TXOPT_ACK (0x01) |
Value for TxOptions parameter in wpan_mcps_data_req().
Referenced by build_data_frame(), mcps_data_request(), and usr_mlme_beacon_notify_ind().
#define WPAN_TXOPT_GTS (0x02) |
Value for TxOptions parameter in wpan_mcps_data_req().
Referenced by mcps_data_request().
#define WPAN_TXOPT_GTS_ACK (0x03) |
Value for TxOptions parameter in wpan_mcps_data_req().
#define WPAN_TXOPT_INDIRECT (0x04) |
Value for TxOptions parameter in wpan_mcps_data_req().
Referenced by mcps_data_request().
#define WPAN_TXOPT_INDIRECT_ACK (0x05) |
Value for TxOptions parameter in wpan_mcps_data_req().
#define WPAN_TXOPT_OFF (0x00) |
Value for TxOptions parameter in wpan_mcps_data_req().
typedef enum cca_mode_tag cca_mode_t |
CCA mode enumeration.
typedef enum phy_enum_tag phy_enum_t |
typedef enum trx_cca_mode_tag trx_cca_mode_t |
CCA Modes of the transceiver.
enum cca_mode_tag |
enum ch_pg_tag |
enum phy_enum_tag |
enum trx_cca_mode_tag |