Declarations for low-level security API.
Copyright (c) 2013-2018 Microchip Technology Inc. and its subsidiaries.
Macros | |
#define | AES_DIR_DECRYPT (1) |
Defines AES direction as decryption. More... | |
#define | AES_DIR_ENCRYPT (0) |
Defines AES direction as encryption. More... | |
#define | AES_MODE_CBC (2) |
Defines AES mode as CBC. More... | |
#define | AES_MODE_ECB (0) |
Defines AES mode as ECB. More... | |
#define | sal_aes_clean_up() _sal_aes_clean_up() |
Route function macro to the corresponding function. More... | |
Functions | |
void | _sal_aes_clean_up (void) |
Cleans up the SAL/AES after STB has been completed. More... | |
void | sal_aes_exec (uint8_t *data) |
En/decrypt one AES block. More... | |
void | sal_aes_read (uint8_t *data) |
Reads the result of previous AES en/decryption. More... | |
void | sal_aes_restart (void) |
Re-inits key and state after a sleep or TRX reset. More... | |
bool | sal_aes_setup (uint8_t *key, uint8_t enc_mode, uint8_t dir) |
Setup AES unit. More... | |
void | sal_aes_wrrd (uint8_t *idata, uint8_t *odata) |
Writes data, reads previous result and does the AES en/decryption. More... | |
void | sal_init (void) |
Initialization of SAL. More... | |
#define AES_DIR_DECRYPT (1) |
Defines AES direction as decryption.
#define AES_DIR_ENCRYPT (0) |
Defines AES direction as encryption.
#define AES_MODE_CBC (2) |
Defines AES mode as CBC.
#define AES_MODE_ECB (0) |
Defines AES mode as ECB.
#define sal_aes_clean_up | ( | ) | _sal_aes_clean_up() |
Route function macro to the corresponding function.
Referenced by stb_ccm_secure().
void _sal_aes_clean_up | ( | void | ) |
Cleans up the SAL/AES after STB has been completed.
This function puts the radio to SLEEP if it has been in SLEEP before sal_aes_restart().
void sal_aes_exec | ( | uint8_t * | data | ) |
En/decrypt one AES block.
The function returns after the AES operation is finished.
[in] | data | AES block to be en/decrypted |
References AES_BLOCKSIZE, and keyp.
Referenced by compute_mic(), encrypt_pldmic(), encrypt_with_padding(), and sal_aes_setup().
void sal_aes_read | ( | uint8_t * | data | ) |
Reads the result of previous AES en/decryption.
This function returns the result of the previous AES operation, so this function is needed in order to get the last result of a series of sal_aes_wrrd() calls.
[out] | data | - result of previous operation |
This function returns the result of the previous AES operation.
[out] | data | - result of previous operation |
References AES_BLOCKSIZE.
Referenced by compute_mic(), and encrypt_pldmic().
void sal_aes_restart | ( | void | ) |
Re-inits key and state after a sleep or TRX reset.
This function re-initializes the AES key and the state of the AES engine after TRX sleep or reset. The contents of AES register AES_CON is restored, the next AES operation started with sal_aes_exec() will be executed correctly.
Re-inits key and state after a sleep or TRX reset.
This function is void for ATxmega since the key must be re-initialized before every block encryption anyway.
bool sal_aes_setup | ( | uint8_t * | key, |
uint8_t | enc_mode, | ||
uint8_t | dir | ||
) |
Setup AES unit.
This function perform the following tasks as part of the setup of the AES unit: key initialization, set encryption mode.
[in] | key | AES key or NULL (NULL: use last key) |
[in] | enc_mode | AES_MODE_ECB or AES_MODE_CBC |
[in] | dir | must be AES_DIR_ENCRYPT |
This function performs the following tasks as part of the setup of the AES unit: key initialization, set encryption direction and encryption mode.
In general, the contents of SRAM buffer is destroyed. When using sal_aes_wrrd(), sal_aes_read() needs to be called in order to get the result of the last AES operation before you may call sal_aes_setup() again.
[in] | key | AES key or NULL (NULL: use last key) |
[in] | enc_mode | AES_MODE_ECB or AES_MODE_CBC |
[in] | dir | AES_DIR_ENCRYPT or AES_DIR_DECRYPT |
References AES_BLOCKSIZE, AES_DIR_DECRYPT, AES_DIR_ENCRYPT, AES_DIR_VOID, AES_KEYSIZE, AES_MODE_CBC, AES_MODE_ECB, COMP_SR, dec_initialized, dec_key, enc_key, keyp, last_dir, mode_byte, and sal_aes_exec().
Referenced by compute_mic(), encrypt_pldmic(), and stb_ccm_secure().
void sal_aes_wrrd | ( | uint8_t * | idata, |
uint8_t * | odata | ||
) |
Writes data, reads previous result and does the AES en/decryption.
The function returns after the AES operation is finished.
When sal_aes_wrrd() is called several times in sequence, from the second call onwards, odata contains the result of the previous operation. To obtain the last result, you must call sal_aes_read() at the end. Please note that any call of sal_aes_setup() as well as putting the transceiver to sleep state destroys the SRAM contents, i.e. the next call of sal_aes_wrrd() yields no meaningful result.
[in] | idata | AES block to be en/decrypted |
[out] | odata | Result of previous operation (odata may be NULL or equal to idata) |
Referenced by compute_mic(), and encrypt_with_padding().
void sal_init | ( | void | ) |
Initialization of SAL.
This functions initializes the SAL.
References COMP_SR, SYSCLK_AES, sysclk_enable_module(), and SYSCLK_PORT_GEN.
Referenced by stb_init().