Microchip® Advanced Software Framework

trx_access.c File Reference
#include "board.h"
#include "spi_master.h"
#include "trx_access.h"
#include "delay.h"
#include "interrupt.h"
#include "conf_board.h"
#include "asf.h"

Functions

 if (irq_hdl_trx)
 
void PhyReset (void)
 Resets the TRX radio. More...
 
void trx_aes_wrrd (uint8_t addr, uint8_t *idata, uint8_t length)
 Writes and reads data into/from SRAM of the transceiver. More...
 
uint8_t trx_bit_read (uint8_t addr, uint8_t mask, uint8_t pos)
 Subregister read. More...
 
void trx_bit_write (uint8_t reg_addr, uint8_t mask, uint8_t pos, uint8_t new_value)
 Subregister write. More...
 
void trx_frame_read (uint8_t *data, uint8_t length)
 Reads frame buffer of the transceiver. More...
 
void trx_frame_write (uint8_t *data, uint8_t length)
 Writes data into frame buffer of the transceiver. More...
 
void trx_irq_init (FUNC_PTR trx_irq_cb)
 
uint8_t trx_reg_read (uint8_t addr)
 Reads current value from a transceiver register. More...
 
void trx_reg_write (uint8_t addr, uint8_t data)
 Writes data into a transceiver register. More...
 
void trx_spi_disable (void)
 Disables the SPI interface for communication with the transceiver. More...
 
void trx_spi_enable (void)
 enables the SPI interface for communication with the transceiver More...
 
void trx_spi_init (void)
 Initializes the SPI interface for communication with the transceiver. More...
 
void trx_sram_read (uint8_t addr, uint8_t *data, uint8_t length)
 Reads data from SRAM of the transceiver. More...
 
void trx_sram_write (uint8_t addr, uint8_t *data, uint8_t length)
 Writes data into SRAM of the transceiver. More...
 

Variables

static irq_handler_t irq_hdl_trx = NULL
 
struct spi_device SPI_AT86RFX_DEVICE
 

irq_handler_t irq_hdl_trx = NULL
static

Referenced by if(), and trx_irq_init().

struct spi_device SPI_AT86RFX_DEVICE
Initial value:
= {
}
#define AT86RFX_SPI_CS
Definition: xmega_rf212b_zigbit.h:134