#include <tal.h>
Data Fields | |
uint16_t | agc_settle_dur |
Settling duration of the AGC. More... | |
uint8_t | CCAMode |
CCA Mode. More... | |
uint8_t | CurrentChannel |
Current RF channel to be used for all transmissions and receptions. More... | |
uint8_t | CurrentPage |
Current channel page. More... | |
uint64_t | IeeeAddress |
64-bit (IEEE) address of the node. More... | |
uint8_t | MaxBE |
The maximum value of the backoff exponent BE in the CSMA-CA algorithm. More... | |
uint8_t | MaxCSMABackoffs |
The maximum number of back-offs the CSMA-CA algorithm will attempt before declaring a CSMA_CA failure. More... | |
uint16_t | MaxFrameDuration |
Maximum number of symbols in a frame: = phySHRDuration + ceiling([aMaxPHYPacketSize + 1] x phySymbolsPerOctet) More... | |
uint8_t | MaxFrameRetries |
The maximum number of retries allowed after a transmission failure. More... | |
uint8_t | MinBE |
The minimum value of the backoff exponent BE in the CSMA-CA algorithm. More... | |
uint16_t | PANId |
16-bit PAN ID More... | |
bool | PrivatePanCoordinator |
Indicates if the node is a PAN coordinator or not. More... | |
uint16_t | ShortAddress |
16-bit short address of the node. More... | |
uint8_t | SHRDuration |
Duration of the synchronization header (SHR) in symbols for the current PHY. More... | |
uint32_t | SupportedChannels |
Supported channels. More... | |
uint8_t | SymbolsPerOctet |
Number of symbols per octet for the current PHY. More... | |
uint8_t | TransmitPower |
Default value of transmit power of transceiver using IEEE defined format of phyTransmitPower. More... | |
uint16_t tal_pib_tag::agc_settle_dur |
Settling duration of the AGC.
uint8_t tal_pib_tag::CCAMode |
CCA Mode.
uint8_t tal_pib_tag::CurrentChannel |
Current RF channel to be used for all transmissions and receptions.
uint8_t tal_pib_tag::CurrentPage |
Current channel page.
uint64_t tal_pib_tag::IeeeAddress |
64-bit (IEEE) address of the node.
uint8_t tal_pib_tag::MaxBE |
The maximum value of the backoff exponent BE in the CSMA-CA algorithm.
uint8_t tal_pib_tag::MaxCSMABackoffs |
The maximum number of back-offs the CSMA-CA algorithm will attempt before declaring a CSMA_CA failure.
uint16_t tal_pib_tag::MaxFrameDuration |
Maximum number of symbols in a frame: = phySHRDuration + ceiling([aMaxPHYPacketSize + 1] x phySymbolsPerOctet)
uint8_t tal_pib_tag::MaxFrameRetries |
The maximum number of retries allowed after a transmission failure.
uint8_t tal_pib_tag::MinBE |
The minimum value of the backoff exponent BE in the CSMA-CA algorithm.
uint16_t tal_pib_tag::PANId |
16-bit PAN ID
bool tal_pib_tag::PrivatePanCoordinator |
Indicates if the node is a PAN coordinator or not.
uint16_t tal_pib_tag::ShortAddress |
16-bit short address of the node.
uint8_t tal_pib_tag::SHRDuration |
Duration of the synchronization header (SHR) in symbols for the current PHY.
uint32_t tal_pib_tag::SupportedChannels |
Supported channels.
Legacy trx: Bit mask, whereas each bit position set indicates that the channel, corresponding to this particular bit position, is actually supported
Multi-Trx devices: Min channel: Low word of variable SupportedChannels: (uint16_t)(SupportedChannels) Max channel: High word of variable SupportedChannels: (uint16_t)(SupportedChannels >> 16)
uint8_t tal_pib_tag::SymbolsPerOctet |
Number of symbols per octet for the current PHY.
uint8_t tal_pib_tag::TransmitPower |
Default value of transmit power of transceiver using IEEE defined format of phyTransmitPower.