PAN descriptor information structure.
#include <mac_api.h>
Data Fields | |
uint8_t | ChannelPage |
The current channel page occupied by the network. More... | |
wpan_addr_spec_t | CoordAddrSpec |
Coordinator address specification in received beacon frame. More... | |
bool | GTSPermit |
Set to true if the beacon is from a PAN coordinator accepting GTS requests. More... | |
uint8_t | LinkQuality |
LQI at which the beacon was received. More... | |
uint8_t | LogicalChannel |
The current logical channel used by the network. More... | |
uint16_t | SuperframeSpec |
Superframe specification in received beacon frame. More... | |
uint32_t | TimeStamp |
Time at which the beacon frame was received, in symbol counts. More... | |
uint8_t wpan_pandescriptor_tag::ChannelPage |
The current channel page occupied by the network.
Referenced by mac_process_beacon_frame().
wpan_addr_spec_t wpan_pandescriptor_tag::CoordAddrSpec |
Coordinator address specification in received beacon frame.
Referenced by mac_process_beacon_frame().
bool wpan_pandescriptor_tag::GTSPermit |
Set to true if the beacon is from a PAN coordinator accepting GTS requests.
Referenced by mac_process_beacon_frame().
uint8_t wpan_pandescriptor_tag::LinkQuality |
LQI at which the beacon was received.
Lower values represent poorer link quality.
Referenced by mac_process_beacon_frame().
uint8_t wpan_pandescriptor_tag::LogicalChannel |
The current logical channel used by the network.
Referenced by mac_process_beacon_frame().
uint16_t wpan_pandescriptor_tag::SuperframeSpec |
Superframe specification in received beacon frame.
Referenced by mac_process_beacon_frame().
uint32_t wpan_pandescriptor_tag::TimeStamp |
Time at which the beacon frame was received, in symbol counts.
This quantity shall be interpreted as only 24-bits, with the most significant 8-bits entirely ignored.
Referenced by mac_process_beacon_frame().