Provides MAC API to access MAC Layer functionality.
Copyright (c) 2013-2018 Microchip Technology Inc. and its subsidiaries.
#include <stdint.h>
#include <stdbool.h>
#include "stack_config.h"
#include "tal_generic.h"
#include "return_val.h"
#include "mac_api.h"
#include "qmm.h"
#include "mac_build_config.h"
Macros | |
#define | FCF_ADDR_MASK (3) |
#define | FCF_GET_DEST_ADDR_MODE(x) (((x) >> FCF_DEST_ADDR_OFFSET) & FCF_ADDR_MASK) |
#define | FCF_GET_SOURCE_ADDR_MODE(x) (((x) >> FCF_SOURCE_ADDR_OFFSET) & FCF_ADDR_MASK) |
#define | MAX_ALLOWED_PAN_DESCRIPTORS |
Maximum allowed PANDescriptors that is calculated using the large buffer size. More... | |
#define | MAX_PANDESCRIPTORS (MAX_ALLOWED_PAN_DESCRIPTORS > 5 ? 5 : MAX_ALLOWED_PAN_DESCRIPTORS) |
Active/passive scan: implementation-defined maximum number of PANDescriptors that can be stored. More... | |
Functions | |
uint8_t | mac_extract_mhr_addr_info (uint8_t *frame_ptr) |
retval_t | mac_init (void) |
Initializes the MAC sublayer. More... | |
bool | mac_task (void) |
Runs the MAC scheduler. More... | |
void | mcps_data_conf (uint8_t *m) |
Wrapper function for messages of type mcps_data_conf_t. More... | |
void | mcps_data_ind (uint8_t *m) |
Wrapper function for messages of type mcps_data_ind_t. More... | |
void | mcps_data_request (uint8_t *msg) |
Builds the data frame for transmission. More... | |
void | mlme_associate_conf (uint8_t *m) |
Wrapper function for messages of type mlme_associate_conf_t. More... | |
void | mlme_associate_request (uint8_t *m) |
Handles the MLME associate request command from the NWK layer. More... | |
void | mlme_beacon_notify_ind (uint8_t *m) |
Wrapper function for messages of type mlme_beacon_notify_ind_t. More... | |
void | mlme_disassociate_conf (uint8_t *m) |
Wrapper function for messages of type mlme_disassociate_conf_t. More... | |
void | mlme_disassociate_ind (uint8_t *m) |
Wrapper function for messages of type mlme_disassociate_ind_t. More... | |
void | mlme_disassociate_request (uint8_t *m) |
Handles the MLME disassociate request command from the NWK layer. More... | |
retval_t | mlme_get (uint8_t attribute, pib_value_t *attribute_value) |
void | mlme_get_conf (uint8_t *m) |
Wrapper function for messages of type mlme_get_conf_t. More... | |
void | mlme_get_request (uint8_t *m) |
Handles an MLME-GET.request. More... | |
void | mlme_poll_conf (uint8_t *m) |
Wrapper function for messages of type mlme_poll_conf_t. More... | |
void | mlme_poll_request (uint8_t *m) |
Implements MLME-POLL.request. More... | |
void | mlme_reset_conf (uint8_t *m) |
Wrapper function for messages of type mlme_reset_conf_t. More... | |
void | mlme_reset_request (uint8_t *m) |
Resets the MAC layer. More... | |
void | mlme_rx_enable_conf (uint8_t *m) |
Wrapper function for messages of type mlme_rx_enable_conf_t. More... | |
void | mlme_rx_enable_request (uint8_t *m) |
Implement the MLME-RX-ENABLE.request primitive. More... | |
void | mlme_scan_conf (uint8_t *m) |
Wrapper function for messages of type mlme_scan_conf_t. More... | |
void | mlme_scan_request (uint8_t *m) |
The MLME-SCAN.request primitive makes a request for a node to start a scan procedure. More... | |
retval_t | mlme_set (uint8_t attribute, pib_value_t *attribute_value, bool set_trx_to_sleep) |
void | mlme_set_conf (uint8_t *m) |
Wrapper function for messages of type mlme_set_conf_t. More... | |
void | mlme_set_request (uint8_t *m) |
Handles an MLME-SET.request primitive. More... | |
void | mlme_sync_loss_ind (uint8_t *m) |
Wrapper function for messages of type mlme_sync_loss_ind_t. More... | |
void | mlme_sync_request (uint8_t *m) |
Implements the MLME-SYNC request. More... | |
Variables | |
queue_t | mac_nhle_q |
Queue used by MAC for communication to next higher layer. More... | |
queue_t | nhle_mac_q |
#define FCF_ADDR_MASK (3) |
#define FCF_GET_DEST_ADDR_MODE | ( | x | ) | (((x) >> FCF_DEST_ADDR_OFFSET) & FCF_ADDR_MASK) |
#define FCF_GET_SOURCE_ADDR_MODE | ( | x | ) | (((x) >> FCF_SOURCE_ADDR_OFFSET) & FCF_ADDR_MASK) |
#define MAX_ALLOWED_PAN_DESCRIPTORS |
Maximum allowed PANDescriptors that is calculated using the large buffer size.
#define MAX_PANDESCRIPTORS (MAX_ALLOWED_PAN_DESCRIPTORS > 5 ? 5 : MAX_ALLOWED_PAN_DESCRIPTORS) |
Active/passive scan: implementation-defined maximum number of PANDescriptors that can be stored.
uint8_t mac_extract_mhr_addr_info | ( | uint8_t * | frame_ptr | ) |
retval_t mlme_get | ( | uint8_t | attribute, |
pib_value_t * | attribute_value | ||
) |
queue_t mac_nhle_q |
Queue used by MAC for communication to next higher layer.
queue_t nhle_mac_q |