MAC Example Nobeacon Application - Device.
Copyright (c) 2013-2018 Microchip Technology Inc. and its subsidiaries.
#include <string.h>
#include <inttypes.h>
#include <stdio.h>
#include "conf_board.h"
#include "avr2025_mac.h"
#include "delay.h"
#include "common_sw_timer.h"
#include "sio2host.h"
#include "common_hw_timer.h"
#include "beacon_app.h"
#include <asf.h>
Macros | |
#define | APP_GUARD_TIME_US (10000) |
#define | APP_POLL_PERIOD_MS (5000) |
This is the time period in micro seconds for polling transmissions. More... | |
#define | CHANNEL_OFFSET (2) |
Channel Offset will give us the channel number as (CHANNEL_OFFSET + 11) More... | |
#define | LED_DATA (LED0) |
#define | LED_DATA (LED0) |
#define | LED_NWK_SETUP (LED0) |
#define | LED_ON_DURATION (500000) |
Define the LED on duration time. More... | |
#define | LED_START (LED0) |
#define | MCU_WAKEUP_TIME (150) |
#define | PAYLOAD_LEN (104) |
#define | SCAN_DURATION_LONG (6) |
Defines the long scan duration time. More... | |
#define | SCAN_DURATION_SHORT (5) |
Defines the short scan duration time. More... | |
#define | TIMER_SYNC_BEFORE_ASSOC_MS (3000) |
Functions | |
static void | app_alert (void) |
Alert to indicate something has gone wrong in the application. More... | |
static void | app_initiate_polling (void *parameter) |
Callback function for the application timer initiating polling of coordinator. More... | |
int | main (void) |
Main function of the device application. More... | |
static void | network_search_indication_cb (void *parameter) |
Callback function indicating network search. More... | |
static void | print_stack_app_build_features (void) |
This function shows the stack and application capabilities on terminal if SIO_HUB switch is enabled. More... | |
static void | rx_data_led_off_cb (void *parameter) |
Callback function for switching off the LED after data reception. More... | |
static void | send_data (uint8_t *data) |
function for the sending received data back to coordinator More... | |
void | usr_mcps_data_conf (uint8_t msduHandle, uint8_t status, uint32_t Timestamp) |
Callback function that must be implemented by application (NHLE) for MAC service MCPS-DATA.confirm. More... | |
void | usr_mcps_data_ind (wpan_addr_spec_t *SrcAddrSpec, wpan_addr_spec_t *DstAddrSpec, uint8_t msduLength, uint8_t *msdu, uint8_t mpduLinkQuality, uint8_t DSN, uint32_t Timestamp) |
void | usr_mlme_associate_conf (uint16_t AssocShortAddress, uint8_t status) |
Callback function that must be implemented by application (NHLE) for MAC service MLME-ASSOCIATE.confirm. More... | |
void | usr_mlme_beacon_notify_ind (uint8_t BSN, wpan_pandescriptor_t *PANDescriptor, uint8_t PendAddrSpec, uint8_t *AddrList, uint8_t sduLength, uint8_t *sdu) |
Callback function that must be implemented by application (NHLE) for MAC service MLME-BEACON-NOTIFY.indication. More... | |
void | usr_mlme_disassociate_conf (uint8_t status, wpan_addr_spec_t *DeviceAddrSpec) |
Callback function that must be implemented by application (NHLE) for MAC service MLME-DISASSOCIATE.confirm. More... | |
void | usr_mlme_disassociate_ind (uint64_t DeviceAddress, uint8_t DisassociateReason) |
Callback function that must be implemented by application (NHLE) for MAC service MLME-DISASSOCIATE.indication. More... | |
void | usr_mlme_get_conf (uint8_t status, uint8_t PIBAttribute, void *PIBAttributeValue) |
Callback function that must be implemented by application (NHLE) for MAC service MLME-GET.confirm. More... | |
void | usr_mlme_poll_conf (uint8_t status) |
Callback function that must be implemented by application (NHLE) for MAC service MLME-POLL.confirm. More... | |
void | usr_mlme_reset_conf (uint8_t status) |
Callback function that must be implemented by application (NHLE) for MAC service MLME-RESET.confirm. More... | |
void | usr_mlme_rx_enable_conf (uint8_t status) |
Callback function that must be implemented by application (NHLE) for MAC service MLME-RX-ENABLE.confirm. More... | |
void | usr_mlme_scan_conf (uint8_t status, uint8_t ScanType, uint8_t ChannelPage, uint32_t UnscannedChannels, uint8_t ResultListSize, void *ResultList) |
Callback function that must be implemented by application (NHLE) for MAC service MLME-SCAN.confirm. More... | |
void | usr_mlme_set_conf (uint8_t status, uint8_t PIBAttribute) |
Callback function that must be implemented by application (NHLE) for MAC service MLME-SET.confirm. More... | |
void | usr_mlme_sync_loss_ind (uint8_t LossReason, uint16_t PANId, uint8_t LogicalChannel, uint8_t ChannelPage) |
Callback function that must be implemented by application (NHLE) for MAC service MLME-SYNC-LOSS.indication. More... | |
Variables | |
app_state_t | app_state = APP_IDLE |
This variable stores the current state of the node. More... | |
static uint8_t | APP_TIMER |
static uint8_t | APP_TIMER_POLL_DATA |
static uint32_t | bc_rx_cnt |
static uint32_t | channels_supported |
static uint16_t | coord_addr |
This structure stores the short address of the coordinator. More... | |
wpan_addr_spec_t | coord_addr_spec |
uint8_t | current_channel |
uint8_t | current_channel_page |
uint8_t | default_key_source [8] |
static uint32_t | indirect_rx_cnt |
static uint8_t | msdu_payload [PAYLOAD_LEN] |
This array stores the current msdu payload. More... | |
#define APP_GUARD_TIME_US (10000) |
Referenced by main().
#define APP_POLL_PERIOD_MS (5000) |
This is the time period in micro seconds for polling transmissions.
Referenced by usr_mlme_associate_conf(), and usr_mlme_poll_conf().
#define CHANNEL_OFFSET (2) |
Channel Offset will give us the channel number as (CHANNEL_OFFSET + 11)
Referenced by usr_mlme_get_conf().
#define LED_DATA (LED0) |
Referenced by main(), rx_data_led_off_cb(), and usr_mcps_data_ind().
#define LED_DATA (LED0) |
#define LED_NWK_SETUP (LED0) |
Referenced by main(), network_search_indication_cb(), and usr_mlme_associate_conf().
#define LED_ON_DURATION (500000) |
Define the LED on duration time.
Referenced by network_search_indication_cb(), usr_mcps_data_ind(), and usr_mlme_get_conf().
#define MCU_WAKEUP_TIME (150) |
#define PAYLOAD_LEN (104) |
Referenced by usr_mlme_beacon_notify_ind().
#define SCAN_DURATION_LONG (6) |
Defines the long scan duration time.
Referenced by usr_mlme_get_conf(), and usr_mlme_scan_conf().
#define SCAN_DURATION_SHORT (5) |
Defines the short scan duration time.
Referenced by usr_mlme_scan_conf().
#define TIMER_SYNC_BEFORE_ASSOC_MS (3000) |
|
static |
Alert to indicate something has gone wrong in the application.
References delay_us, LED0, and LED_Toggle.
Referenced by main().
|
static |
Callback function for the application timer initiating polling of coordinator.
parameter | Pointer to callback parameter (not used in this application, but could be if desired). |
References wpan_addr_spec_tag::Addr, wpan_addr_spec_tag::AddrMode, coord_addr, coord_addr_spec, DEFAULT_PAN_ID, wpan_addr_spec_tag::PANId, address_field_t::short_address, WPAN_ADDRMODE_SHORT, and wpan_mlme_poll_req().
Referenced by usr_mlme_associate_conf(), and usr_mlme_poll_conf().
int main | ( | void | ) |
Main function of the device application.
References app_alert(), APP_GUARD_TIME_US, APP_TIMER, APP_TIMER_POLL_DATA, board_init(), cpu_irq_enable, delay_init, irq_initialize_vectors, LED_DATA, LED_NWK_SETUP, LED_Off, LED_On, LED_START, mac_ready_to_sleep(), MAC_SUCCESS, print_stack_app_build_features(), sio2host_getchar(), sio2host_init(), sw_timer_get_id(), sw_timer_init(), sysclk_init(), wpan_init(), wpan_mlme_reset_req(), and wpan_task().
|
static |
Callback function indicating network search.
parameter | Pointer to callback parameter (not used in this application, but could be if desired). |
References APP_TIMER, FUNC_PTR, LED_NWK_SETUP, LED_ON_DURATION, LED_Toggle, SW_TIMEOUT_RELATIVE, and sw_timer_start().
Referenced by usr_mlme_get_conf().
|
static |
This function shows the stack and application capabilities on terminal if SIO_HUB switch is enabled.
Referenced by main().
|
static |
Callback function for switching off the LED after data reception.
parameter | Pointer to callback parameter (not used in this application, but could be if desired). |
References LED_DATA, and LED_Off.
Referenced by usr_mcps_data_ind().
|
static |
function for the sending received data back to coordinator
data | Pointer to received data |
References wpan_addr_spec_tag::Addr, ADDR_COPY_DST_SRC_16, wpan_addr_spec_tag::AddrMode, coord_addr, DEFAULT_PAN_ID, wpan_addr_spec_tag::PANId, address_field_t::short_address, WPAN_ADDRMODE_SHORT, wpan_mcps_data_req(), and WPAN_TXOPT_ACK.
Referenced by usr_mcps_data_ind().
void usr_mcps_data_ind | ( | wpan_addr_spec_t * | SrcAddrSpec, |
wpan_addr_spec_t * | DstAddrSpec, | ||
uint8_t | msduLength, | ||
uint8_t * | msdu, | ||
uint8_t | mpduLinkQuality, | ||
uint8_t | DSN, | ||
uint32_t | Timestamp | ||
) |
References wpan_addr_spec_tag::Addr, APP_TIMER, bc_rx_cnt, BROADCAST, FUNC_PTR, indirect_rx_cnt, LED_DATA, LED_On, LED_ON_DURATION, rx_data_led_off_cb(), send_data(), address_field_t::short_address, SW_TIMEOUT_RELATIVE, and sw_timer_start().
Referenced by mcps_data_ind().
app_state_t app_state = APP_IDLE |
This variable stores the current state of the node.
Referenced by usr_mlme_associate_conf(), usr_mlme_beacon_notify_ind(), usr_mlme_reset_conf(), usr_mlme_scan_conf(), and usr_mlme_set_conf().
|
static |
Referenced by main(), network_search_indication_cb(), usr_mcps_data_ind(), usr_mlme_associate_conf(), and usr_mlme_get_conf().
|
static |
Referenced by main(), usr_mlme_associate_conf(), and usr_mlme_poll_conf().
|
static |
Referenced by usr_mcps_data_ind().
|
static |
Referenced by usr_mlme_get_conf().
|
static |
This structure stores the short address of the coordinator.
Referenced by app_initiate_polling(), mlme_poll_request(), and send_data().
wpan_addr_spec_t coord_addr_spec |
Referenced by app_initiate_polling().
uint8_t current_channel |
Referenced by usr_mlme_beacon_notify_ind(), usr_mlme_get_conf(), usr_mlme_scan_conf(), and usr_mlme_set_conf().
uint8_t current_channel_page |
Referenced by usr_mlme_beacon_notify_ind(), usr_mlme_get_conf(), usr_mlme_scan_conf(), and usr_mlme_set_conf().
uint8_t default_key_source[8] |
Referenced by usr_mlme_reset_conf().
|
static |
Referenced by usr_mcps_data_ind().
|
static |
This array stores the current msdu payload.
Referenced by usr_mlme_beacon_notify_ind().