These are application-specific resources which are used in the example application of the coordinator in addition to the underlaying stack.
Copyright (c) 2013-2018 Microchip Technology Inc. and its subsidiaries.
Data Structures | |
struct | associated_device_tag |
This type definition of a structure can store the short address and the extended address of a device. More... | |
Macros | |
#define | COORD_SHORT_ADDR (0x0000) |
Defines the short address of the coordinator. More... | |
#define | DEFAULT_PAN_ID CCPU_ENDIAN_TO_LE16(0x1111) |
#define | SCAN_CHANNEL(x) (1ul << x) |
Typedefs | |
typedef enum app_state_tag | app_state_t |
This enum stores the current state of the application. More... | |
typedef struct associated_device_tag | associated_device_t |
This type definition of a structure can store the short address and the extended address of a device. More... | |
Enumerations | |
enum | app_state_tag { APP_IDLE = 0, APP_SCAN_DONE, APP_ASSOC_IN_PROGRESS, APP_DEVICE_RUNNING } |
This enum stores the current state of the application. More... | |
#define COORD_SHORT_ADDR (0x0000) |
Defines the short address of the coordinator.
#define DEFAULT_PAN_ID CCPU_ENDIAN_TO_LE16(0x1111) |
Referenced by app_initiate_polling(), send_data(), and usr_mlme_scan_conf().
#define SCAN_CHANNEL | ( | x | ) | (1ul << x) |
Referenced by usr_mlme_get_conf(), and usr_mlme_scan_conf().
typedef enum app_state_tag app_state_t |
This enum stores the current state of the application.
typedef struct associated_device_tag associated_device_t |
This type definition of a structure can store the short address and the extended address of a device.
enum app_state_tag |