These are application-specific resources which are used in the test harness application in addition to the underlaying stack.
Copyright (c) 2013-2018 Microchip Technology Inc. and its subsidiaries.
Macros | |
#define | NUMBER_OF_APP_TIMERS (0) |
Defines the number of timers used by the application. More... | |
#define | TOTAL_NUMBER_OF_TIMERS (NUMBER_OF_APP_TIMERS) |
Defines the total number of timers used by the application and the layers below. More... | |
#define NUMBER_OF_APP_TIMERS (0) |
Defines the number of timers used by the application.
#define TOTAL_NUMBER_OF_TIMERS (NUMBER_OF_APP_TIMERS) |
Defines the total number of timers used by the application and the layers below.