#include <mac_internal.h>
Data Fields | |
uint8_t | mac_AssociatedPANCoord |
Indication of whether the device is associated to the PAN through the PAN coordinator. More... | |
uint8_t | mac_AssociationPermit |
Holds the value which states whether a coordinator is currently allowing association. More... | |
uint8_t | mac_AutoRequest |
Holds the value which states whether a device automatically sends a data request command if its address is listed in the beacon frame. More... | |
uint8_t | mac_BattLifeExtPeriods |
Holds the value which states the number of backoff periods during which the receiver is enabled following a beacon in battery life extension mode. More... | |
uint8_t | mac_BeaconPayloadLength |
Holds the length, in octets, of the beacon payload. More... | |
uint8_t | mac_BSN |
Holds the sequence number added to the transmitted beacon frame. More... | |
uint64_t | mac_CoordExtendedAddress |
Holds the 64 bit address of the coordinator with which the device is associated. More... | |
uint16_t | mac_CoordShortAddress |
Holds the 16 bit short address of the coordinator with which the device is associated. More... | |
uint8_t | mac_DSN |
Holds the sequence number of the transmitted data or command frame. More... | |
uint8_t | mac_GTSPermit |
uint16_t | mac_MaxFrameTotalWaitTime |
The maximum number of CAP symbols in a beaconenabled PAN, or symbols in a nonbeacon-enabled PAN, to wait either for a frame intended as a response to a data request frame or for a broadcast frame following a beacon with the Frame Pending subfield set to one. More... | |
uint16_t | mac_ResponseWaitTime |
The maximum time, in multiples of aBaseSuperframeDuration, a device shall wait for a response command frame to be available following a request command frame. More... | |
bool | mac_RxOnWhenIdle |
Holds the value which states whether the MAC sublayer is to enable its receiver during idle periods. More... | |
bool | mac_SecurityEnabled |
Indication of whether the MAC sublayer has security enabled. More... | |
uint16_t | mac_TransactionPersistenceTime |
Holds the maximum time (in superframe periods) that a indirect transaction is stored by a PAN coordinator. More... | |
uint8_t | privateIllegalFrameType |
Holds the private MAC PIB attribute to generate a frame with an illegale frame type. More... | |
uint8_t | privateNoDataAfterAssocReq |
Holds the private MAC PIB attribute which suppresses the initiation of a data request frame after association request. More... | |
uint8_t | privateVirtualPANs |
Holds the private MAC PIB attribute to pretend virtual Beacon-enabled PANs. More... | |