mlme_rx_enable_conf_tag Struct Reference
MAC Data Structures
This is the MLME-RX-ENABLE.confirm message structure.
#include <mac_msg_types.h>
Data Fields
enum
msg_code
cmdcode
This identifies the message as
MLME_RX_ENABLE_CONFIRM
.
More...
uint8_t
status
The result of the receiver enable request.
More...
Generated on Sat Mar 5 2022 00:34:27 for MAC Serial Interface Beacon FFD AT86RF233 (ATREB233-XPRO) - SAM4S Xplained Pro by
1.8.5