Buffer Management (large and small buffers): provides services for dynamically allocating and freeing memory buffers.
Data Structures | |
struct | buffer_t |
Buffer structure holding information of each buffer. More... | |
Macros | |
#define | BMM_BUFFER_POINTER(buf) ((buf)->body) |
This macro provides the pointer to the corresponding body of the supplied buffer header. More... | |
Functions | |
buffer_t * | bmm_buffer_alloc (uint8_t size) |
Allocates a buffer. More... | |
void | bmm_buffer_free (buffer_t *pbuffer) |
Frees up a buffer. More... | |
__PACK__RST_DATA__ void | bmm_buffer_init (void) |
Initializes the buffer module. More... | |
Variables | |
uint8_t * | buffer_t::body |
Pointer to the buffer body. More... | |
struct buffer_tag * | buffer_t::next |
Pointer to next free buffer. More... | |
#define BMM_BUFFER_POINTER | ( | buf | ) | ((buf)->body) |
This macro provides the pointer to the corresponding body of the supplied buffer header.
Referenced by build_null_data_frame(), dispatch_event(), find_buffer_cb(), gen_mlme_poll_conf(), gen_mlme_start_conf(), gen_rx_enable_conf(), handle_exp_persistence_timer(), handle_gts_data_req(), handle_received_frame_irq(), mac_awake_disassociate(), mac_awake_scan(), mac_build_and_tx_beacon(), mac_build_and_tx_data_req(), mac_gen_mcps_data_conf(), mac_gen_mlme_associate_conf(), mac_gen_mlme_disassociate_conf(), mac_gen_mlme_gts_conf(), mac_gts_table_update(), mac_handle_tx_null_data_frame(), mac_mlme_comm_status(), mac_prep_disassoc_conf(), mac_process_associate_request(), mac_process_beacon_frame(), mac_process_data_frame(), mac_process_data_request(), mac_process_disassociate_notification(), mac_process_gts_request(), mac_process_orphan_notification(), mac_process_orphan_realign(), mac_process_tal_data_ind(), mac_process_tal_tx_status(), mac_send_gts_ind(), mac_t_scan_duration_cb(), mac_tx_coord_realignment_command(), mac_tx_gts_data(), mac_tx_pending_bc_data(), mcps_data_conf(), mcps_data_ind(), mcps_data_request(), mcps_purge_conf(), mcps_purge_request(), mlme_associate_conf(), mlme_associate_ind(), mlme_associate_request(), mlme_associate_response(), mlme_beacon_notify_ind(), mlme_comm_status_ind(), mlme_disassociate_conf(), mlme_disassociate_ind(), mlme_disassociate_request(), mlme_get_conf(), mlme_get_request(), mlme_gts_conf(), mlme_gts_ind(), mlme_gts_request(), mlme_orphan_ind(), mlme_poll_conf(), mlme_poll_request(), mlme_reset_conf(), mlme_reset_request(), mlme_rx_enable_conf(), mlme_rx_enable_request(), mlme_scan_conf(), mlme_scan_request(), mlme_set_conf(), mlme_set_request(), mlme_start_conf(), mlme_start_request(), mlme_sync_loss_ind(), mlme_sync_request(), parse_mpdu(), process_deallocate_data_q(), process_incoming_frame(), scan_proceed(), send_reset_conf(), send_scan_cmd(), tal_ed_end_cb(), tx_pan_id_conf_notif(), wpan_mcps_data_req(), wpan_mcps_purge_req(), wpan_mlme_associate_req(), wpan_mlme_associate_resp(), wpan_mlme_disassociate_req(), wpan_mlme_get_req(), wpan_mlme_gts_req(), wpan_mlme_orphan_resp(), wpan_mlme_poll_req(), wpan_mlme_reset_req(), wpan_mlme_rx_enable_req(), wpan_mlme_scan_req(), wpan_mlme_set_req(), wpan_mlme_start_req(), and wpan_mlme_sync_req().
buffer_t* bmm_buffer_alloc | ( | uint8_t | size | ) |
Allocates a buffer.
This function allocates a buffer and returns a pointer to the buffer. The same pointer should be used while freeing the buffer.User should call BMM_BUFFER_POINTER(buf) to get the pointer to buffer user area.
size | size of buffer to be allocated. |
References LARGE_BUFFER_SIZE, qmm_queue_remove(), and SMALL_BUFFER_SIZE.
Referenced by build_null_data_frame(), handle_received_frame_irq(), mac_awake_scan(), mac_build_and_tx_data_req(), mac_gts_table_update(), mac_send_gts_ind(), parse_mpdu(), tal_init(), tal_task(), tx_pan_id_conf_notif(), wpan_mcps_data_req(), wpan_mcps_purge_req(), wpan_mlme_associate_req(), wpan_mlme_associate_resp(), wpan_mlme_disassociate_req(), wpan_mlme_get_req(), wpan_mlme_gts_req(), wpan_mlme_orphan_resp(), wpan_mlme_poll_req(), wpan_mlme_reset_req(), wpan_mlme_rx_enable_req(), wpan_mlme_scan_req(), wpan_mlme_set_req(), wpan_mlme_start_req(), and wpan_mlme_sync_req().
void bmm_buffer_free | ( | buffer_t * | pbuffer | ) |
Frees up a buffer.
This function frees up a buffer. The pointer passed to this function should be the pointer returned during buffer allocation. The result is unpredictable if an incorrect pointer is passed.
pbuffer | Pointer to buffer that has to be freed. |
References qmm_queue_append().
Referenced by dispatch_event(), mac_awake_scan(), mac_buffer_purge(), mac_build_and_tx_data_req(), mac_handle_tx_null_data_frame(), mac_process_associate_request(), mac_process_associate_response(), mac_process_beacon_frame(), mac_process_beacon_request(), mac_process_coord_realign(), mac_process_data_frame(), mac_process_data_request(), mac_process_gts_request(), mac_process_orphan_realign(), mac_process_tal_data_ind(), mac_process_tal_tx_status(), mcps_data_conf(), mcps_data_ind(), mcps_purge_conf(), mlme_associate_conf(), mlme_associate_ind(), mlme_associate_response(), mlme_beacon_notify_ind(), mlme_comm_status_ind(), mlme_disassociate_conf(), mlme_disassociate_ind(), mlme_get_conf(), mlme_gts_conf(), mlme_gts_ind(), mlme_orphan_ind(), mlme_poll_conf(), mlme_reset_conf(), mlme_rx_enable_conf(), mlme_scan_conf(), mlme_set_conf(), mlme_start_conf(), mlme_sync_request(), process_data_ind_not_transient(), qmm_queue_flush(), scan_proceed(), tal_reset(), tx_pan_id_conf_notif(), wpan_mcps_data_req(), wpan_mcps_purge_req(), wpan_mlme_associate_req(), wpan_mlme_associate_resp(), wpan_mlme_disassociate_req(), wpan_mlme_get_req(), wpan_mlme_gts_req(), wpan_mlme_orphan_resp(), wpan_mlme_poll_req(), wpan_mlme_reset_req(), wpan_mlme_rx_enable_req(), wpan_mlme_scan_req(), wpan_mlme_set_req(), wpan_mlme_start_req(), and wpan_mlme_sync_req().
__PACK__RST_DATA__ void bmm_buffer_init | ( | void | ) |
Initializes the buffer module.
This function initializes the buffer module. This function should be called before using any other functionality of buffer module.
References buffer_t::body, buf_pool, LARGE_BUFFER_SIZE, qmm_queue_append(), qmm_queue_init(), SMALL_BUFFER_SIZE, TOTAL_NUMBER_OF_LARGE_BUFS, and TOTAL_NUMBER_OF_SMALL_BUFS.
Referenced by tal_init().
uint8_t* buffer_t::body |
Pointer to the buffer body.
Referenced by bmm_buffer_init(), mac_sync_loss(), and queue_read_or_remove().
struct buffer_tag* buffer_t::next |
Pointer to next free buffer.
Referenced by qmm_queue_append(), and queue_read_or_remove().