This module describes all MAC Confirmation Callback's.
Functions | |
void | usr_mcps_data_conf (uint8_t msduHandle, uint8_t status, uint32_t Timestamp) |
Callback function that must be implemented by application (NHLE) for MAC service MCPS-DATA.confirm. More... | |
void | usr_mcps_purge_conf (uint8_t msduHandle, uint8_t status) |
Callback function that must be implemented by application (NHLE) for MAC service MCPS-PURGE.confirm. More... | |
void | usr_mlme_associate_conf (uint16_t AssocShortAddress, uint8_t status) |
Callback function that must be implemented by application (NHLE) for MAC service MLME-ASSOCIATE.confirm. More... | |
void | usr_mlme_disassociate_conf (uint8_t status, wpan_addr_spec_t *DeviceAddrSpec) |
Callback function that must be implemented by application (NHLE) for MAC service MLME-DISASSOCIATE.confirm. More... | |
void | usr_mlme_get_conf (uint8_t status, uint8_t PIBAttribute, void *PIBAttributeValue) |
Callback function that must be implemented by application (NHLE) for MAC service MLME-GET.confirm. More... | |
void | usr_mlme_poll_conf (uint8_t status) |
Callback function that must be implemented by application (NHLE) for MAC service MLME-POLL.confirm. More... | |
void | usr_mlme_reset_conf (uint8_t status) |
Callback function that must be implemented by application (NHLE) for MAC service MLME-RESET.confirm. More... | |
void | usr_mlme_rx_enable_conf (uint8_t status) |
Callback function that must be implemented by application (NHLE) for MAC service MLME-RX-ENABLE.confirm. More... | |
void | usr_mlme_scan_conf (uint8_t status, uint8_t ScanType, uint8_t ChannelPage, uint32_t UnscannedChannels, uint8_t ResultListSize, void *ResultList) |
Callback function that must be implemented by application (NHLE) for MAC service MLME-SCAN.confirm. More... | |
void | usr_mlme_set_conf (uint8_t status, uint8_t PIBAttribute) |
Callback function that must be implemented by application (NHLE) for MAC service MLME-SET.confirm. More... | |
void | usr_mlme_start_conf (uint8_t status) |
Callback function that must be implemented by application (NHLE) for MAC service MLME-START.confirm. More... | |
void usr_mcps_data_conf | ( | uint8_t | msduHandle, |
uint8_t | status, | ||
uint32_t | Timestamp | ||
) |
Callback function that must be implemented by application (NHLE) for MAC service MCPS-DATA.confirm.
msduHandle | Handle of MSDU handed over to MAC earlier. |
status | Result for requested data transmission request. |
Timestamp | The time, in symbols, at which the data were transmitted; this parameter is only available if timestamping is enabled via compile switch ENABLE_TSTAMP. |
References EOT, get_next_tx_buffer(), MAC_PID, MAC_PID_LEN, MCPS_DATA_CON_LEN, and MCPS_DATA_CONFIRM.
Referenced by handle_rx_frame().
void usr_mcps_purge_conf | ( | uint8_t | msduHandle, |
uint8_t | status | ||
) |
Callback function that must be implemented by application (NHLE) for MAC service MCPS-PURGE.confirm.
msduHandle | Handle (id) of MSDU to be purged. |
status | Result of requested purge operation. |
Referenced by handle_rx_frame().
void usr_mlme_associate_conf | ( | uint16_t | AssocShortAddress, |
uint8_t | status | ||
) |
Callback function that must be implemented by application (NHLE) for MAC service MLME-ASSOCIATE.confirm.
AssocShortAddress | Short address allocated by the coordinator. |
status | Result of requested association operation. |
References EOT, get_next_tx_buffer(), MAC_PID, MAC_PID_LEN, MLME_ASSOCIATE_CONF_LEN, and MLME_ASSOCIATE_CONFIRM.
Referenced by handle_rx_frame().
void usr_mlme_disassociate_conf | ( | uint8_t | status, |
wpan_addr_spec_t * | DeviceAddrSpec | ||
) |
Callback function that must be implemented by application (NHLE) for MAC service MLME-DISASSOCIATE.confirm.
status | Result of requested disassociate operation. |
DeviceAddrSpec | Pointer to wpan_addr_spec_t structure for device that has either requested disassociation or been instructed to disassociate by its coordinator. |
References wpan_addr_spec_tag::Addr, wpan_addr_spec_tag::AddrMode, EOT, get_next_tx_buffer(), MAC_PID, MAC_PID_LEN, MLME_DISASSOCIATE_CONF_LEN, MLME_DISASSOCIATE_CONFIRM, and wpan_addr_spec_tag::PANId.
Referenced by handle_rx_frame().
void usr_mlme_get_conf | ( | uint8_t | status, |
uint8_t | PIBAttribute, | ||
void * | PIBAttributeValue | ||
) |
Callback function that must be implemented by application (NHLE) for MAC service MLME-GET.confirm.
status | Result of requested PIB attribute get operation. |
PIBAttribute | Retrieved PIB attribute. |
PIBAttributeIndex | Index of the PIB attribute to be read. |
PIBAttributeValue | Pointer to data containing retrieved PIB attribute, |
References EOT, get_next_tx_buffer(), mac_get_pib_attribute_size(), MAC_PID, MAC_PID_LEN, macBeaconTxTime, macMaxFrameTotalWaitTime, macResponseWaitTime, macTransactionPersistenceTime, MLME_GET_CONF_LEN, and MLME_GET_CONFIRM.
Referenced by handle_rx_frame().
void usr_mlme_poll_conf | ( | uint8_t | status | ) |
Callback function that must be implemented by application (NHLE) for MAC service MLME-POLL.confirm.
status | Result of requested poll operation. |
References EOT, get_next_tx_buffer(), MAC_PID, MAC_PID_LEN, MLME_POLL_CONF_LEN, and MLME_POLL_CONFIRM.
Referenced by handle_rx_frame().
void usr_mlme_reset_conf | ( | uint8_t | status | ) |
Callback function that must be implemented by application (NHLE) for MAC service MLME-RESET.confirm.
status | Result of requested reset operation. |
References EOT, get_next_tx_buffer(), MAC_PID, MAC_PID_LEN, MLME_RESET_CONF_LEN, and MLME_RESET_CONFIRM.
Referenced by handle_rx_frame().
void usr_mlme_rx_enable_conf | ( | uint8_t | status | ) |
Callback function that must be implemented by application (NHLE) for MAC service MLME-RX-ENABLE.confirm.
status | Result of requested receiver enable operation. |
References EOT, get_next_tx_buffer(), MAC_PID, MAC_PID_LEN, MLME_RX_ENABLE_CONF_LEN, and MLME_RX_ENABLE_CONFIRM.
Referenced by handle_rx_frame().
void usr_mlme_scan_conf | ( | uint8_t | status, |
uint8_t | ScanType, | ||
uint8_t | ChannelPage, | ||
uint32_t | UnscannedChannels, | ||
uint8_t | ResultListSize, | ||
void * | ResultList | ||
) |
Callback function that must be implemented by application (NHLE) for MAC service MLME-SCAN.confirm.
status | Result of requested scan operation. |
ScanType | Type of scan performed. |
ChannelPage | The channel page on which the scan was performed. |
UnscannedChannels | Bitmap of unscanned channels |
ResultListSize | Number of elements in ResultList. |
ResultList | Pointer to array of scan results . |
References wpan_addr_spec_tag::AddrMode, wpan_pandescriptor_tag::ChannelPage, wpan_pandescriptor_tag::CoordAddrSpec, EOT, get_next_tx_buffer(), wpan_pandescriptor_tag::GTSPermit, wpan_pandescriptor_tag::LinkQuality, wpan_pandescriptor_tag::LogicalChannel, MAC_PID, MAC_PID_LEN, MLME_SCAN_CONF_LEN, MLME_SCAN_CONFIRM, MLME_SCAN_TYPE_ACTIVE, MLME_SCAN_TYPE_ED, MLME_SCAN_TYPE_PASSIVE, wpan_addr_spec_tag::PANId, wpan_pandescriptor_tag::SuperframeSpec, wpan_pandescriptor_tag::TimeStamp, and WPAN_DESCRIPTOR_LEN.
Referenced by handle_rx_frame().
void usr_mlme_set_conf | ( | uint8_t | status, |
uint8_t | PIBAttribute | ||
) |
Callback function that must be implemented by application (NHLE) for MAC service MLME-SET.confirm.
status | Result of requested PIB attribute set operation. |
PIBAttribute | Updated PIB attribute. |
PIBAttributeIndex | Index of updated PIB attribute. |
References EOT, get_next_tx_buffer(), MAC_PID, MAC_PID_LEN, MLME_SET_CONF_LEN, and MLME_SET_CONFIRM.
Referenced by handle_rx_frame().
void usr_mlme_start_conf | ( | uint8_t | status | ) |
Callback function that must be implemented by application (NHLE) for MAC service MLME-START.confirm.
status | Result of requested start operation. |
Referenced by handle_rx_frame().