Low-level crypto API for an AES unit implemented in AT86RFA1.
Copyright (c) 2013-2018 Microchip Technology Inc. and its subsidiaries.
Macros | |
#define | _SR_MASK(addr, mask, pos, val) (((uint8_t)val << pos) & mask) |
#define | _trx_bit_read(addr, mask, pos) (((*(volatile uint8_t *)(addr)) & (mask)) >> (pos)) |
#define | AES_COMPLETED (1) |
Constant AES_COMPLETED for sub-register SR_AES_DONE in register AES_STATUS. More... | |
#define | AES_DIR_DECRYPT (1) |
Constant AES_DIR_DECRYPT for sub-register SR_AES_DIR in register AES_CTRL. More... | |
#define | AES_DIR_ENCRYPT (0) |
Constant AES_DIR_ENCRYPT for sub-register SR_AES_DIR in register AES_CTRL. More... | |
#define | AES_DIR_VOID (AES_DIR_ENCRYPT + AES_DIR_DECRYPT + 1) |
#define | AES_NOT_COMPLETED (0) |
Constant AES_NOT_COMPLETED for sub-register SR_AES_DONE in register AES_STATUS. More... | |
#define | AES_START (1) |
Constant AES_START for sub-register SR_AES_REQUEST in register AES_CTRL. More... | |
#define | AES_START (1) |
Constant AES_START for sub-register SR_AES_REQUEST in register AES_CTRL. More... | |
#define | RG_AES_CTRL (0x13C) |
Offset for register AES_CTRL. More... | |
#define | RG_AES_KEY (0x13F) |
Offset for register AES_KEY. More... | |
#define | RG_AES_STATE (0x13E) |
Offset for register AES_STATE. More... | |
#define | RG_AES_STATUS (0x13D) |
Offset for register AES_STATUS. More... | |
#define | RG_TRX_STATUS (0x141) |
Offset for register TRX_STATUS. More... | |
#define | SR_AES_DIR 0x13C, 0x08, 3 |
Access parameters for sub-register AES_DIR in register RG_AES_CTRL. More... | |
#define | SR_AES_DONE 0x13D, 0x01, 0 |
Sub-registers of Register RG_AES_STATUS. More... | |
#define | SR_AES_ER 0x13D, 0x80, 7 |
Access parameters for sub-register AES_ER in register RG_AES_STATUS. More... | |
#define | SR_AES_IM 0x13C, 0x04, 2 |
Sub-registers of Register RG_AES_CTRL. More... | |
#define | SR_AES_MODE 0x13C, 0x20, 5 |
Access parameters for sub-register AES_MODE in register RG_AES_CTRL. More... | |
#define | SR_AES_REQUEST 0x13C, 0x80, 7 |
Access parameters for sub-register AES_REQUEST in register RG_AES_CTRL. More... | |
#define | SR_MASK(SR, val) _SR_MASK(SR, val) |
#define | trx_bit_read(arg) _trx_bit_read(arg) |
Subregister read. More... | |
#define | trx_reg_read(addr) (*(volatile uint8_t *)(addr)) |
Reads current value from a transceiver register. More... | |
#define | trx_reg_write(addr, data) (*(volatile uint8_t *)(addr)) = (data) |
Writes data into a transceiver register. More... | |
Functions | |
void | _sal_aes_clean_up (void) |
Cleans up the SAL/AES after STB has been finished. More... | |
void | sal_aes_exec (uint8_t *data) |
En/decrypt one AES block. More... | |
void | sal_aes_read (uint8_t *data) |
Reads the result of previous AES en/decryption. More... | |
void | sal_aes_restart (void) |
Re-inits key and state after a sleep or TRX reset. More... | |
bool | sal_aes_setup (uint8_t *key, uint8_t enc_mode, uint8_t dir) |
Setup AES unit. More... | |
void | sal_init (void) |
Initialization of SAL. More... | |
Variables | |
static bool | dec_initialized = false |
static uint8_t | dec_key [AES_KEYSIZE] |
static uint8_t | enc_key [AES_KEYSIZE] |
static uint8_t | last_dir = AES_DIR_VOID |
static uint8_t | mode_byte |
#define _SR_MASK | ( | addr, | |
mask, | |||
pos, | |||
val | |||
) | (((uint8_t)val << pos) & mask) |
#define _trx_bit_read | ( | addr, | |
mask, | |||
pos | |||
) | (((*(volatile uint8_t *)(addr)) & (mask)) >> (pos)) |
#define AES_COMPLETED (1) |
Constant AES_COMPLETED for sub-register SR_AES_DONE in register AES_STATUS.
#define AES_DIR_DECRYPT (1) |
Constant AES_DIR_DECRYPT for sub-register SR_AES_DIR in register AES_CTRL.
Referenced by sal_aes_setup().
#define AES_DIR_ENCRYPT (0) |
Constant AES_DIR_ENCRYPT for sub-register SR_AES_DIR in register AES_CTRL.
Referenced by compute_mic(), encrypt_pldmic(), sal_aes_restart(), sal_aes_setup(), and stb_ccm_secure().
#define AES_DIR_VOID (AES_DIR_ENCRYPT + AES_DIR_DECRYPT + 1) |
Referenced by sal_aes_setup().
#define AES_NOT_COMPLETED (0) |
Constant AES_NOT_COMPLETED for sub-register SR_AES_DONE in register AES_STATUS.
#define AES_START (1) |
Constant AES_START for sub-register SR_AES_REQUEST in register AES_CTRL.
Referenced by sal_aes_exec().
#define AES_START (1) |
Constant AES_START for sub-register SR_AES_REQUEST in register AES_CTRL.
#define RG_AES_CTRL (0x13C) |
Offset for register AES_CTRL.
Referenced by sal_aes_exec(), sal_aes_restart(), and sal_aes_setup().
#define RG_AES_KEY (0x13F) |
Offset for register AES_KEY.
Referenced by sal_aes_restart(), and sal_aes_setup().
#define RG_AES_STATE (0x13E) |
Offset for register AES_STATE.
Referenced by sal_aes_exec(), and sal_aes_read().
#define RG_AES_STATUS (0x13D) |
Offset for register AES_STATUS.
#define RG_TRX_STATUS (0x141) |
Offset for register TRX_STATUS.
#define SR_AES_DIR 0x13C, 0x08, 3 |
Access parameters for sub-register AES_DIR in register RG_AES_CTRL.
Referenced by sal_aes_setup().
#define SR_AES_DONE 0x13D, 0x01, 0 |
Sub-registers of Register RG_AES_STATUS.
Access parameters for sub-register AES_DONE in register RG_AES_STATUS
Referenced by sal_aes_exec().
#define SR_AES_ER 0x13D, 0x80, 7 |
Access parameters for sub-register AES_ER in register RG_AES_STATUS.
#define SR_AES_IM 0x13C, 0x04, 2 |
Sub-registers of Register RG_AES_CTRL.
Access parameters for sub-register AES_IM in register RG_AES_CTRL
#define SR_AES_MODE 0x13C, 0x20, 5 |
Access parameters for sub-register AES_MODE in register RG_AES_CTRL.
Referenced by sal_aes_setup().
#define SR_AES_REQUEST 0x13C, 0x80, 7 |
Access parameters for sub-register AES_REQUEST in register RG_AES_CTRL.
Referenced by sal_aes_exec().
#define SR_MASK | ( | SR, | |
val | |||
) | _SR_MASK(SR, val) |
Referenced by sal_aes_exec(), and sal_aes_setup().
#define trx_bit_read | ( | arg | ) | _trx_bit_read(arg) |
Subregister read.
arg | Subregister |
Referenced by handle_received_frame_irq(), handle_tx_end_irq(), perform_cca_twice(), sal_aes_exec(), set_trx_state(), switch_pll_on(), tal_ant_div_config(), tal_ext_pa_ctrl(), tal_generate_rand_seed(), tal_get_curr_trx_config(), tal_get_trx_status(), tal_rxaack_prom_mode_ctrl(), tal_rxsafe_mode_ctrl(), tal_set_frequency(), tal_set_frequency_regs(), tal_set_rx_sensitivity_level(), tal_set_tx_pwr(), trx_init(), and trx_reset().
#define trx_reg_read | ( | addr | ) | (*(volatile uint8_t *)(addr)) |
Reads current value from a transceiver register.
This macro reads the current value from a transceiver register.
addr | Specifies the address of the trx register from which the data shall be read |
Referenced by handle_received_frame_irq(), sal_aes_read(), sal_aes_setup(), switch_pll_on(), tal_dump_registers(), tal_get_curr_trx_config(), tal_rpc_mode_config(), tal_set_frequency(), tal_set_frequency_regs(), tal_trx_reg_read(), tal_trx_reg_write(), and trx_init().
Writes data into a transceiver register.
This macro writes a value into transceiver register.
addr | Address of the trx register |
data | Data to be written to trx register |
Referenced by perform_cca_twice(), sal_aes_exec(), sal_aes_restart(), sal_aes_setup(), send_frame(), set_trx_state(), switch_pll_on(), tal_generate_rand_seed(), tal_pib_set(), tal_rpc_mode_config(), tal_set_frequency(), tal_set_frequency_regs(), tal_trx_reg_write(), trx_config(), and write_all_tal_pib_to_trx().
void _sal_aes_clean_up | ( | void | ) |
Cleans up the SAL/AES after STB has been finished.
Cleans up the SAL/AES after STB has been completed.
void sal_aes_exec | ( | uint8_t * | data | ) |
En/decrypt one AES block.
The function returns after the AES operation is finished.
[in] | data | AES block to be en/decrypted |
References AES_BLOCKSIZE, AES_START, mode_byte, RG_AES_CTRL, RG_AES_STATE, SR_AES_DONE, SR_AES_REQUEST, SR_MASK, trx_bit_read, and trx_reg_write.
Referenced by compute_mic(), encrypt_pldmic(), encrypt_with_padding(), and sal_aes_setup().
void sal_aes_read | ( | uint8_t * | data | ) |
Reads the result of previous AES en/decryption.
This function returns the result of the previous AES operation, so this function is needed in order to get the last result of a series of sal_aes_wrrd() calls.
[out] | data | - result of previous operation |
References AES_BLOCKSIZE, RG_AES_STATE, and trx_reg_read.
Referenced by compute_mic(), and encrypt_pldmic().
void sal_aes_restart | ( | void | ) |
Re-inits key and state after a sleep or TRX reset.
This function re-initializes the AES key and the state of the AES engine after TRX sleep or reset. The contents of AES register AES_CON is restored, the next AES operation started with sal_aes_exec() will be executed correctly.
References AES_BLOCKSIZE, AES_DIR_ENCRYPT, dec_key, enc_key, last_dir, mode_byte, RG_AES_CTRL, RG_AES_KEY, and trx_reg_write.
Referenced by stb_ccm_secure().
bool sal_aes_setup | ( | uint8_t * | key, |
uint8_t | enc_mode, | ||
uint8_t | dir | ||
) |
Setup AES unit.
This function perform the following tasks as part of the setup of the AES unit: key initialization, set encryption direction and encryption mode.
In general, the contents of SRAM buffer is destroyed. When using sal_aes_wrrd(), sal_aes_read() needs to be called in order to get the result of the last AES operation before you may call sal_aes_setup() again.
[in] | key | AES key or NULL (NULL: use last key) |
[in] | enc_mode | AES_MODE_ECB or AES_MODE_CBC |
[in] | dir | AES_DIR_ENCRYPT or AES_DIR_DECRYPT |
References AES_BLOCKSIZE, AES_DIR_DECRYPT, AES_DIR_ENCRYPT, AES_DIR_VOID, AES_KEYSIZE, AES_MODE_CBC, AES_MODE_ECB, dec_initialized, dec_key, enc_key, last_dir, mode_byte, RG_AES_CTRL, RG_AES_KEY, sal_aes_exec(), SR_AES_DIR, SR_AES_MODE, SR_MASK, trx_reg_read, and trx_reg_write.
Referenced by compute_mic(), encrypt_pldmic(), and stb_ccm_secure().
void sal_init | ( | void | ) |
|
static |
Referenced by sal_aes_setup().
|
static |
Referenced by sal_aes_restart(), and sal_aes_setup().
|
static |
Referenced by sal_aes_restart(), and sal_aes_setup().
|
static |
Referenced by sal_aes_restart(), and sal_aes_setup().
|
static |
Referenced by sal_aes_exec(), sal_aes_restart(), and sal_aes_setup().