This file handles the interrupts generated by the transceiver.
Copyright (c) 2013-2018 Microchip Technology Inc. and its subsidiaries.
#include <stdint.h>
#include <stdbool.h>
#include <stddef.h>
#include "return_val.h"
#include "tal.h"
#include "ieee_const.h"
#include "stack_config.h"
#include "bmm.h"
#include "qmm.h"
#include "tal_irq_handler.h"
#include "tal_rx.h"
#include "atmega256rfr2.h"
#include "tal_internal.h"
#include "tal_constants.h"
#include "tal_tx.h"
#include "mac_build_config.h"
Macros | |
#define | CONCAT(a, b) a ## b |
String concatenation by preprocessor used to create proper register names. More... | |
#define | PAL_US_PER_SYMBOLS (16) |
Conversion factor: us per symbol for 2,4 GHz. More... | |
#define | SC_READ32(reg) |
Creates proper subregister names and reads the corresponding values. More... | |
#define | SC_WRITE32(reg, val) |
Creates proper subregister names and writes the corresponding values. More... | |
Functions | |
ISR (TRX24_TX_END_vect) | |
ISR for transceiver's transmit end interrupt. More... | |
ISR (TRX24_RX_END_vect) | |
ISR for transceiver's receive end interrupt. More... | |
ISR (TRX24_CCA_ED_DONE_vect) | |
ISR for transceiver's CCA/ED measurement done interrupt. More... | |
ISR (TRX24_AWAKE_vect) | |
ISR for transceiver's Awake interrupt. More... | |
ISR (TRX24_RX_START_vect) | |
ISR for transceiver's rx start interrupt. More... | |
ISR (TRX24_PLL_LOCK_vect) | |
ISR for transceiver's PLL lock interrupt. More... | |
ISR (TRX24_PLL_UNLOCK_vect) | |
ISR for transceiver's PLL unlock interrupt. More... | |
ISR (TRX24_XAH_AMI_vect) | |
ISR for transceiver's address match interrupt. More... | |
ISR (BAT_LOW_vect) | |
ISR for transceiver's battery low interrupt. More... | |
ISR (AES_READY_vect) | |
ISR for transceiver's AES interrupt. More... | |
ISR (TRX24_TX_START_vect) | |
ISR for transceiver's TX_START interrupt. More... | |
ISR (TRX24_AMI0_vect) | |
ISR for transceiver's AMI0 interrupt. More... | |
ISR (TRX24_AMI1_vect) | |
ISR for transceiver's AMI1 interrupt. More... | |
ISR (TRX24_AMI2_vect) | |
ISR for transceiver's AMI2 interrupt. More... | |
ISR (TRX24_AMI3_vect) | |
ISR for transceiver's AMI3 interrupt. More... | |
void | pal_trx_irq_init_aes_ready (FUNC_PTR trx_irq_cb) |
void | pal_trx_irq_init_ami (FUNC_PTR trx_irq_cb) |
void | pal_trx_irq_init_awake (FUNC_PTR trx_irq_cb) |
Initializes the transceiver AWAKE interrupt. More... | |
void | pal_trx_irq_init_batmon (FUNC_PTR trx_irq_cb) |
void | pal_trx_irq_init_cca_ed (FUNC_PTR trx_irq_cb) |
Initializes the transceiver CCA ED END interrupt. More... | |
void | pal_trx_irq_init_maf_0_ami (FUNC_PTR trx_irq_cb) |
void | pal_trx_irq_init_maf_1_ami (FUNC_PTR trx_irq_cb) |
void | pal_trx_irq_init_maf_2_ami (FUNC_PTR trx_irq_cb) |
void | pal_trx_irq_init_maf_3_ami (FUNC_PTR trx_irq_cb) |
void | pal_trx_irq_init_pll_lock (FUNC_PTR trx_irq_cb) |
void | pal_trx_irq_init_pll_unlock (FUNC_PTR trx_irq_cb) |
void | pal_trx_irq_init_rx_end (FUNC_PTR trx_irq_cb) |
Initializes the transceiver RX END interrupt. More... | |
void | pal_trx_irq_init_tstamp (FUNC_PTR trx_irq_cb) |
Initializes the transceiver timestamp interrupt. More... | |
void | pal_trx_irq_init_tx_end (FUNC_PTR trx_irq_cb) |
Initializes the transceiver TX END interrupt. More... | |
void | pal_trx_irq_init_tx_start (FUNC_PTR trx_irq_cb) |
static uint32_t | sc_read32 (volatile uint8_t *hh, volatile uint8_t *hl, volatile uint8_t *lh, volatile uint8_t *ll) |
Reads the 32-bit timer register in the required order of bytes. More... | |
void | trx_awake_handler_cb (void) |
void | trx_irq_timestamp_handler_cb (void) |
Timestamp interrupt handler. More... | |
void | trx_rx_end_handler_cb (void) |
Transceiver interrupt handler. More... | |
void | trx_tx_end_handler_cb (void) |
Transceiver interrupt handler. More... | |
Variables | |
static irq_handler_t | irq_hdl_trx_aes_ready |
Function pointer to store callback for transceiver AES_READY interrupt. More... | |
static irq_handler_t | irq_hdl_trx_ami |
Function pointer to store callback for transceiver AMI interrupt. More... | |
static irq_handler_t | irq_hdl_trx_ami0 |
Function pointer to store callback for transceiver AMI0 interrupt. More... | |
static irq_handler_t | irq_hdl_trx_ami1 |
Function pointer to store callback for transceiver AMI1 interrupt. More... | |
static irq_handler_t | irq_hdl_trx_ami2 |
Function pointer to store callback for transceiver AMI2 interrupt. More... | |
static irq_handler_t | irq_hdl_trx_ami3 |
Function pointer to store callback for transceiver AMI3 interrupt. More... | |
static irq_handler_t | irq_hdl_trx_awake |
Function pointer to store callback for transceiver AWAKE interrupt. More... | |
static irq_handler_t | irq_hdl_trx_batmon |
Function pointer to store callback for transceiver BATMON interrupt. More... | |
static irq_handler_t | irq_hdl_trx_cca_ed |
Function pointer to store callback for transceiver CCA_ED interrupt. More... | |
static irq_handler_t | irq_hdl_trx_pll_lock |
Function pointer to store callback for transceiver PLL_LOCK interrupt. More... | |
static irq_handler_t | irq_hdl_trx_pll_unlock |
Function pointer to store callback for transceiver PLL_UNLOCK interrupt. More... | |
static irq_handler_t | irq_hdl_trx_rx_end |
Function pointer to store callback for transceiver RX_END interrupt. More... | |
static irq_handler_t | irq_hdl_trx_tstamp |
Function pointer to store callback for transceiver timestamp (RX_START) interrupt. More... | |
static irq_handler_t | irq_hdl_trx_tx_end |
Function pointer to store callback for transceiver TX_END interrupt. More... | |
static irq_handler_t | irq_hdl_trx_tx_start |
Function pointer to store callback for transceiver TX_START interrupt. More... | |
uint32_t | pal_tx_timestamp |
Timestamp of the last frame transmission (including auto-ACK) More... | |
#define CONCAT | ( | a, | |
b | |||
) | a ## b |
String concatenation by preprocessor used to create proper register names.
#define PAL_US_PER_SYMBOLS (16) |
Conversion factor: us per symbol for 2,4 GHz.
Referenced by ISR().
#define SC_READ32 | ( | reg | ) |
Creates proper subregister names and reads the corresponding values.
Referenced by ISR().
#define SC_WRITE32 | ( | reg, | |
val | |||
) |
Creates proper subregister names and writes the corresponding values.
ISR | ( | TRX24_TX_END_vect | ) |
ISR for transceiver's transmit end interrupt.
References irq_hdl_trx_tx_end.
ISR | ( | TRX24_RX_END_vect | ) |
ISR for transceiver's receive end interrupt.
References irq_hdl_trx_rx_end.
ISR | ( | TRX24_CCA_ED_DONE_vect | ) |
ISR for transceiver's CCA/ED measurement done interrupt.
References irq_hdl_trx_cca_ed.
ISR | ( | TRX24_AWAKE_vect | ) |
ISR for transceiver's Awake interrupt.
References irq_hdl_trx_awake.
ISR | ( | TRX24_RX_START_vect | ) |
ISR for transceiver's rx start interrupt.
By the time the SFD is detected, the hardware timestamps the current frame in the SCTSR register.
References irq_hdl_trx_tstamp.
ISR | ( | TRX24_PLL_LOCK_vect | ) |
ISR for transceiver's PLL lock interrupt.
References irq_hdl_trx_pll_lock.
ISR | ( | TRX24_PLL_UNLOCK_vect | ) |
ISR for transceiver's PLL unlock interrupt.
References irq_hdl_trx_pll_unlock.
ISR | ( | TRX24_XAH_AMI_vect | ) |
ISR for transceiver's address match interrupt.
References irq_hdl_trx_ami.
ISR | ( | BAT_LOW_vect | ) |
ISR for transceiver's battery low interrupt.
References irq_hdl_trx_batmon.
ISR | ( | AES_READY_vect | ) |
ISR for transceiver's AES interrupt.
References irq_hdl_trx_aes_ready.
ISR | ( | TRX24_TX_START_vect | ) |
ISR for transceiver's TX_START interrupt.
References irq_hdl_trx_tx_start, pal_tx_timestamp, PAL_US_PER_SYMBOLS, and SC_READ32.
ISR | ( | TRX24_AMI0_vect | ) |
ISR for transceiver's AMI0 interrupt.
References irq_hdl_trx_ami0.
ISR | ( | TRX24_AMI1_vect | ) |
ISR for transceiver's AMI1 interrupt.
References irq_hdl_trx_ami1.
ISR | ( | TRX24_AMI2_vect | ) |
ISR for transceiver's AMI2 interrupt.
References irq_hdl_trx_ami2.
ISR | ( | TRX24_AMI3_vect | ) |
ISR for transceiver's AMI3 interrupt.
References irq_hdl_trx_ami3.
void pal_trx_irq_init_aes_ready | ( | FUNC_PTR | trx_irq_cb | ) |
References irq_hdl_trx_aes_ready.
void pal_trx_irq_init_ami | ( | FUNC_PTR | trx_irq_cb | ) |
References irq_hdl_trx_ami.
void pal_trx_irq_init_awake | ( | FUNC_PTR | trx_irq_cb | ) |
Initializes the transceiver AWAKE interrupt.
This function sets the microcontroller specific registers responsible for handling the transceiver AWAKE interrupt
trx_irq_cb | Callback function for the transceiver AWAKE interrupt |
References irq_hdl_trx_awake.
Referenced by set_trx_state(), and tal_init().
void pal_trx_irq_init_batmon | ( | FUNC_PTR | trx_irq_cb | ) |
References irq_hdl_trx_batmon.
void pal_trx_irq_init_cca_ed | ( | FUNC_PTR | trx_irq_cb | ) |
Initializes the transceiver CCA ED END interrupt.
This function sets the microcontroller specific registers responsible for handling the transceiver CCA ED END interrupt
trx_irq_cb | Callback function for the transceiver CCA ED END interrupt |
References irq_hdl_trx_cca_ed.
void pal_trx_irq_init_maf_0_ami | ( | FUNC_PTR | trx_irq_cb | ) |
References irq_hdl_trx_ami0.
void pal_trx_irq_init_maf_1_ami | ( | FUNC_PTR | trx_irq_cb | ) |
References irq_hdl_trx_ami1.
void pal_trx_irq_init_maf_2_ami | ( | FUNC_PTR | trx_irq_cb | ) |
References irq_hdl_trx_ami2.
void pal_trx_irq_init_maf_3_ami | ( | FUNC_PTR | trx_irq_cb | ) |
References irq_hdl_trx_ami3.
void pal_trx_irq_init_pll_lock | ( | FUNC_PTR | trx_irq_cb | ) |
References irq_hdl_trx_pll_lock.
void pal_trx_irq_init_pll_unlock | ( | FUNC_PTR | trx_irq_cb | ) |
References irq_hdl_trx_pll_unlock.
void pal_trx_irq_init_rx_end | ( | FUNC_PTR | trx_irq_cb | ) |
Initializes the transceiver RX END interrupt.
This function sets the microcontroller specific registers responsible for handling the transceiver RX END interrupt
trx_irq_cb | Callback function for the transceiver RX END interrupt |
References irq_hdl_trx_rx_end.
Referenced by tal_init().
void pal_trx_irq_init_tx_end | ( | FUNC_PTR | trx_irq_cb | ) |
Initializes the transceiver TX END interrupt.
This function sets the microcontroller specific registers responsible for handling the transceiver TX END interrupt
trx_irq_cb | Callback function for the transceiver TX END interrupt |
References irq_hdl_trx_tx_end.
Referenced by tal_init().
void pal_trx_irq_init_tx_start | ( | FUNC_PTR | trx_irq_cb | ) |
References irq_hdl_trx_tx_start.
|
inlinestatic |
Reads the 32-bit timer register in the required order of bytes.
hh | hh octet of 32-bit register |
hl | hl octet of 32-bit register |
lh | lh octet of 32-bit register |
ll | ll octet of 32-bit register |
|
static |
Function pointer to store callback for transceiver AES_READY interrupt.
Referenced by ISR(), and pal_trx_irq_init_aes_ready().
|
static |
Function pointer to store callback for transceiver AMI interrupt.
Referenced by ISR(), and pal_trx_irq_init_ami().
|
static |
Function pointer to store callback for transceiver AMI0 interrupt.
Referenced by ISR(), and pal_trx_irq_init_maf_0_ami().
|
static |
Function pointer to store callback for transceiver AMI1 interrupt.
Referenced by ISR(), and pal_trx_irq_init_maf_1_ami().
|
static |
Function pointer to store callback for transceiver AMI2 interrupt.
Referenced by ISR(), and pal_trx_irq_init_maf_2_ami().
|
static |
Function pointer to store callback for transceiver AMI3 interrupt.
Referenced by ISR(), and pal_trx_irq_init_maf_3_ami().
|
static |
Function pointer to store callback for transceiver AWAKE interrupt.
Referenced by ISR(), and pal_trx_irq_init_awake().
|
static |
Function pointer to store callback for transceiver BATMON interrupt.
Referenced by ISR(), and pal_trx_irq_init_batmon().
|
static |
Function pointer to store callback for transceiver CCA_ED interrupt.
Referenced by ISR(), and pal_trx_irq_init_cca_ed().
|
static |
Function pointer to store callback for transceiver PLL_LOCK interrupt.
Referenced by ISR(), and pal_trx_irq_init_pll_lock().
|
static |
Function pointer to store callback for transceiver PLL_UNLOCK interrupt.
Referenced by ISR(), and pal_trx_irq_init_pll_unlock().
|
static |
Function pointer to store callback for transceiver RX_END interrupt.
Referenced by ISR(), and pal_trx_irq_init_rx_end().
|
static |
Function pointer to store callback for transceiver timestamp (RX_START) interrupt.
Referenced by ISR(), and pal_trx_irq_init_tstamp().
|
static |
Function pointer to store callback for transceiver TX_END interrupt.
Referenced by ISR(), and pal_trx_irq_init_tx_end().
|
static |
Function pointer to store callback for transceiver TX_START interrupt.
Referenced by ISR(), and pal_trx_irq_init_tx_start().
uint32_t pal_tx_timestamp |
Timestamp of the last frame transmission (including auto-ACK)
Referenced by ISR(), and tx_done_handling().