|
void | AT86RFX_ISR (void) |
|
void | PhyReset (void) |
| Resets the TRX radio. More...
|
|
void | trx_aes_wrrd (uint8_t addr, uint8_t *idata, uint8_t length) |
| Writes and reads data into/from SRAM of the transceiver. More...
|
|
uint8_t | trx_bit_read (uint8_t addr, uint8_t mask, uint8_t pos) |
| Subregister read. More...
|
|
void | trx_bit_write (uint8_t reg_addr, uint8_t mask, uint8_t pos, uint8_t new_value) |
| Subregister write. More...
|
|
void | trx_frame_read (uint8_t *data, uint8_t length) |
| Reads frame buffer of the transceiver. More...
|
|
void | trx_frame_write (uint8_t *data, uint8_t length) |
| Writes data into frame buffer of the transceiver. More...
|
|
void | trx_irq_init (FUNC_PTR trx_irq_cb) |
|
uint8_t | trx_reg_read (uint8_t addr) |
| Reads current value from a transceiver register. More...
|
|
void | trx_reg_write (uint8_t addr, uint8_t data) |
| Writes data into a transceiver register. More...
|
|
void | trx_spi_disable (void) |
| Disables the SPI interface for communication with the transceiver. More...
|
|
void | trx_spi_enable (void) |
| enables the SPI interface for communication with the transceiver More...
|
|
void | trx_spi_init (void) |
| Initializes the SPI interface for communication with the transceiver. More...
|
|
void | trx_sram_read (uint8_t addr, uint8_t *data, uint8_t length) |
| Reads data from SRAM of the transceiver. More...
|
|
void | trx_sram_write (uint8_t addr, uint8_t *data, uint8_t length) |
| Writes data into SRAM of the transceiver. More...
|
|