Microchip® Advanced Software Framework

sal.c File Reference

Low-level crypto API for an AES unit implemented in AT86RF2xx.

Copyright (c) 2013-2018 Microchip Technology Inc. and its subsidiaries.

#include "trx_access.h"
#include "sal_types.h"
#include <string.h>
#include "sal.h"
#include "delay.h"

Macros

#define _SR_MASK(addr, mask, pos, val)   (((uint8_t)val << pos) & mask)
 
#define AES_DIR_VOID   (AES_DIR_ENCRYPT + AES_DIR_DECRYPT + 1)
 
#define AES_RY_BIT   (1) /* AES_RY: poll on finished op */
 
#define SR_MASK(SR, val)   _SR_MASK(SR, val)
 

Functions

void _sal_aes_clean_up (void)
 Cleans up the SAL/AES after STB has been finished. More...
 
void sal_aes_read (uint8_t *data)
 Reads the result of previous AES en/decryption. More...
 
void sal_aes_restart (void)
 Re-inits key and state after a sleep or TRX reset. More...
 
bool sal_aes_setup (uint8_t *key, uint8_t enc_mode, uint8_t dir)
 Setup AES unit. More...
 
void sal_aes_wrrd (uint8_t *idata, uint8_t *odata)
 Writes data, reads previous result and does the AES en/decryption. More...
 
void sal_init (void)
 Initialization of SAL. More...
 

Variables

static uint8_t aes_buf [AES_BLOCKSIZE+2]
 
static bool dec_initialized = false
 
static uint8_t dec_key [AES_KEYSIZE]
 
static uint8_t enc_key [AES_KEYSIZE]
 
static uint8_t last_dir = AES_DIR_VOID
 
static bool setup_flag
 

#define _SR_MASK (   addr,
  mask,
  pos,
  val 
)    (((uint8_t)val << pos) & mask)
#define AES_DIR_VOID   (AES_DIR_ENCRYPT + AES_DIR_DECRYPT + 1)

Referenced by sal_aes_setup().

#define AES_RY_BIT   (1) /* AES_RY: poll on finished op */
Author
Microchip Technology Inc: http://www.microchip.com Support: https://www.microchip.com/support/
#define SR_MASK (   SR,
  val 
)    _SR_MASK(SR, val)

Referenced by sal_aes_restart(), and sal_aes_setup().

void _sal_aes_clean_up ( void  )

Cleans up the SAL/AES after STB has been finished.

Cleans up the SAL/AES after STB has been completed.

void sal_aes_read ( uint8_t *  data)

Reads the result of previous AES en/decryption.

This function returns the result of the previous AES operation, so this function is needed in order to get the last result of a series of sal_aes_wrrd() calls.

Parameters
[out]data- result of previous operation

References AES_BASE_ADDR, AES_BLOCKSIZE, RG_AES_STATE_KEY_0, and trx_sram_read().

Referenced by compute_mic(), and encrypt_pldmic().

void sal_aes_restart ( void  )

Re-inits key and state after a sleep or TRX reset.

This function re-initializes the AES key and the state of the AES engine after TRX sleep or reset. The contents of AES registers AES_CON and AES_CON_MIRROR are restored, the next AES operation started with sal_aes_wrrd() will be executed correctly. However, the contents of SRAM buffers is destroyed, in general. When using sal_aes_wrrd(), call sal_aes_read() to get the result of the last AES operation BEFORE you put the transceiver unit to sleep state!

References AES_BASE_ADDR, AES_BLOCKSIZE, aes_buf, AES_DIR_ENCRYPT, AES_KEYSIZE, AES_MODE_KEY, dec_key, enc_key, last_dir, RG_AES_CTRL, setup_flag, SR_AES_MODE, SR_MASK, and trx_sram_write().

Referenced by stb_ccm_secure().

bool sal_aes_setup ( uint8_t *  key,
uint8_t  enc_mode,
uint8_t  dir 
)

Setup AES unit.

This function perform the following tasks as part of the setup of the AES unit: key initialization, set encryption direction and encryption mode.

In general, the contents of SRAM buffer is destroyed. When using sal_aes_wrrd(), sal_aes_read() needs to be called in order to get the result of the last AES operation before you may call sal_aes_setup() again.

Parameters
[in]keyAES key or NULL (NULL: use last key)
[in]enc_modeAES_MODE_ECB or AES_MODE_CBC
[in]dirAES_DIR_ENCRYPT or AES_DIR_DECRYPT
Returns
False if some parameter was illegal, true else

References AES_BASE_ADDR, AES_BLOCKSIZE, aes_buf, AES_DIR_DECRYPT, AES_DIR_ENCRYPT, AES_DIR_VOID, AES_KEYSIZE, AES_MODE_CBC, AES_MODE_ECB, AES_MODE_KEY, AES_REQUEST, dec_initialized, dec_key, enc_key, last_dir, RG_AES_CTRL, RG_AES_STATE_KEY_0, sal_aes_wrrd(), setup_flag, SR_AES_DIR, SR_AES_MODE, SR_AES_REQUEST, SR_MASK, trx_sram_read(), and trx_sram_write().

Referenced by compute_mic(), encrypt_pldmic(), and stb_ccm_secure().

void sal_aes_wrrd ( uint8_t *  idata,
uint8_t *  odata 
)

Writes data, reads previous result and does the AES en/decryption.

The function returns after the AES operation is finished.

When sal_aes_wrrd() is called several times in sequence, from the second call onwards, odata contains the result of the previous operation. To obtain the last result, you must call sal_aes_read() at the end. Please note that any call of sal_aes_setup() as well as putting the transceiver to sleep state destroys the SRAM contents, i.e. the next call of sal_aes_wrrd() yields no meaningful result.

Parameters
[in]idataAES block to be en/decrypted
[out]odataResult of previous operation (odata may be NULL or equal to idata)

References AES_BASE_ADDR, AES_BLOCKSIZE, aes_buf, delay_us, RG_AES_CTRL, RG_AES_STATE_KEY_0, setup_flag, and trx_aes_wrrd().

Referenced by compute_mic(), encrypt_pldmic(), encrypt_with_padding(), and sal_aes_setup().

void sal_init ( void  )

Initialization of SAL.

This functions initializes the SAL.

Referenced by stb_init().

uint8_t aes_buf[AES_BLOCKSIZE+2]
static
bool dec_initialized = false
static

Referenced by sal_aes_setup().

uint8_t dec_key[AES_KEYSIZE]
static

Referenced by sal_aes_restart(), and sal_aes_setup().

uint8_t enc_key[AES_KEYSIZE]
static

Referenced by sal_aes_restart(), and sal_aes_setup().

uint8_t last_dir = AES_DIR_VOID
static

Referenced by sal_aes_restart(), and sal_aes_setup().

bool setup_flag
static