This module describes all MAC Indication Callback's.
Functions | |
void | usr_mcps_data_ind (wpan_addr_spec_t *SrcAddrSpec, wpan_addr_spec_t *DstAddrSpec, uint8_t msduLength, uint8_t *msdu, uint8_t mpduLinkQuality, uint8_t DSN, uint32_t Timestamp, uint8_t SecurityLevel, uint8_t KeyIdMode, uint8_t KeyIndex) |
Callback function that must be implemented by application (NHLE) for MAC service MCPS-DATA.indication. More... | |
void | usr_mlme_associate_ind (uint64_t DeviceAddress, uint8_t CapabilityInformation) |
Callback function that must be implemented by application (NHLE) for MAC service MLME-ASSOCIATE.indication. More... | |
void | usr_mlme_beacon_notify_ind (uint8_t BSN, wpan_pandescriptor_t *PANDescriptor, uint8_t PendAddrSpec, uint8_t *AddrList, uint8_t sduLength, uint8_t *sdu) |
Callback function that must be implemented by application (NHLE) for MAC service MLME-BEACON-NOTIFY.indication. More... | |
void | usr_mlme_comm_status_ind (wpan_addr_spec_t *SrcAddrSpec, wpan_addr_spec_t *DstAddrSpec, uint8_t status) |
Callback function that must be implemented by application (NHLE) for MAC service MLME-COMM-STATUS.indication. More... | |
void | usr_mlme_disassociate_ind (uint64_t DeviceAddress, uint8_t DisassociateReason) |
Callback function that must be implemented by application (NHLE) for MAC service MLME-DISASSOCIATE.indication. More... | |
void | usr_mlme_orphan_ind (uint64_t OrphanAddress) |
Callback function that must be implemented by application (NHLE) for MAC service MLME-ORPHAN.indication. More... | |
void | usr_mlme_sync_loss_ind (uint8_t LossReason, uint16_t PANId, uint8_t LogicalChannel, uint8_t ChannelPage) |
Callback function that must be implemented by application (NHLE) for MAC service MLME-SYNC-LOSS.indication. More... | |
void usr_mcps_data_ind | ( | wpan_addr_spec_t * | SrcAddrSpec, |
wpan_addr_spec_t * | DstAddrSpec, | ||
uint8_t | msduLength, | ||
uint8_t * | msdu, | ||
uint8_t | mpduLinkQuality, | ||
uint8_t | DSN, | ||
uint32_t | Timestamp, | ||
uint8_t | SecurityLevel, | ||
uint8_t | KeyIdMode, | ||
uint8_t | KeyIndex | ||
) |
Callback function that must be implemented by application (NHLE) for MAC service MCPS-DATA.indication.
SrcAddrSpec | Pointer to source address specification. |
DstAddrSpec | Pointer to destination address specification. |
msduLength | Number of octets contained in MSDU. |
msdu | Pointer to MSDU. |
mpduLinkQuality | LQI measured during reception of the MPDU. |
DSN | The DSN of the received data frame. |
Timestamp | The time, in symbols, at which the data were received; this parameter is only available if timestamping is enabled via compile switch ENABLE_TSTAMP. |
SecurityLevel | Used security level; this parameter is only available if MAC security is enabled via MAC_SECURITY_ZIP |
KeyIdMode | Used mode to identify the key; this parameter is only available if MAC security is enabled via MAC_SECURITY_ZIP |
KeyIndex | Used index of the key; this parameter is only available if MAC security is enabled via MAC_SECURITY_ZIP |
References wpan_addr_spec_tag::Addr, wpan_addr_spec_tag::AddrMode, EOT, get_next_tx_buffer(), MAC_PID, MAC_PID_LEN, MCPS_DATA_IND_LEN, MCPS_DATA_INDICATION, and wpan_addr_spec_tag::PANId.
Referenced by mcps_data_ind().
void usr_mlme_associate_ind | ( | uint64_t | DeviceAddress, |
uint8_t | CapabilityInformation | ||
) |
Callback function that must be implemented by application (NHLE) for MAC service MLME-ASSOCIATE.indication.
DeviceAddress | Extended address of device requesting association. |
CapabilityInformation | Capabilities of device requesting association. (WPAN_CAP_ALTPANCOORD | WPAN_CAP_FFD | WPAN_CAP_PWRSOURCE | WPAN_CAP_RXONWHENIDLE | WPAN_CAP_ALLOCADDRESS) |
void usr_mlme_beacon_notify_ind | ( | uint8_t | BSN, |
wpan_pandescriptor_t * | PANDescriptor, | ||
uint8_t | PendAddrSpec, | ||
uint8_t * | AddrList, | ||
uint8_t | sduLength, | ||
uint8_t * | sdu | ||
) |
Callback function that must be implemented by application (NHLE) for MAC service MLME-BEACON-NOTIFY.indication.
BSN | Beacon sequence number. |
PANDescriptor | Pointer to PAN descriptor for received beacon. |
PendAddrSpec | Pending address specification in received beacon. |
AddrList | List of addresses of devices the coordinator has pending data. |
sduLength | Length of beacon payload. |
sdu | Pointer to beacon payload. |
References wpan_addr_spec_tag::Addr, wpan_addr_spec_tag::AddrMode, wpan_pandescriptor_tag::ChannelPage, wpan_pandescriptor_tag::CoordAddrSpec, EOT, get_next_tx_buffer(), wpan_pandescriptor_tag::GTSPermit, wpan_pandescriptor_tag::LinkQuality, wpan_pandescriptor_tag::LogicalChannel, MAC_PID, MAC_PID_LEN, MLME_BEACON_NOTIFY_IND_LEN, MLME_BEACON_NOTIFY_INDICATION, wpan_addr_spec_tag::PANId, wpan_pandescriptor_tag::SuperframeSpec, wpan_pandescriptor_tag::TimeStamp, WPAN_DESCRIPTOR_LEN, WPAN_NUM_EXTENDED_ADDR_PENDING, and WPAN_NUM_SHORT_ADDR_PENDING.
Referenced by mlme_beacon_notify_ind().
void usr_mlme_comm_status_ind | ( | wpan_addr_spec_t * | SrcAddrSpec, |
wpan_addr_spec_t * | DstAddrSpec, | ||
uint8_t | status | ||
) |
Callback function that must be implemented by application (NHLE) for MAC service MLME-COMM-STATUS.indication.
SrcAddrSpec | Pointer to source address specification. |
DstAddrSpec | Pointer to destination address specification. |
status | Result for related response operation. |
void usr_mlme_disassociate_ind | ( | uint64_t | DeviceAddress, |
uint8_t | DisassociateReason | ||
) |
Callback function that must be implemented by application (NHLE) for MAC service MLME-DISASSOCIATE.indication.
DeviceAddress | Extended address of device which initiated the disassociation request. |
DisassociateReason | Reason for the disassociation. Valid values: |
References EOT, get_next_tx_buffer(), MAC_PID, MAC_PID_LEN, MLME_DISASSOCIATE_IND_LEN, and MLME_DISASSOCIATE_INDICATION.
Referenced by mlme_disassociate_ind().
void usr_mlme_orphan_ind | ( | uint64_t | OrphanAddress | ) |
Callback function that must be implemented by application (NHLE) for MAC service MLME-ORPHAN.indication.
OrphanAddress | Address of orphaned device. |
void usr_mlme_sync_loss_ind | ( | uint8_t | LossReason, |
uint16_t | PANId, | ||
uint8_t | LogicalChannel, | ||
uint8_t | ChannelPage | ||
) |
Callback function that must be implemented by application (NHLE) for MAC service MLME-SYNC-LOSS.indication.
LossReason | Reason for synchronization loss. |
PANId | The PAN identifier with which the device lost synchronization or to which it was realigned. |
LogicalChannel | The logical channel on which the device lost synchronization or to which it was realigned. |
ChannelPage | The channel page on which the device lost synchronization or to which it was realigned. |
References EOT, get_next_tx_buffer(), MAC_PID, MAC_PID_LEN, MLME_SYNC_LOSS_IND_LEN, and MLME_SYNC_LOSS_INDICATION.
Referenced by mlme_sync_loss_ind().