This group contains functions and definitions related to configuring and enabling/disabling on-chip oscillators.
Internal RC-oscillators, external crystal oscillators and external clock generators are supported by this module. What all of these have in common is that they swing at a fixed, nominal frequency which is normally not adjustable.
The following example demonstrates how to enable the external oscillator on XMEGA A and wait for it to be ready to use. The oscillator identifiers are platform-specific, so while the same procedure is used on all platforms, the parameter to osc_enable() will be different from device to device.
If external oscillators are used, the board code must provide the following definitions for each of those:
Macros | |
#define | BOARD_XOSC_STARTUP_CYCLES (BOARD_XOSC_HZ / 1000000 * BOARD_XOSC_STARTUP_US) |
#define | CONFIG_XOSC_32KHZ_LPM |
Define for enabling Low Power Mode for 32 kHz external oscillator. More... | |
#define | CONFIG_XOSC_RANGE 0 |
Board-dependent value that sets the frequency range of the external oscillator. More... | |
#define | CONFIG_XOSC_STARTUP 0 |
Board-dependent value that determines the number of start-up cycles for external resonators, based on BOARD_XOSC_STARTUP_US. More... | |
Functions | |
static void | osc_enable_external (uint8_t id) |
Enable external oscillator id. More... | |
static void | osc_enable_internal (uint8_t id) |
Enable internal oscillator id. More... | |
Oscillator Management | |
static void | osc_wait_ready (uint8_t id) |
Wait until the oscillator identified by id is ready. More... | |
static void | osc_disable (uint8_t id) |
Disable oscillator id. More... | |
static void | osc_enable (uint8_t id) |
Enable oscillator id. More... | |
static bool | osc_is_ready (uint8_t id) |
Determine whether oscillator id is ready. More... | |
static uint32_t | osc_get_rate (uint8_t id) |
Return the frequency of oscillator id in Hz. More... | |
Oscillator identifiers | |
#define | OSC_ID_RC2MHZ OSC_RC2MEN_bm |
2 MHz Internal RC Oscillator More... | |
#define | OSC_ID_RC32MHZ OSC_RC32MEN_bm |
32 MHz Internal RC Oscillator More... | |
#define | OSC_ID_RC32KHZ OSC_RC32KEN_bm |
32 KHz Internal RC Oscillator More... | |
#define | OSC_ID_XOSC OSC_XOSCEN_bm |
External Oscillator. More... | |
#define | OSC_ID_RC8MHZ OSC_RC8MEN_bm |
8 MHz Internal RC Oscillator More... | |
#define | OSC_ID_USBSOF 0xff |
Reference from USB Start Of Frame. More... | |
External oscillator types | |
#define | XOSC_TYPE_EXTERNAL 0 |
External clock signal. More... | |
#define | XOSC_TYPE_32KHZ 2 |
32.768 kHz resonator on TOSC More... | |
#define | XOSC_TYPE_XTAL 3 |
0.4 to 16 MHz resonator on XTAL More... | |
XTAL resonator start-up cycles | |
#define | XOSC_STARTUP_256 0 |
256 cycle start-up time More... | |
#define | XOSC_STARTUP_1024 1 |
1 k cycle start-up time More... | |
#define | XOSC_STARTUP_16384 2 |
16 k cycle start-up time More... | |
XTAL resonator frequency range | |
#define | XOSC_RANGE_04TO2 OSC_FRQRANGE_04TO2_gc |
0.4 to 2 MHz frequency range More... | |
#define | XOSC_RANGE_2TO9 OSC_FRQRANGE_2TO9_gc |
2 to 9 MHz frequency range More... | |
#define | XOSC_RANGE_9TO12 OSC_FRQRANGE_9TO12_gc |
9 to 12 MHz frequency range More... | |
#define | XOSC_RANGE_12TO16 OSC_FRQRANGE_12TO16_gc |
12 to 16 MHz frequency range More... | |
XMEGA-Specific Oscillator Features | |
static void | osc_enable_autocalibration (uint8_t id, uint8_t ref_id) |
Enable DFLL-based automatic calibration of an internal oscillator. More... | |
static void | osc_disable_autocalibration (uint8_t id) |
Disable DFLL-based automatic calibration of an internal oscillator. More... | |
static void | osc_user_calibration (uint8_t id, uint16_t calib) |
Load a specific calibration value for the specified oscillator. More... | |
#define BOARD_XOSC_STARTUP_CYCLES (BOARD_XOSC_HZ / 1000000 * BOARD_XOSC_STARTUP_US) |
Number of start-up cycles for the board's XOSC.
#define CONFIG_XOSC_32KHZ_LPM |
Define for enabling Low Power Mode for 32 kHz external oscillator.
#define CONFIG_XOSC_RANGE 0 |
Board-dependent value that sets the frequency range of the external oscillator.
This is written to the FRQRANGE field of OSC.XOSCCTRL.
Referenced by osc_enable_external().
#define CONFIG_XOSC_STARTUP 0 |
Board-dependent value that determines the number of start-up cycles for external resonators, based on BOARD_XOSC_STARTUP_US.
This is written to the two MSB of the XOSCSEL field of OSC.XOSCCTRL.
Referenced by osc_enable_external().
#define OSC_ID_RC2MHZ OSC_RC2MEN_bm |
2 MHz Internal RC Oscillator
Referenced by osc_disable_autocalibration(), osc_enable_autocalibration(), osc_get_rate(), osc_user_calibration(), and sysclk_init().
#define OSC_ID_RC32KHZ OSC_RC32KEN_bm |
32 KHz Internal RC Oscillator
Referenced by osc_enable_autocalibration(), osc_get_rate(), sysclk_init(), and sysclk_rtcsrc_enable().
#define OSC_ID_RC32MHZ OSC_RC32MEN_bm |
32 MHz Internal RC Oscillator
Referenced by osc_disable_autocalibration(), osc_enable_autocalibration(), osc_get_rate(), osc_user_calibration(), pll_enable_source(), and sysclk_init().
#define OSC_ID_RC8MHZ OSC_RC8MEN_bm |
8 MHz Internal RC Oscillator
Referenced by osc_enable_internal(), osc_user_calibration(), and sysclk_init().
#define OSC_ID_USBSOF 0xff |
Reference from USB Start Of Frame.
Referenced by osc_disable(), osc_enable_autocalibration(), osc_enable_internal(), osc_get_rate(), osc_is_ready(), pll_enable_source(), and sysclk_init().
#define OSC_ID_XOSC OSC_XOSCEN_bm |
External Oscillator.
Referenced by osc_enable(), osc_enable_autocalibration(), osc_enable_external(), osc_get_rate(), pll_enable_source(), pll_get_default_rate_priv(), sysclk_init(), and sysclk_rtcsrc_enable().
#define XOSC_RANGE_04TO2 OSC_FRQRANGE_04TO2_gc |
0.4 to 2 MHz frequency range
#define XOSC_RANGE_12TO16 OSC_FRQRANGE_12TO16_gc |
12 to 16 MHz frequency range
#define XOSC_RANGE_2TO9 OSC_FRQRANGE_2TO9_gc |
2 to 9 MHz frequency range
#define XOSC_RANGE_9TO12 OSC_FRQRANGE_9TO12_gc |
9 to 12 MHz frequency range
#define XOSC_STARTUP_1024 1 |
1 k cycle start-up time
#define XOSC_STARTUP_16384 2 |
16 k cycle start-up time
#define XOSC_STARTUP_256 0 |
256 cycle start-up time
#define XOSC_TYPE_32KHZ 2 |
32.768 kHz resonator on TOSC
#define XOSC_TYPE_EXTERNAL 0 |
External clock signal.
#define XOSC_TYPE_XTAL 3 |
0.4 to 16 MHz resonator on XTAL
|
inlinestatic |
Disable oscillator id.
References Assert, cpu_irq_restore(), cpu_irq_save(), and OSC_ID_USBSOF.
Referenced by sysclk_init().
|
inlinestatic |
Disable DFLL-based automatic calibration of an internal oscillator.
id | The ID of the oscillator for which to disable auto-calibration:
|
References Assert, OSC_ID_RC2MHZ, and OSC_ID_RC32MHZ.
|
inlinestatic |
Enable oscillator id.
The startup time and mode value is automatically determined based on definitions in the board code.
References osc_enable_external(), osc_enable_internal(), and OSC_ID_XOSC.
Referenced by osc_enable_autocalibration(), pll_enable_source(), sysclk_init(), and sysclk_rtcsrc_enable().
|
inlinestatic |
Enable DFLL-based automatic calibration of an internal oscillator.
The XMEGA features two Digital Frequency Locked Loops (DFLLs) which can be used to improve the accuracy of the 2 MHz and 32 MHz internal RC oscillators. The DFLL compares the oscillator frequency with a more accurate reference clock to do automatic run-time calibration of the oscillator.
This function enables auto-calibration for either the 2 MHz or 32 MHz internal oscillator using either the 32.768 kHz calibrated internal oscillator or an external crystal oscillator as a reference. If the latter option is used, the crystal must be connected to the TOSC pins and run at 32.768 kHz.
id | The ID of the oscillator for which to enable auto-calibration:
|
ref_id | The ID of the oscillator to use as a reference:
|
References Assert, cpu_irq_restore(), cpu_irq_save(), osc_enable(), OSC_ID_RC2MHZ, OSC_ID_RC32KHZ, OSC_ID_RC32MHZ, OSC_ID_USBSOF, OSC_ID_XOSC, and XMEGA_E.
Referenced by pll_enable_source(), and sysclk_init().
|
inlinestatic |
Enable external oscillator id.
Do not call this function directly. Use osc_enable() instead. Also note that this function is only available if the board actually has an external oscillator crystal.
References Assert, BOARD_XOSC_TYPE, CONFIG_XOSC_RANGE, CONFIG_XOSC_STARTUP, cpu_irq_restore(), cpu_irq_save(), and OSC_ID_XOSC.
Referenced by osc_enable().
|
inlinestatic |
Enable internal oscillator id.
Do not call this function directly. Use osc_enable() instead.
References Assert, cpu_irq_restore(), cpu_irq_save(), OSC_ID_RC8MHZ, and OSC_ID_USBSOF.
Referenced by osc_enable().
|
inlinestatic |
Return the frequency of oscillator id in Hz.
References Assert, BOARD_XOSC_HZ, CONFIG_OSC_RC32_CAL, OSC_ID_RC2MHZ, OSC_ID_RC32KHZ, OSC_ID_RC32MHZ, OSC_ID_USBSOF, and OSC_ID_XOSC.
Referenced by pll_get_default_rate_priv().
|
inlinestatic |
Determine whether oscillator id is ready.
true | Oscillator id is running and ready to use as a clock source. |
false | Oscillator id is not running. |
References Assert, and OSC_ID_USBSOF.
Referenced by osc_wait_ready(), and pll_enable_source().
|
inlinestatic |
Load a specific calibration value for the specified oscillator.
id | The ID of the oscillator for which to disable auto-calibration:
|
calib | The specific calibration value required: |
References Assert, LSB, MSB, OSC_ID_RC2MHZ, OSC_ID_RC32MHZ, and OSC_ID_RC8MHZ.
Referenced by sysclk_init().
|
inlinestatic |
Wait until the oscillator identified by id is ready.
This function will busy-wait for the oscillator identified by id to become stable and ready to use as a clock source.
id | A number identifying the oscillator to wait for. |
References osc_is_ready().
Referenced by pll_enable_source(), sysclk_init(), and sysclk_rtcsrc_enable().