This file handles the interrupts generated by the transceiver.
Copyright (c) 2013-2018 Microchip Technology Inc. and its subsidiaries.
#include <stdint.h>
#include <stdbool.h>
#include <stddef.h>
#include "return_val.h"
#include "tal.h"
#include "ieee_const.h"
#include "stack_config.h"
#include "bmm.h"
#include "qmm.h"
#include "tal_irq_handler.h"
#include "tal_rx.h"
#include "atmega128rfa1.h"
#include "tal_internal.h"
#include "tal_constants.h"
#include "tal_tx.h"
#include "mac_build_config.h"
Functions | |
ISR (TRX24_TX_END_vect) | |
ISR for transceiver's transmit end interrupt. More... | |
ISR (TRX24_RX_END_vect) | |
ISR for transceiver's receive end interrupt. More... | |
ISR (TRX24_CCA_ED_DONE_vect) | |
ISR for transceiver's CCA/ED measurement done interrupt. More... | |
ISR (TRX24_AWAKE_vect) | |
ISR for transceiver's Awake interrupt. More... | |
ISR (TRX24_RX_START_vect) | |
ISR for transceiver's rx start interrupt. More... | |
ISR (TRX24_PLL_LOCK_vect) | |
ISR for transceiver's PLL lock interrupt. More... | |
ISR (TRX24_PLL_UNLOCK_vect) | |
ISR for transceiver's PLL unlock interrupt. More... | |
ISR (TRX24_XAH_AMI_vect) | |
ISR for transceiver's address match interrupt. More... | |
ISR (BAT_LOW_vect) | |
ISR for transceiver's battery low interrupt. More... | |
ISR (AES_READY_vect) | |
ISR for transceiver's AES interrupt. More... | |
void | pal_trx_irq_init_awake (FUNC_PTR trx_irq_cb) |
Initializes the transceiver AWAKE interrupt. More... | |
void | pal_trx_irq_init_cca_ed (FUNC_PTR trx_irq_cb) |
Initializes the transceiver CCA ED END interrupt. More... | |
void | pal_trx_irq_init_rx_end (FUNC_PTR trx_irq_cb) |
Initializes the transceiver RX END interrupt. More... | |
void | pal_trx_irq_init_tx_end (FUNC_PTR trx_irq_cb) |
Initializes the transceiver TX END interrupt. More... | |
void | trx_awake_handler_cb (void) |
void | trx_rx_end_handler_cb (void) |
Transceiver interrupt handler. More... | |
void | trx_tx_end_handler_cb (void) |
Transceiver interrupt handler. More... | |
Variables | |
static irq_handler_t | irq_hdl_trx_awake |
Function pointer to store callback for transceiver AWAKE interrupt. More... | |
static irq_handler_t | irq_hdl_trx_cca_ed |
Function pointer to store callback for transceiver CCA_ED interrupt. More... | |
static irq_handler_t | irq_hdl_trx_rx_end |
Function pointer to store callback for transceiver RX_END interrupt. More... | |
static irq_handler_t | irq_hdl_trx_tx_end |
Function pointer to store callback for transceiver TX_END interrupt. More... | |
ISR | ( | TRX24_TX_END_vect | ) |
ISR for transceiver's transmit end interrupt.
References irq_hdl_trx_tx_end.
ISR | ( | TRX24_RX_END_vect | ) |
ISR for transceiver's receive end interrupt.
References irq_hdl_trx_rx_end.
ISR | ( | TRX24_CCA_ED_DONE_vect | ) |
ISR for transceiver's CCA/ED measurement done interrupt.
References irq_hdl_trx_cca_ed.
ISR | ( | TRX24_AWAKE_vect | ) |
ISR for transceiver's Awake interrupt.
References irq_hdl_trx_awake.
ISR | ( | TRX24_RX_START_vect | ) |
ISR for transceiver's rx start interrupt.
By the time the SFD is detected, the hardware timestamps the current frame in the SCTSR register.
ISR | ( | TRX24_PLL_LOCK_vect | ) |
ISR for transceiver's PLL lock interrupt.
ISR | ( | TRX24_PLL_UNLOCK_vect | ) |
ISR for transceiver's PLL unlock interrupt.
ISR | ( | TRX24_XAH_AMI_vect | ) |
ISR for transceiver's address match interrupt.
ISR | ( | BAT_LOW_vect | ) |
ISR for transceiver's battery low interrupt.
ISR | ( | AES_READY_vect | ) |
ISR for transceiver's AES interrupt.
void pal_trx_irq_init_awake | ( | FUNC_PTR | trx_irq_cb | ) |
Initializes the transceiver AWAKE interrupt.
This function sets the microcontroller specific registers responsible for handling the transceiver AWAKE interrupt
trx_irq_cb | Callback function for the transceiver AWAKE interrupt |
References irq_hdl_trx_awake.
Referenced by set_trx_state(), and tal_init().
void pal_trx_irq_init_cca_ed | ( | FUNC_PTR | trx_irq_cb | ) |
Initializes the transceiver CCA ED END interrupt.
This function sets the microcontroller specific registers responsible for handling the transceiver CCA ED END interrupt
trx_irq_cb | Callback function for the transceiver CCA ED END interrupt |
References irq_hdl_trx_cca_ed.
Referenced by tal_ed_start().
void pal_trx_irq_init_rx_end | ( | FUNC_PTR | trx_irq_cb | ) |
Initializes the transceiver RX END interrupt.
This function sets the microcontroller specific registers responsible for handling the transceiver RX END interrupt
trx_irq_cb | Callback function for the transceiver RX END interrupt |
References irq_hdl_trx_rx_end.
Referenced by tal_init().
void pal_trx_irq_init_tx_end | ( | FUNC_PTR | trx_irq_cb | ) |
Initializes the transceiver TX END interrupt.
This function sets the microcontroller specific registers responsible for handling the transceiver TX END interrupt
trx_irq_cb | Callback function for the transceiver TX END interrupt |
References irq_hdl_trx_tx_end.
Referenced by tal_init().
|
static |
Function pointer to store callback for transceiver AWAKE interrupt.
Referenced by ISR(), and pal_trx_irq_init_awake().
|
static |
Function pointer to store callback for transceiver CCA_ED interrupt.
Referenced by ISR(), and pal_trx_irq_init_cca_ed().
|
static |
Function pointer to store callback for transceiver RX_END interrupt.
Referenced by ISR(), and pal_trx_irq_init_rx_end().
|
static |
Function pointer to store callback for transceiver TX_END interrupt.
Referenced by ISR(), and pal_trx_irq_init_tx_end().