Implementation of Transceiver Feature Access (TFA) functionality.
Copyright (c) 2013-2018 Microchip Technology Inc. and its subsidiaries.
#include <stdint.h>
#include <string.h>
#include <stdbool.h>
#include <stdlib.h>
#include "pal.h"
#include "return_val.h"
#include "tal.h"
#include "tal_irq_handler.h"
#include "tal_constants.h"
#include "tal_internal.h"
#include "ieee_const.h"
#include "atmega128rfa1.h"
#include "tfa.h"
Macros | |
#define | CLIP_VALUE_REG (55) |
#define | NUM_SAMPLES 16 |
Typedefs | |
typedef enum pin_state_tag | pin_state_t |
Pin State. More... | |
Enumerations | |
enum | pin_state_tag { LOW, HIGH, LOW, HIGH } |
Pin State. More... | |
Functions | |
static void | init_tfa_pib (void) |
Initialize the TFA PIB. More... | |
phy_enum_t | tfa_cca_perform (void) |
Perform a CCA. More... | |
void | tfa_continuous_tx_start (continuous_tx_mode_t tx_mode, bool random_content) |
Starts continuous transmission on current channel. More... | |
void | tfa_continuous_tx_stop (void) |
Stops CW transmission. More... | |
uint8_t | tfa_ed_sample (void) |
Perform a single ED measurement. More... | |
uint16_t | tfa_get_batmon_voltage (void) |
Gets the transceiver's supply voltage. More... | |
double | tfa_get_temperature (void) |
Get the temperature value from the integrated sensor. More... | |
retval_t | tfa_init (void) |
Initializes the TFA. More... | |
retval_t | tfa_pib_get (tfa_pib_t tfa_pib_attribute, void *value) |
Gets a TFA PIB attribute. More... | |
retval_t | tfa_pib_set (tfa_pib_t tfa_pib_attribute, void *value) |
Sets a TFA PIB attribute. More... | |
void | tfa_reset (bool set_default_pib) |
Reset the TFA. More... | |
static void | write_all_tfa_pibs_to_trx (void) |
Write all shadow PIB variables to the transceiver. More... | |
Variables | |
static int8_t | tfa_pib_rx_sens |
TFA PIB attribute to reduce the Rx sensitivity. More... | |
#define CLIP_VALUE_REG (55) |
Referenced by tfa_ed_sample().
#define NUM_SAMPLES 16 |
Referenced by tfa_get_temperature().
typedef enum pin_state_tag pin_state_t |
Pin State.
enum pin_state_tag |
|
static |
TFA PIB attribute to reduce the Rx sensitivity.
Represents the Rx sensitivity value in dBm; example: -52
Referenced by init_tfa_pib(), tfa_pib_get(), tfa_pib_set(), and write_all_tfa_pibs_to_trx().