PER Measuremnt mode prototypes and defines.
-Performance Analyzer application
Copyright (c) 2013-2018 Microchip Technology Inc. and its subsidiaries.
Data Structures | |
struct | ed_scan_result_t |
ED scan result structure to hold the channel and its ED value. More... | |
struct | trx_config_params_t |
Structure to hold all configurable parameter values. More... | |
Macros | |
#define | BASE_ISM_FREQUENCY_MHZ (2306) |
#define | CC_BAND_0 (0x00) |
#define | CC_BAND_8 (0x08) |
#define | CC_BAND_9 (0x09) |
#define | CC_NUMBER_0 (0x00) |
#define | CHANNEL (0) |
#define | CHANNEL_PAGE (1) |
#define | DISABLE_ALL_RPC_MODES (0xC1) |
#define | DISABLE_RX_SAFE_MODE (0x60) |
#define | ENABLE_ALL_RPC_MODES (0xff) |
#define | ENABLE_RX_SAFE_MODE (0xA0) |
#define | FREQ_BAND_08 (4) |
#define | FREQ_BAND_09 (5) |
#define | LED_TOGGLE_COUNT_FOR_PER (50) |
#define | MAX_ISM_FREQUENCY_MHZ (2527) |
#define | MID_ISM_FREQUENCY_MHZ (2434) |
#define | MIN_ISM_FREQUENCY_MHZ (2322) |
#define | MIN_TX_PWR_REG_VAL (0x0f) |
#define | PULSE_CW_TX_TIME_IN_MICRO_SEC (50000) |
#define | TX_POWER_DBM (2) |
Request and response Ids which sent over the air | |
#define | SET_PARAM (0x01) |
#define | RESULT_REQ (0x02) |
#define | RESULT_RSP (0x03) |
#define | IDENTIFY_NODE (0x07) |
#define | PER_TEST_PKT (0x0B) |
#define | PEER_INFO_REQ (0x0C) |
#define | PEER_INFO_RSP (0x0D) |
#define | DISCONNECT_NODE (0x0E) |
#define | SET_DEFAULT_REQ (0x0F) |
#define | PER_TEST_START_PKT (0x10) |
#define | RANGE_TEST_START_PKT (0x11) |
#define | RANGE_TEST_PKT (0x12) |
#define | RANGE_TEST_RSP (0x13) |
#define | RANGE_TEST_STOP_PKT (0x14) |
#define | RANGE_TEST_MARKER_CMD (0x15) |
#define | RANGE_TEST_MARKER_RSP (0x16) |
#define | REMOTE_TEST_CMD (0x17) |
#define | REMOTE_TEST_REPLY_CMD (0x18) |
#define | PKT_STREAM_PKT (0x18) |
#define | RANGE_TEST_PKT_LENGTH (19) |
#define | LED_BLINK_RATE_IN_MICRO_SEC (50000) |
Functions | |
void | app_reset (void) |
void | configure_pkt_stream_frames (uint16_t frame_len) |
Configure the frame to be used for Packet Streaming. More... | |
void | marker_rsp_timer_handler_cb (void *parameter) |
Timer Callback function if marker command is received on air This is used to blink the LED and thus identify that the marker frame is received. More... | |
void | marker_tx_timer_handler_cb (void *parameter) |
Timer Callback function if marker response command is transmitted on air This is used to blink the LED and thus identify that the transmission is done. More... | |
void | per_mode_initiator_ed_end_cb (uint8_t energy_level) |
User call back function after ED Scan completion. More... | |
void | per_mode_initiator_init (void *parameter) |
Initialize the application in PER Measurement mode as Initiator. More... | |
void | per_mode_initiator_rx_cb (frame_info_t *frame) |
Callback that is called if data has been received by trx in the PER_FOUND_PER_INITIATOR state. More... | |
void | per_mode_initiator_task (void) |
Application task for PER Measurement mode as initiator. More... | |
void | per_mode_initiator_tx_done_cb (retval_t status, frame_info_t *frame) |
Callback that is called once tx is done in the PER_FOUND_PER_INITIATOR state . More... | |
void | per_mode_receptor_init (void *parameter) |
Initialize the application in PER Measurement mode as Receptor. More... | |
void | per_mode_receptor_rx_cb (frame_info_t *frame) |
Callback that is called if data has been received by trx in the PER_TEST_RECEPTOR state This call back is used when the node is operating as PER Measurement mode Receptor. More... | |
void | per_mode_receptor_task (void) |
The application task when the node is in PER_TEST_RECEPTOR state i.e.PER Measurement mode as Receptor. More... | |
void | per_mode_receptor_tx_done_cb (retval_t status, frame_info_t *frame) |
Callback that is called once tx is done in PER_TEST_RECEPTOR state This call back is used when the node is operating as PER Measurement mode Receptor. More... | |
void | pkt_stream_gap_timer (void *parameter) |
Timer used in Packet Streaming Mode to add gap in between consecutive frames. More... | |
float | reverse_float (const float float_val) |
The reverse_float is used for reversing a float variable for supporting BIG ENDIAN systems. More... | |
bool | send_remote_reply_cmd (uint8_t *serial_buf, uint8_t len) |
This function is used to send a remote test repsonse command back to the initiator. More... | |
void | stop_pkt_streaming (void *parameter) |
This function is called to abort the packet streaming mode in progress. More... | |
Variables | |
trx_config_params_t | curr_trx_config_params |
trx_config_params_t | default_trx_config_params |
#define BASE_ISM_FREQUENCY_MHZ (2306) |
Referenced by tal_calculate_frequency(), and tal_set_frequency().
#define CC_BAND_0 (0x00) |
#define CC_BAND_8 (0x08) |
#define CC_BAND_9 (0x09) |
#define CC_NUMBER_0 (0x00) |
Referenced by set_channel(), set_parameter_on_transmitter_node(), and set_paramter_on_recptor_node().
#define CHANNEL (0) |
Referenced by set_channel(), set_parameter_on_transmitter_node(), and set_paramter_on_recptor_node().
#define CHANNEL_PAGE (1) |
Referenced by set_channel_page(), set_parameter_on_transmitter_node(), and set_paramter_on_recptor_node().
#define DISABLE_ALL_RPC_MODES (0xC1) |
Referenced by config_per_test_parameters(), config_rpc_mode(), recover_all_settings(), and set_paramter_on_recptor_node().
#define DISABLE_RX_SAFE_MODE (0x60) |
Referenced by config_rpc_mode().
#define ENABLE_ALL_RPC_MODES (0xff) |
Referenced by config_rpc_mode(), and recover_all_settings().
#define ENABLE_RX_SAFE_MODE (0xA0) |
Referenced by config_per_test_parameters(), and config_rpc_mode().
#define FREQ_BAND_08 (4) |
Referenced by set_parameter_on_transmitter_node(), and set_paramter_on_recptor_node().
#define FREQ_BAND_09 (5) |
Referenced by set_parameter_on_transmitter_node(), and set_paramter_on_recptor_node().
#define LED_TOGGLE_COUNT_FOR_PER (50) |
Referenced by per_mode_initiator_tx_done_cb(), and per_mode_receptor_rx_cb().
#define MAX_ISM_FREQUENCY_MHZ (2527) |
Referenced by tal_set_frequency().
#define MID_ISM_FREQUENCY_MHZ (2434) |
Referenced by tal_calculate_frequency(), and tal_set_frequency().
#define MIN_ISM_FREQUENCY_MHZ (2322) |
Referenced by tal_set_frequency().
#define MIN_TX_PWR_REG_VAL (0x0f) |
Referenced by set_paramter_on_recptor_node(), and set_tx_power().
#define TX_POWER_DBM (2) |
Referenced by set_paramter_on_recptor_node().