Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
Oscillator Management

This group contains functions and definitions related to configuring and enabling/disabling on-chip oscillators.

Internal RC-oscillators, external crystal oscillators and external clock generators are supported by this module. What all of these have in common is that they swing at a fixed, nominal frequency which is normally not adjustable.

Example: Enabling an oscillator

The following example demonstrates how to enable the external oscillator on XMEGA A and wait for it to be ready to use. The oscillator identifiers are platform-specific, so while the same procedure is used on all platforms, the parameter to osc_enable() will be different from device to device.

Board-specific Definitions

If external oscillators are used, the board code must provide the following definitions for each of those:

Errata

Macros

#define CONFIG_XOSC_32KHZ_LPM
 Define for enabling Low Power Mode for 32 kHz external oscillator. More...
 

Functions

static void osc_enable_external (uint8_t id)
 Enable external oscillator id. More...
 
static void osc_enable_internal (uint8_t id)
 Enable internal oscillator id. More...
 

Oscillator Management

static void osc_wait_ready (uint8_t id)
 Wait until the oscillator identified by id is ready. More...
 
static void osc_disable (uint8_t id)
 Disable oscillator id. More...
 
static void osc_enable (uint8_t id)
 Enable oscillator id. More...
 
static bool osc_is_ready (uint8_t id)
 Determine whether oscillator id is ready. More...
 
static uint32_t osc_get_rate (uint8_t id)
 Return the frequency of oscillator id in Hz. More...
 

Oscillator identifiers

#define OSC_ID_RC2MHZ   OSC_RC2MEN_bm
 2 MHz Internal RC Oscillator More...
 
#define OSC_ID_RC32MHZ   OSC_RC32MEN_bm
 32 MHz Internal RC Oscillator More...
 
#define OSC_ID_RC32KHZ   OSC_RC32KEN_bm
 32 KHz Internal RC Oscillator More...
 
#define OSC_ID_XOSC   OSC_XOSCEN_bm
 External Oscillator. More...
 
#define OSC_ID_RC8MHZ   OSC_RC8MEN_bm
 8 MHz Internal RC Oscillator More...
 
#define OSC_ID_USBSOF   0xff
 Reference from USB Start Of Frame. More...
 

External oscillator types

#define XOSC_TYPE_EXTERNAL   0
 External clock signal. More...
 
#define XOSC_TYPE_32KHZ   2
 32.768 kHz resonator on TOSC More...
 
#define XOSC_TYPE_XTAL   3
 0.4 to 16 MHz resonator on XTAL More...
 

XTAL resonator start-up cycles

#define XOSC_STARTUP_256   0
 256 cycle start-up time More...
 
#define XOSC_STARTUP_1024   1
 1 k cycle start-up time More...
 
#define XOSC_STARTUP_16384   2
 16 k cycle start-up time More...
 

XTAL resonator frequency range

#define XOSC_RANGE_04TO2   OSC_FRQRANGE_04TO2_gc
 0.4 to 2 MHz frequency range More...
 
#define XOSC_RANGE_2TO9   OSC_FRQRANGE_2TO9_gc
 2 to 9 MHz frequency range More...
 
#define XOSC_RANGE_9TO12   OSC_FRQRANGE_9TO12_gc
 9 to 12 MHz frequency range More...
 
#define XOSC_RANGE_12TO16   OSC_FRQRANGE_12TO16_gc
 12 to 16 MHz frequency range More...
 

XMEGA-Specific Oscillator Features

static void osc_enable_autocalibration (uint8_t id, uint8_t ref_id)
 Enable DFLL-based automatic calibration of an internal oscillator. More...
 
static void osc_disable_autocalibration (uint8_t id)
 Disable DFLL-based automatic calibration of an internal oscillator. More...
 
static void osc_user_calibration (uint8_t id, uint16_t calib)
 Load a specific calibration value for the specified oscillator. More...
 

#define CONFIG_XOSC_32KHZ_LPM

Define for enabling Low Power Mode for 32 kHz external oscillator.

#define OSC_ID_RC2MHZ   OSC_RC2MEN_bm
#define OSC_ID_RC32KHZ   OSC_RC32KEN_bm

32 KHz Internal RC Oscillator

Referenced by osc_enable_autocalibration(), osc_get_rate(), sysclk_init(), and sysclk_rtcsrc_enable().

#define OSC_ID_RC32MHZ   OSC_RC32MEN_bm
#define OSC_ID_RC8MHZ   OSC_RC8MEN_bm

8 MHz Internal RC Oscillator

Referenced by osc_enable_internal(), osc_user_calibration(), and sysclk_init().

#define OSC_ID_USBSOF   0xff

Reference from USB Start Of Frame.

Note
This cannot be enabled or disabled, but can be used as a reference for the autocalibration (DFLL).

Referenced by osc_disable(), osc_enable_autocalibration(), osc_enable_internal(), osc_get_rate(), osc_is_ready(), pll_enable_source(), and sysclk_init().

#define XOSC_RANGE_04TO2   OSC_FRQRANGE_04TO2_gc

0.4 to 2 MHz frequency range

#define XOSC_RANGE_12TO16   OSC_FRQRANGE_12TO16_gc

12 to 16 MHz frequency range

#define XOSC_RANGE_2TO9   OSC_FRQRANGE_2TO9_gc

2 to 9 MHz frequency range

#define XOSC_RANGE_9TO12   OSC_FRQRANGE_9TO12_gc

9 to 12 MHz frequency range

#define XOSC_STARTUP_1024   1

1 k cycle start-up time

#define XOSC_STARTUP_16384   2

16 k cycle start-up time

#define XOSC_STARTUP_256   0

256 cycle start-up time

#define XOSC_TYPE_32KHZ   2

32.768 kHz resonator on TOSC

#define XOSC_TYPE_EXTERNAL   0

External clock signal.

#define XOSC_TYPE_XTAL   3

0.4 to 16 MHz resonator on XTAL

void osc_disable ( uint8_t  id)
inlinestatic

Disable oscillator id.

References Assert, cpu_irq_restore(), cpu_irq_save(), and OSC_ID_USBSOF.

Referenced by sysclk_init().

static void osc_disable_autocalibration ( uint8_t  id)
inlinestatic

Disable DFLL-based automatic calibration of an internal oscillator.

See Also
osc_enable_autocalibration
Parameters
idThe ID of the oscillator for which to disable auto-calibration:
  • OSC_ID_RC2MHZ or OSC_ID_RC32MHZ.

References Assert, OSC_ID_RC2MHZ, and OSC_ID_RC32MHZ.

void osc_enable ( uint8_t  id)
inlinestatic

Enable oscillator id.

The startup time and mode value is automatically determined based on definitions in the board code.

References osc_enable_external(), osc_enable_internal(), and OSC_ID_XOSC.

Referenced by osc_enable_autocalibration(), pll_enable_source(), sysclk_init(), and sysclk_rtcsrc_enable().

static void osc_enable_autocalibration ( uint8_t  id,
uint8_t  ref_id 
)
inlinestatic

Enable DFLL-based automatic calibration of an internal oscillator.

The XMEGA features two Digital Frequency Locked Loops (DFLLs) which can be used to improve the accuracy of the 2 MHz and 32 MHz internal RC oscillators. The DFLL compares the oscillator frequency with a more accurate reference clock to do automatic run-time calibration of the oscillator.

This function enables auto-calibration for either the 2 MHz or 32 MHz internal oscillator using either the 32.768 kHz calibrated internal oscillator or an external crystal oscillator as a reference. If the latter option is used, the crystal must be connected to the TOSC pins and run at 32.768 kHz.

Parameters
idThe ID of the oscillator for which to enable auto-calibration:
  • OSC_ID_RC2MHZ or OSC_ID_RC32MHZ.
ref_idThe ID of the oscillator to use as a reference:
  • OSC_ID_RC32KHZ or OSC_ID_XOSC for internal or external 32 kHz reference, respectively.
  • OSC_ID_USBSOF for 32 MHz only when USB is available and running.

References Assert, cpu_irq_restore(), cpu_irq_save(), osc_enable(), OSC_ID_RC2MHZ, OSC_ID_RC32KHZ, OSC_ID_RC32MHZ, OSC_ID_USBSOF, OSC_ID_XOSC, and XMEGA_E.

Referenced by pll_enable_source(), and sysclk_init().

static void osc_enable_external ( uint8_t  id)
inlinestatic

Enable external oscillator id.

Do not call this function directly. Use osc_enable() instead. Also note that this function is only available if the board actually has an external oscillator crystal.

References Assert, cpu_irq_restore(), cpu_irq_save(), and OSC_ID_XOSC.

Referenced by osc_enable().

static void osc_enable_internal ( uint8_t  id)
inlinestatic

Enable internal oscillator id.

Do not call this function directly. Use osc_enable() instead.

References Assert, cpu_irq_restore(), cpu_irq_save(), OSC_ID_RC8MHZ, and OSC_ID_USBSOF.

Referenced by osc_enable().

uint32_t osc_get_rate ( uint8_t  id)
inlinestatic

Return the frequency of oscillator id in Hz.

References Assert, OSC_ID_RC2MHZ, OSC_ID_RC32KHZ, OSC_ID_RC32MHZ, OSC_ID_USBSOF, and OSC_ID_XOSC.

Referenced by pll_get_default_rate_priv().

osc_is_ready ( uint8_t  id)
inlinestatic

Determine whether oscillator id is ready.

Return values
trueOscillator id is running and ready to use as a clock source.
falseOscillator id is not running.

References Assert, and OSC_ID_USBSOF.

Referenced by osc_wait_ready(), and pll_enable_source().

static void osc_user_calibration ( uint8_t  id,
uint16_t  calib 
)
inlinestatic

Load a specific calibration value for the specified oscillator.

Parameters
idThe ID of the oscillator for which to disable auto-calibration:
  • OSC_ID_RC2MHZ or OSC_ID_RC32MHZ.
calibThe specific calibration value required:

References Assert, LSB, MSB, OSC_ID_RC2MHZ, OSC_ID_RC32MHZ, and OSC_ID_RC8MHZ.

Referenced by sysclk_init().

static void osc_wait_ready ( uint8_t  id)
inlinestatic

Wait until the oscillator identified by id is ready.

This function will busy-wait for the oscillator identified by id to become stable and ready to use as a clock source.

Parameters
idA number identifying the oscillator to wait for.

References osc_is_ready().

Referenced by pll_enable_source(), sysclk_init(), and sysclk_rtcsrc_enable().