Functions | |
void | board_init (void) |
This function initializes the board target resources. More... | |
void board_init | ( | void | ) |
This function initializes the board target resources.
This function should be called to ensure proper initialization of the target board hardware connected to the part.
References AT86RFX_RST_PIN, AT86RFX_SLP_PIN, AT86RFX_SPI_CS, AT86RFX_SPI_MISO, AT86RFX_SPI_MOSI, AT86RFX_SPI_SCK, GPIO_PUSH_BUTTON_0, ioport_configure_pin(), IOPORT_CREATE_PIN, IOPORT_DIR_INPUT, IOPORT_DIR_OUTPUT, IOPORT_INIT_HIGH, IOPORT_LEVEL, IOPORT_PULL_UP, LED0_GPIO, LED1_GPIO, and LED2_GPIO.
Referenced by main().