Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
System Clock Management

See Quick Start Guide for the System Clock Management service (XMEGA).

The sysclk API covers the system clock and all clocks derived from it. The system clock is a chip-internal clock on which all synchronous clocks, i.e. CPU and bus/peripheral clocks, are based. The system clock is typically generated from one of a variety of sources, which may include crystal and RC oscillators as well as PLLs. The clocks derived from the system clock are sometimes also known as synchronous clocks, since they always run synchronously with respect to each other, as opposed to generic clocks which may run from different oscillators or PLLs.

Most applications should simply call sysclk_init() to initialize everything related to the system clock and its source (oscillator, PLL or DFLL), and leave it at that. More advanced applications, and platform-specific drivers, may require additional services from the clock system, some of which may be platform-specific.

Platform Dependencies

The sysclk API is partially chip- or platform-specific. While all platforms provide mostly the same functionality, there are some variations around how different bus types and clock tree structures are handled.

The following functions are available on all platforms with the same parameters and functionality. These functions may be called freely by portable applications, drivers and services:

The following functions are available on all platforms, but there may be variations in the function signature (i.e. parameters) and behavior. These functions are typically called by platform-specific parts of drivers, and applications that aren't intended to be portable:

All other functions should be considered platform-specific. Enabling/disabling clocks to specific peripherals as well as determining the speed of these clocks should be done by calling functions provided by the driver for that peripheral.

Configuration Symbols

The following configuration symbols may be used to specify the initial system clock configuration. If any of the symbols are not set, reasonable defaults will be provided.

System Clock Sources

#define SYSCLK_SRC_RC2MHZ   CLK_SCLKSEL_RC2M_gc
 Internal 2 MHz RC oscillator. More...
 
#define SYSCLK_SRC_RC32MHZ   CLK_SCLKSEL_RC32M_gc
 Internal 32 MHz RC oscillator. More...
 
#define SYSCLK_SRC_RC32KHZ   CLK_SCLKSEL_RC32K_gc
 Internal 32 KHz RC oscillator. More...
 
#define SYSCLK_SRC_XOSC   CLK_SCLKSEL_XOSC_gc
 External oscillator. More...
 
#define SYSCLK_SRC_PLL   CLK_SCLKSEL_PLL_gc
 Phase-Locked Loop. More...
 

Prescaler A Setting (relative to CLKsys)

#define SYSCLK_PSADIV_1   CLK_PSADIV_1_gc
 Do not prescale. More...
 
#define SYSCLK_PSADIV_2   CLK_PSADIV_2_gc
 Prescale CLKper4 by 2. More...
 
#define SYSCLK_PSADIV_4   CLK_PSADIV_4_gc
 Prescale CLKper4 by 4. More...
 
#define SYSCLK_PSADIV_8   CLK_PSADIV_8_gc
 Prescale CLKper4 by 8. More...
 
#define SYSCLK_PSADIV_16   CLK_PSADIV_16_gc
 Prescale CLKper4 by 16. More...
 
#define SYSCLK_PSADIV_32   CLK_PSADIV_32_gc
 Prescale CLKper4 by 32. More...
 
#define SYSCLK_PSADIV_64   CLK_PSADIV_64_gc
 Prescale CLKper4 by 64. More...
 
#define SYSCLK_PSADIV_128   CLK_PSADIV_128_gc
 Prescale CLKper4 by 128. More...
 
#define SYSCLK_PSADIV_256   CLK_PSADIV_256_gc
 Prescale CLKper4 by 256. More...
 
#define SYSCLK_PSADIV_512   CLK_PSADIV_512_gc
 Prescale CLKper4 by 512. More...
 

Prescaler B and C Setting (relative to CLKper4)

#define SYSCLK_PSBCDIV_1_1   CLK_PSBCDIV_1_1_gc
 Do not prescale. More...
 
#define SYSCLK_PSBCDIV_1_2   CLK_PSBCDIV_1_2_gc
 Prescale CLKper and CLKcpu by 2. More...
 
#define SYSCLK_PSBCDIV_4_1   CLK_PSBCDIV_4_1_gc
 Prescale CLKper2, CLKper and CLKcpu by 4. More...
 
#define SYSCLK_PSBCDIV_2_2   CLK_PSBCDIV_2_2_gc
 Prescale CLKper2 by 2, CLKper and CLKcpu by 4. More...
 

System Clock Port Numbers

enum  sysclk_port_id {
  SYSCLK_PORT_GEN,
  SYSCLK_PORT_A,
  SYSCLK_PORT_B,
  SYSCLK_PORT_C,
  SYSCLK_PORT_D,
  SYSCLK_PORT_E,
  SYSCLK_PORT_F
}
 

Clocks not associated with any port

Note
See the datasheet for available modules in the device.
#define SYSCLK_DMA   PR_DMA_bm
 DMA Controller. More...
 
#define SYSCLK_EDMA   PR_EDMA_bm
 EDMA Controller. More...
 
#define SYSCLK_EVSYS   PR_EVSYS_bm
 Event System. More...
 
#define SYSCLK_RTC   PR_RTC_bm
 Real-Time Counter. More...
 
#define SYSCLK_EBI   PR_EBI_bm
 Ext Bus Interface. More...
 
#define SYSCLK_AES   PR_AES_bm
 AES Module. More...
 
#define SYSCLK_USB   PR_USB_bm
 USB Module. More...
 
#define SYSCLK_XCL   PR_XCL_bm
 USB Module. More...
 

Clocks on PORTA and PORTB

Note
See the datasheet for available modules in the device.
#define SYSCLK_AC   PR_AC_bm
 Analog Comparator. More...
 
#define SYSCLK_ADC   PR_ADC_bm
 A/D Converter. More...
 
#define SYSCLK_DAC   PR_DAC_bm
 D/A Converter. More...
 

Clocks on PORTC, PORTD, PORTE and PORTF

Note
See the datasheet for available modules in the device.
#define SYSCLK_TC0   PR_TC0_bm
 Timer/Counter 0. More...
 
#define SYSCLK_TC1   PR_TC1_bm
 Timer/Counter 1. More...
 
#define SYSCLK_TC4   PR_TC4_bm
 Timer/Counter 0. More...
 
#define SYSCLK_TC5   PR_TC5_bm
 Timer/Counter 1. More...
 
#define SYSCLK_HIRES   PR_HIRES_bm
 Hi-Res Extension. More...
 
#define SYSCLK_SPI   PR_SPI_bm
 SPI controller. More...
 
#define SYSCLK_USART0   PR_USART0_bm
 USART 0. More...
 
#define SYSCLK_USART1   PR_USART1_bm
 USART 1. More...
 
#define SYSCLK_TWI   PR_TWI_bm
 TWI controller. More...
 

RTC clock source identifiers

#define SYSCLK_RTCSRC_ULP   CLK_RTCSRC_ULP_gc
 1kHz from internal ULP oscillator. More...
 
#define SYSCLK_RTCSRC_TOSC   CLK_RTCSRC_TOSC_gc
 1.024kHz from 32.768kHz crystal oscillator TOSC More...
 
#define SYSCLK_RTCSRC_RCOSC   CLK_RTCSRC_RCOSC_gc
 1.024kHz from 32.768kHz internal RC oscillator More...
 
#define SYSCLK_RTCSRC_TOSC32   CLK_RTCSRC_TOSC32_gc
 32.768kHz from crystal oscillator TOSC More...
 
#define SYSCLK_RTCSRC_RCOSC32   CLK_RTCSRC_RCOSC32_gc
 32.768kHz from internal RC oscillator More...
 
#define SYSCLK_RTCSRC_EXTCLK   CLK_RTCSRC_EXTCLK_gc
 External clock on TOSC1. More...
 

Querying the system clock and its derived clocks

static uint32_t sysclk_get_main_hz (void)
 Return the current rate in Hz of the main system clock. More...
 
static uint32_t sysclk_get_per4_hz (void)
 Return the current rate in Hz of clk_PER4. More...
 
static uint32_t sysclk_get_per2_hz (void)
 Return the current rate in Hz of clk_PER2. More...
 
static uint32_t sysclk_get_per_hz (void)
 Return the current rate in Hz of clk_PER. More...
 
static uint32_t sysclk_get_cpu_hz (void)
 Return the current rate in Hz of the CPU clock. More...
 
static uint32_t sysclk_get_peripheral_bus_hz (const volatile void *module)
 Retrieves the current rate in Hz of the Peripheral Bus clock attached to the specified peripheral. More...
 

Enabling and disabling synchronous clocks

void sysclk_enable_module (enum sysclk_port_id port, uint8_t id)
 Enable the clock to peripheral id on port port. More...
 
void sysclk_disable_module (enum sysclk_port_id port, uint8_t id)
 Disable the clock to peripheral id on port port. More...
 
static void sysclk_enable_peripheral_clock (const volatile void *module)
 Enable a peripheral's clock from its base address. More...
 
static void sysclk_disable_peripheral_clock (const volatile void *module)
 Disable a peripheral's clock from its base address. More...
 
static bool sysclk_module_is_enabled (enum sysclk_port_id port, uint8_t id)
 Check if the synchronous clock is enabled for a module. More...
 

System Clock Source and Prescaler configuration

static void sysclk_set_prescalers (uint8_t psadiv, uint8_t psbcdiv)
 Set system clock prescaler configuration. More...
 
static void sysclk_set_source (uint8_t src)
 Change the source of the main system clock. More...
 
static void sysclk_lock (void)
 Lock the system clock configuration. More...
 

RTC clock source control

static void sysclk_rtcsrc_enable (uint8_t id)
 Enable RTC clock with specified clock source. More...
 
static void sysclk_rtcsrc_disable (void)
 Disable RTC clock. More...
 

System Clock Initialization

void sysclk_init (void)
 Initialize the synchronous clock system. More...
 

#define SYSCLK_AC   PR_AC_bm
#define SYSCLK_ADC   PR_ADC_bm
#define SYSCLK_AES   PR_AES_bm
#define SYSCLK_DAC   PR_DAC_bm
#define SYSCLK_DMA   PR_DMA_bm
#define SYSCLK_EBI   PR_EBI_bm
#define SYSCLK_EDMA   PR_EDMA_bm
#define SYSCLK_EVSYS   PR_EVSYS_bm
#define SYSCLK_HIRES   PR_HIRES_bm
#define SYSCLK_PSADIV_1   CLK_PSADIV_1_gc

Do not prescale.

Referenced by sysclk_init().

#define SYSCLK_PSADIV_128   CLK_PSADIV_128_gc

Prescale CLKper4 by 128.

#define SYSCLK_PSADIV_16   CLK_PSADIV_16_gc

Prescale CLKper4 by 16.

#define SYSCLK_PSADIV_2   CLK_PSADIV_2_gc

Prescale CLKper4 by 2.

#define SYSCLK_PSADIV_256   CLK_PSADIV_256_gc

Prescale CLKper4 by 256.

#define SYSCLK_PSADIV_32   CLK_PSADIV_32_gc

Prescale CLKper4 by 32.

#define SYSCLK_PSADIV_4   CLK_PSADIV_4_gc

Prescale CLKper4 by 4.

#define SYSCLK_PSADIV_512   CLK_PSADIV_512_gc

Prescale CLKper4 by 512.

Referenced by sysclk_get_per4_hz().

#define SYSCLK_PSADIV_64   CLK_PSADIV_64_gc

Prescale CLKper4 by 64.

#define SYSCLK_PSADIV_8   CLK_PSADIV_8_gc

Prescale CLKper4 by 8.

#define SYSCLK_PSBCDIV_1_1   CLK_PSBCDIV_1_1_gc

Do not prescale.

Referenced by sysclk_get_per2_hz(), and sysclk_init().

#define SYSCLK_PSBCDIV_1_2   CLK_PSBCDIV_1_2_gc

Prescale CLKper and CLKcpu by 2.

Referenced by sysclk_get_per2_hz().

#define SYSCLK_PSBCDIV_2_2   CLK_PSBCDIV_2_2_gc

Prescale CLKper2 by 2, CLKper and CLKcpu by 4.

Referenced by sysclk_get_per2_hz().

#define SYSCLK_PSBCDIV_4_1   CLK_PSBCDIV_4_1_gc

Prescale CLKper2, CLKper and CLKcpu by 4.

Referenced by sysclk_get_per2_hz().

#define SYSCLK_RTC   PR_RTC_bm
#define SYSCLK_RTCSRC_EXTCLK   CLK_RTCSRC_EXTCLK_gc

External clock on TOSC1.

Referenced by sysclk_rtcsrc_enable().

#define SYSCLK_RTCSRC_RCOSC   CLK_RTCSRC_RCOSC_gc

1.024kHz from 32.768kHz internal RC oscillator

Referenced by sysclk_rtcsrc_enable().

#define SYSCLK_RTCSRC_RCOSC32   CLK_RTCSRC_RCOSC32_gc

32.768kHz from internal RC oscillator

Referenced by sysclk_rtcsrc_enable().

#define SYSCLK_RTCSRC_TOSC   CLK_RTCSRC_TOSC_gc

1.024kHz from 32.768kHz crystal oscillator TOSC

Referenced by sysclk_rtcsrc_enable().

#define SYSCLK_RTCSRC_TOSC32   CLK_RTCSRC_TOSC32_gc

32.768kHz from crystal oscillator TOSC

Referenced by sysclk_rtcsrc_enable().

#define SYSCLK_RTCSRC_ULP   CLK_RTCSRC_ULP_gc

1kHz from internal ULP oscillator.

Low precision

#define SYSCLK_SPI   PR_SPI_bm
#define SYSCLK_SRC_PLL   CLK_SCLKSEL_PLL_gc

Phase-Locked Loop.

Referenced by sysclk_get_main_hz(), and sysclk_init().

#define SYSCLK_SRC_RC2MHZ   CLK_SCLKSEL_RC2M_gc

Internal 2 MHz RC oscillator.

Referenced by sysclk_get_main_hz(), and sysclk_init().

#define SYSCLK_SRC_RC32KHZ   CLK_SCLKSEL_RC32K_gc

Internal 32 KHz RC oscillator.

Referenced by sysclk_get_main_hz(), and sysclk_init().

#define SYSCLK_SRC_RC32MHZ   CLK_SCLKSEL_RC32M_gc

Internal 32 MHz RC oscillator.

Referenced by sysclk_get_main_hz(), and sysclk_init().

#define SYSCLK_SRC_XOSC   CLK_SCLKSEL_XOSC_gc

External oscillator.

Referenced by sysclk_get_main_hz(), and sysclk_init().

#define SYSCLK_TC0   PR_TC0_bm
#define SYSCLK_TC1   PR_TC1_bm
#define SYSCLK_TC4   PR_TC4_bm
#define SYSCLK_TC5   PR_TC5_bm
#define SYSCLK_TWI   PR_TWI_bm
#define SYSCLK_USART0   PR_USART0_bm
#define SYSCLK_USART1   PR_USART1_bm
#define SYSCLK_USB   PR_USB_bm

USB Module.

#define SYSCLK_XCL   PR_XCL_bm

Enumerator
SYSCLK_PORT_GEN 

Devices not associated with a specific port.

SYSCLK_PORT_A 

Devices on PORTA.

SYSCLK_PORT_B 

Devices on PORTB.

SYSCLK_PORT_C 

Devices on PORTC.

SYSCLK_PORT_D 

Devices on PORTD.

SYSCLK_PORT_E 

Devices on PORTE.

SYSCLK_PORT_F 

Devices on PORTF.

void sysclk_disable_module ( enum sysclk_port_id  port,
uint8_t  id 
)

Disable the clock to peripheral id on port port.

Parameters
portID of the port to which the module is connected (one of the SYSCLK_PORT_* definitions).
idThe ID (bitmask) of the peripheral module to be disabled.

References cpu_irq_restore(), and cpu_irq_save().

Referenced by sysclk_disable_peripheral_clock(), and tc_disable().

static void sysclk_disable_peripheral_clock ( const volatile void *  module)
inlinestatic

Disable a peripheral's clock from its base address.

Disables the clock to a peripheral, given its base address. If the peripheral has an associated clock on the HSB bus, this will be disabled also.

Parameters
modulePointer to the module's base address.

References Assert, SYSCLK_AC, SYSCLK_ADC, SYSCLK_AES, SYSCLK_DAC, sysclk_disable_module(), SYSCLK_DMA, SYSCLK_EBI, SYSCLK_EDMA, SYSCLK_EVSYS, SYSCLK_HIRES, SYSCLK_PORT_A, SYSCLK_PORT_B, SYSCLK_PORT_C, SYSCLK_PORT_D, SYSCLK_PORT_E, SYSCLK_PORT_F, SYSCLK_PORT_GEN, SYSCLK_RTC, SYSCLK_SPI, SYSCLK_TC0, SYSCLK_TC1, SYSCLK_TC4, SYSCLK_TC5, SYSCLK_TWI, SYSCLK_USART0, SYSCLK_USART1, and SYSCLK_XCL.

void sysclk_enable_module ( enum sysclk_port_id  port,
uint8_t  id 
)

Enable the clock to peripheral id on port port.

Parameters
portID of the port to which the module is connected (one of the SYSCLK_PORT_* definitions).
idThe ID (bitmask) of the peripheral module to be enabled.

References cpu_irq_restore(), and cpu_irq_save().

Referenced by spi_master_init(), sysclk_enable_peripheral_clock(), tc_enable(), and usart_serial_init().

static void sysclk_enable_peripheral_clock ( const volatile void *  module)
inlinestatic

Enable a peripheral's clock from its base address.

Enables the clock to a peripheral, given its base address. If the peripheral has an associated clock on the HSB bus, this will be enabled also.

Parameters
modulePointer to the module's base address.

References Assert, SYSCLK_AC, SYSCLK_ADC, SYSCLK_AES, SYSCLK_DAC, SYSCLK_DMA, SYSCLK_EBI, SYSCLK_EDMA, sysclk_enable_module(), SYSCLK_EVSYS, SYSCLK_HIRES, SYSCLK_PORT_A, SYSCLK_PORT_B, SYSCLK_PORT_C, SYSCLK_PORT_D, SYSCLK_PORT_E, SYSCLK_PORT_F, SYSCLK_PORT_GEN, SYSCLK_RTC, SYSCLK_SPI, SYSCLK_TC0, SYSCLK_TC1, SYSCLK_TC4, SYSCLK_TC5, SYSCLK_TWI, SYSCLK_USART0, SYSCLK_USART1, and SYSCLK_XCL.

Referenced by usart_init_rs232(), and usart_init_spi().

static uint32_t sysclk_get_cpu_hz ( void  )
inlinestatic

Return the current rate in Hz of the CPU clock.

Returns
Frequency of the CPU clock, in Hz.

References sysclk_get_per_hz().

Referenced by spi_master_setup_device().

static uint32_t sysclk_get_main_hz ( void  )
inlinestatic

Return the current rate in Hz of the main system clock.

Todo:
This function assumes that the main clock source never changes once it's been set up, and that PLL0 always runs at the compile-time configured default rate. While this is probably the most common configuration, which we want to support as a special case for performance reasons, we will at some point need to support more dynamic setups as well.
Returns
Frequency of the main system clock, in Hz.

References CONFIG_SYSCLK_SOURCE, pll_get_default_rate, SYSCLK_SRC_PLL, SYSCLK_SRC_RC2MHZ, SYSCLK_SRC_RC32KHZ, SYSCLK_SRC_RC32MHZ, and SYSCLK_SRC_XOSC.

Referenced by sysclk_get_per4_hz().

static uint32_t sysclk_get_per2_hz ( void  )
inlinestatic

Return the current rate in Hz of clk_PER2.

This clock can run up to two times faster than the CPU clock.

Returns
Frequency of the clk_PER2 clock, in Hz.

References CONFIG_SYSCLK_PSBCDIV, sysclk_get_per4_hz(), SYSCLK_PSBCDIV_1_1, SYSCLK_PSBCDIV_1_2, SYSCLK_PSBCDIV_2_2, and SYSCLK_PSBCDIV_4_1.

Referenced by sysclk_get_per_hz(), and sysclk_get_peripheral_bus_hz().

static uint32_t sysclk_get_per4_hz ( void  )
inlinestatic

Return the current rate in Hz of clk_PER4.

This clock can run up to four times faster than the CPU clock.

Returns
Frequency of the clk_PER4 clock, in Hz.

References CONFIG_SYSCLK_PSADIV, sysclk_get_main_hz(), and SYSCLK_PSADIV_512.

Referenced by sysclk_get_per2_hz(), and sysclk_get_peripheral_bus_hz().

static uint32_t sysclk_get_per_hz ( void  )
inlinestatic

Return the current rate in Hz of clk_PER.

This clock always runs at the same rate as the CPU clock unless the divider is set.

Returns
Frequency of the clk_PER clock, in Hz.

References CONFIG_SYSCLK_PSBCDIV, and sysclk_get_per2_hz().

Referenced by sysclk_get_cpu_hz(), sysclk_get_peripheral_bus_hz(), tc_get_resolution(), tc_set_resolution(), usart_init_rs232(), and usart_init_spi().

static uint32_t sysclk_get_peripheral_bus_hz ( const volatile void *  module)
inlinestatic

Retrieves the current rate in Hz of the Peripheral Bus clock attached to the specified peripheral.

Parameters
modulePointer to the module's base address.
Returns
Frequency of the bus attached to the specified peripheral, in Hz.

References Assert, sysclk_get_per2_hz(), sysclk_get_per4_hz(), and sysclk_get_per_hz().

Referenced by tmr_init().

void sysclk_init ( void  )

Initialize the synchronous clock system.

This function will initialize the system clock and its source. This includes:

  • Mask all synchronous clocks except for any clocks which are essential for normal operation (for example internal memory clocks).
  • Set up the system clock prescalers as specified by the application's configuration file.
  • Enable the clock source specified by the application's configuration file (oscillator or PLL) and wait for it to become stable.
  • Set the main system clock source to the clock specified by the application's configuration file.

Since all non-essential peripheral clocks are initially disabled, it is the responsibility of the peripheral driver to re-enable any clocks that are needed for normal operation.

References Assert, ccp_write_io(), CONFIG_SYSCLK_PSADIV, CONFIG_SYSCLK_PSBCDIV, CONFIG_SYSCLK_SOURCE, LSB, MSB, osc_disable(), osc_enable(), osc_enable_autocalibration(), OSC_ID_RC2MHZ, OSC_ID_RC32KHZ, OSC_ID_RC32MHZ, OSC_ID_RC8MHZ, OSC_ID_USBSOF, OSC_ID_XOSC, osc_user_calibration(), osc_wait_ready(), pll_enable_config_defaults(), PLL_SRC_RC2MHZ, SYSCLK_PORT_F, SYSCLK_PSADIV_1, SYSCLK_PSBCDIV_1_1, sysclk_rtcsrc_enable(), sysclk_set_prescalers(), SYSCLK_SRC_PLL, SYSCLK_SRC_RC2MHZ, SYSCLK_SRC_RC32KHZ, SYSCLK_SRC_RC32MHZ, SYSCLK_SRC_XOSC, and UNUSED.

Referenced by main().

static void sysclk_lock ( void  )
inlinestatic

Lock the system clock configuration.

This function will lock the current system clock source and prescaler configuration, preventing any further changes.

References ccp_write_io().

static bool sysclk_module_is_enabled ( enum sysclk_port_id  port,
uint8_t  id 
)
inlinestatic

Check if the synchronous clock is enabled for a module.

Parameters
portID of the port to which the module is connected (one of the SYSCLK_PORT_* definitions).
idThe ID (bitmask) of the peripheral module to check (one of the SYSCLK_* module definitions).
Return values
trueIf the clock for module id on port is enabled.
falseIf the clock for module id on port is disabled.
static void sysclk_rtcsrc_disable ( void  )
inlinestatic

Disable RTC clock.

static void sysclk_rtcsrc_enable ( uint8_t  id)
inlinestatic

Enable RTC clock with specified clock source.

Parameters
idRTC clock source ID. Select from SYSCLK_RTCSRC_ULP, SYSCLK_RTCSRC_RCOSC, SYSCLK_RTCSRC_TOSC, SYSCLK_RTCSRC_RCOSC32, SYSCLK_RTCSRC_TOSC32 or SYSCLK_RTCSRC_EXTCLK

References Assert, osc_enable(), OSC_ID_RC32KHZ, OSC_ID_XOSC, osc_wait_ready(), SYSCLK_RTCSRC_EXTCLK, SYSCLK_RTCSRC_RCOSC, SYSCLK_RTCSRC_RCOSC32, SYSCLK_RTCSRC_TOSC, and SYSCLK_RTCSRC_TOSC32.

Referenced by sysclk_init().

static void sysclk_set_prescalers ( uint8_t  psadiv,
uint8_t  psbcdiv 
)
inlinestatic

Set system clock prescaler configuration.

This function will change the system clock prescaler configuration to match the parameters.

Note
The parameters to this function are device-specific.
Parameters
psadivThe prescaler A setting (one of the SYSCLK_PSADIV_* definitions). This determines the clkPER4 frequency.
psbcdivThe prescaler B and C settings (one of the SYSCLK_PSBCDIV_* definitions). These determine the clkPER2, clkPER and clkCPU frequencies.

References ccp_write_io().

Referenced by sysclk_init().

static void sysclk_set_source ( uint8_t  src)
inlinestatic

Change the source of the main system clock.

Parameters
srcThe new system clock source. Must be one of the constants from the System Clock Sources section.

References ccp_write_io().