Microchip® Advanced Software Framework

per_mode_common_utils.c File Reference

Common utilities for both Initiator and Receptor in PER Measurement mode - Performance Analyzer application.

Copyright (c) 2013-2018 Microchip Technology Inc. and its subsidiaries.

#include <stdio.h>
#include "tfa.h"
#include "tal.h"
#include "tal_internal.h"
#include "tal_constants.h"
#include "tal_helper.h"
#include "app_frame_format.h"
#include "app_init.h"
#include "perf_api.h"
#include "perf_api_serial_handler.h"

Macros

#define DEFAULT_FRAME_LENGTH   (20)
 
#define DEFAULT_NO_OF_TEST_FRAMES   (100)
 
#define LED_BLINK_COUNT_FOR_IDENTIFY   (20)
 

Functions

void app_reset (void)
 
void config_per_test_parameters (void)
 Function to set trx configure parameters. More...
 
void configure_pkt_stream_frames (uint16_t frame_len)
 Configure the frame to be used for Packet Streaming. More...
 
void dump_trx_register_values (uint16_t start_reg_addr, uint16_t end_reg_addr)
 Read a set of registers. More...
 
void led_blinker_timer_handler_cb (void *parameter)
 Timer Callback function if identify command is received on air by a node in reflector configuration. More...
 
void pkt_stream_gap_timer (void *parameter)
 Timer used in Packet Streaming Mode to add gap in between consecutive frames. More...
 
void pktstream_test (uint16_t gap_time, uint16_t timeout, bool start_stop, uint16_t frame_len)
 This function initiates packet streaming test. More...
 
void pulse_cw_transmission (void)
 
void read_trx_registers (uint16_t reg_addr)
 Read transceiver register. More...
 
void recover_all_settings (void)
 Recover all user settings before Start of CW transmission. More...
 
float reverse_float (const float float_val)
 The reverse_float is used for reversing a float variable for supporting BIG ENDIAN systems. More...
 
void rx_on_test (bool start_stop_param)
 This function is called to initiate the RX_ON test The transceiver is put into the RX_ON mode and no requests are handled until this mode is stopped. More...
 
void save_all_settings (void)
 Save all user settings before Start of CW transmission. More...
 
void start_cw_transmission (uint8_t tx_mode, uint16_t tmr_val)
 
void stop_cw_transmission (void *parameter)
 
void stop_pkt_streaming (void *parameter)
 This function is called to abort the packet streaming mode inprogress. More...
 
static void stop_pulse_cb (void *callback_parameter)
 Stop sending a CW signal on current channel page. More...
 
void write_trx_registers (uint16_t reg_addr, uint8_t reg_val)
 write Transceiver registers More...
 

Variables

static uint8_t ant_div_before_ct
 
static uint8_t ant_sel_before_ct
 
static uint8_t cc_band_ct
 
static uint8_t cc_number_ct
 
trx_config_params_t curr_trx_config_params
 
bool cw_ack_sent
 
uint8_t cw_start_mode
 
uint16_t cw_tmr_val
 
trx_config_params_t default_trx_config_params
 
uint8_t last_tx_power_format_set
 
bool peer_found
 
uint8_t pkt_buffer [LARGE_BUFFER_SIZE]
 
uint32_t pkt_stream_gap_time
 
bool pulse_mode
 
bool rdy_to_tx
 
bool remote_cw_start
 
bool remote_pulse_cw_start
 
bool remote_serial_tx_failure
 
bool rx_on_mode
 
frame_info_tstream_pkt
 

#define DEFAULT_FRAME_LENGTH   (20)
#define DEFAULT_NO_OF_TEST_FRAMES   (100)
#define LED_BLINK_COUNT_FOR_IDENTIFY   (20)

static void stop_pulse_cb ( void *  callback_parameter)
static

Stop sending a CW signal on current channel page.

Parameters
callback_parameterPointer to callback, not used here

References MAC_SUCCESS, op_mode, recover_all_settings(), tfa_continuous_tx_stop(), TX_OP_MODE, and usr_cont_pulse_tx_confirm().

Referenced by pulse_cw_transmission().

uint8_t ant_div_before_ct
static
uint8_t ant_sel_before_ct
static
uint8_t cc_band_ct
static
uint8_t cc_number_ct
static
uint8_t last_tx_power_format_set
uint8_t pkt_buffer[LARGE_BUFFER_SIZE]