Microchip® Advanced Software Framework

spi.c File Reference

SAM Serial Peripheral Interface Driver.

Copyright (c) 2012-2020 Microchip Technology Inc. and its subsidiaries.

#include "spi.h"

Functions

static enum status_code _spi_check_config (struct spi_module *const module, const struct spi_config *const config)
 
static enum status_code _spi_set_config (struct spi_module *const module, const struct spi_config *const config)
 
enum status_code spi_init (struct spi_module *const module, Sercom *const hw, const struct spi_config *const config)
 Initializes the SERCOM SPI module. More...
 
enum status_code spi_read_buffer_wait (struct spi_module *const module, uint8_t *rx_data, uint16_t length, uint16_t dummy)
 Reads buffer of length SPI characters. More...
 
void spi_reset (struct spi_module *const module)
 Resets the SPI module. More...
 
enum status_code spi_select_slave (struct spi_module *const module, struct spi_slave_inst *const slave, const bool select)
 Selects slave device. More...
 
enum status_code spi_set_baudrate (struct spi_module *const module, uint32_t baudrate)
 Set the baudrate of the SPI module. More...
 
enum status_code spi_transceive_buffer_wait (struct spi_module *const module, uint8_t *tx_data, uint8_t *rx_data, uint16_t length)
 Sends and receives a buffer of length SPI characters. More...
 
enum status_code spi_transceive_wait (struct spi_module *const module, uint16_t tx_data, uint16_t *rx_data)
 Sends and reads a single SPI character. More...
 
enum status_code spi_write_buffer_wait (struct spi_module *const module, const uint8_t *tx_data, uint16_t length)
 Sends a buffer of length SPI characters. More...
 

static enum status_code _spi_check_config ( struct spi_module *const  module,
const struct spi_config *const  config 
)
static

Checks an SPI config against current set config

This function will check that the config does not alter the configuration of the module. If the new config changes any setting, the initialization will be discarded.

Parameters
[in]modulePointer to the software instance struct
[in]configPointer to the configuration struct
Returns
The status of the configuration.
Return values
STATUS_ERR_INVALID_ARGIf invalid argument(s) were provided
STATUS_ERR_DENIEDIf configuration was different from previous
STATUS_OKIf the configuration was written

References _sercom_get_default_pad(), _sercom_get_sync_baud_val(), spi_slave_config::address, spi_slave_config::address_mask, spi_slave_config::address_mode, Assert, spi_master_config::baudrate, spi_config::character_size, spi_config::data_order, spi_slave_config::frame_format, spi_config::master, spi_config::mode, spi_config::mode_specific, spi_config::mux_setting, PINMUX_DEFAULT, spi_config::pinmux_pad0, spi_config::pinmux_pad1, spi_config::pinmux_pad2, spi_config::pinmux_pad3, PINMUX_UNUSED, spi_slave_config::preload_enable, spi_config::receiver_enable, spi_config::run_in_standby, SERCOM_GCLK_ID, spi_config::slave, SPI_MODE_MASTER, SPI_MODE_SLAVE, STATUS_ERR_DENIED, STATUS_ERR_INVALID_ARG, STATUS_OK, system_gclk_chan_get_hz(), system_pinmux_pin_get_mux_position(), and spi_config::transfer_mode.

Referenced by spi_init().

static enum status_code _spi_set_config ( struct spi_module *const  module,
const struct spi_config *const  config 
)
static