Microchip® Advanced Software Framework

result_rsp_t Struct Reference

Result response frame structure to send the results of the PER test.

#include <app_frame_format.h>

Data Fields

uint32_t frames_with_wrong_crc
 
uint32_t lqi_avrg_rx
 
uint32_t num_of_frames_rx
 
uint32_t rssi_avrg_rx
 

uint32_t result_rsp_t::frames_with_wrong_crc
uint32_t result_rsp_t::lqi_avrg_rx
uint32_t result_rsp_t::num_of_frames_rx
uint32_t result_rsp_t::rssi_avrg_rx