Includes IEEE Constant Definitions.
Macros | |
#define | aBaseSlotDuration (60) |
The number of symbols forming a superframe slot when the superframe order is equal to 0. More... | |
#define | aBaseSuperframeDuration |
The number of symbols forming a superframe when the superframe order is equal to 0. More... | |
#define | ACK_PAYLOAD_LEN (0x03) |
Length (in octets) of ACK payload. More... | |
#define | aGTSDescPersistenceTime (4) |
The number of superframes in which a GTS descriptor exists in the beacon frame of a PAN coordinator. More... | |
#define | aMaxBeaconOverhead (75) |
The maximum number of octets added by the MAC sublayer to the payload of its beacon frame. More... | |
#define | aMaxBeaconPayloadLength (aMaxPHYPacketSize - aMaxBeaconOverhead) |
The maximum size, in octets, of a beacon payload. More... | |
#define | aMaxLostBeacons (4) |
The number of consecutive lost beacons that will cause the MAC sublayer of a receiving device to declare a loss of synchronization. More... | |
#define | aMaxMACPayloadSize (aMaxPHYPacketSize - aMinMPDUOverhead) |
The maximum number of octets that can be transmitted in the MAC Payload field. More... | |
#define | aMaxMACSafePayloadSize |
The maximum number of octets that can be transmitted in the MAC Payload field of an unsecured MAC frame that will be guaranteed not to exceed aMaxPHYPacketSize. More... | |
#define | aMaxMPDUUnsecuredOverhead (25) |
The maximum number of octets added by the MAC sublayer to the PSDU without security. More... | |
#define | aMaxPHYPacketSize (127) |
Maximum size of PHY packet. More... | |
#define | aMaxSIFSFrameSize (18) |
The maximum size of an MPDU, in octets, that can be followed by a SIFS period. More... | |
#define | aMinCAPLength (440) |
The minimum number of symbols forming the CAP. More... | |
#define | aMinMPDUOverhead (9) |
The minimum number of octets added by the MAC sublayer to the PSDU. More... | |
#define | aNumSuperframeSlots (16) |
The number of slots contained in any superframe. More... | |
#define | ASSOC_PERMIT_BIT_POS (15) |
Association permit bit position. More... | |
#define | ASSOCIATION_RESERVED (3) |
Association status code value (see wpan_mlme_associate_resp()). More... | |
#define | ASSOCIATION_SUCCESSFUL (0) |
Association status code value (see wpan_mlme_associate_resp()). More... | |
#define | aTurnaroundTime (12) |
Maximum turnaround Time of the radio to switch from Rx to Tx or Tx to Rx in symbols. More... | |
#define | aUnitBackoffPeriod (20) |
The number of symbols forming the basic time period used by the CSMA-CA algorithm. More... | |
#define | BATT_LIFE_EXT_BIT_POS (12) |
Battery life extention bit position. More... | |
#define | BROADCAST (0xFFFF) |
Generic 16 bit broadcast address. More... | |
#define | CLEAR_ADDR_64 (0ULL) |
Unused EUI-64 address. More... | |
#define | CONV_DBM_TO_phyTransmitPower(dbm_value) |
Converts a dBm value to a phyTransmitPower value. More... | |
#define | CONV_phyTransmitPower_TO_DBM(phyTransmitPower_value) |
Converts a phyTransmitPower value to a dBm value. More... | |
#define | ED_VAL_LEN (1) |
Length of the ED value parameter number field. More... | |
#define | EXT_ADDR_LEN (8) |
Length (in octets) of extended address. More... | |
#define | FCF1_FV_2003 (0) |
The mask for a IEEE 802.15.4-2003 compatible frame in the frame version subfield fcf1. More... | |
#define | FCF1_FV_2006 (1) |
The mask for a IEEE 802.15.4-2006 compatible frame in the frame version subfield fcf1. More... | |
#define | FCF1_FV_2012 (2) |
The mask for a IEEE 802.15.4e-2012 compatible frame in the frame version subfield fcf1. More... | |
#define | FCF1_FV_MASK (3 << FCF1_FV_SHIFT) |
The mask for the frame version subfield fcf1. More... | |
#define | FCF1_FV_SHIFT (4) |
Shift value for the frame version subfield fcf1. More... | |
#define | FCF_2_DEST_ADDR_OFFSET (2) |
Offset of Destination Addressing Mode of octet two of MHR. More... | |
#define | FCF_2_SOURCE_ADDR_OFFSET (6) |
Offset of Source Addressing Mode of octet two of MHR. More... | |
#define | FCF_ACK_REQUEST (1 << 5) |
The mask for the ACK request bit of the FCF. More... | |
#define | FCF_DEST_ADDR_OFFSET (10) |
Defines the offset of the destination address. More... | |
#define | FCF_FRAME_PENDING (1 << 4) |
The mask for the frame pending bit of the FCF. More... | |
#define | FCF_FRAME_VERSION_2003 (0 << 12) |
The mask for a IEEE 802.15.4-2003 compatible frame in the frame version subfield. More... | |
#define | FCF_FRAME_VERSION_2006 (1 << 12) |
The mask for a IEEE 802.15.4-2006 compatible frame in the frame version subfield. More... | |
#define | FCF_FRAME_VERSION_2012 (2 << 12) |
The mask for a IEEE 802.15.4e-2012 compatible frame in the frame version subfield. More... | |
#define | FCF_FRAMETYPE_ACK (0x02) |
Define the ACK frame type. More... | |
#define | FCF_FRAMETYPE_BEACON (0x00) |
Defines the beacon frame type. More... | |
#define | FCF_FRAMETYPE_DATA (0x01) |
Define the data frame type. More... | |
#define | FCF_FRAMETYPE_LLDN (0x04) |
Define the LLDN frame type. More... | |
#define | FCF_FRAMETYPE_MAC_CMD (0x03) |
Define the command frame type. More... | |
#define | FCF_FRAMETYPE_MASK (0x07) |
Defines a mask for the frame type. More... | |
#define | FCF_FRAMETYPE_MP (0x05) |
Define the multipurpose frame type. More... | |
#define | FCF_GET_FRAMETYPE(x) ((x) & FCF_FRAMETYPE_MASK) |
Macro to get the frame type. More... | |
#define | FCF_LEN (2) |
Length (in octets) of FCF. More... | |
#define | FCF_LONG_ADDR (0x03) |
Address Mode: LONG. More... | |
#define | FCF_NO_ADDR (0x00) |
Address Mode: NO ADDRESS. More... | |
#define | FCF_PAN_ID_COMPRESSION (1 << 6) |
The mask for the PAN ID compression bit of the FCF. More... | |
#define | FCF_RESERVED_ADDR (0x01) |
Address Mode: RESERVED. More... | |
#define | FCF_SECURITY_ENABLED (1 << 3) |
The mask for the security enable bit of the FCF. More... | |
#define | FCF_SET_DEST_ADDR_MODE(x) |
Macro to set the destination address mode. More... | |
#define | FCF_SET_FRAMETYPE(x) (x) |
A macro to set the frame type. More... | |
#define | FCF_SET_SOURCE_ADDR_MODE(x) |
Macro to set the source address mode. More... | |
#define | FCF_SHORT_ADDR (0x02) |
Address Mode: SHORT. More... | |
#define | FCF_SOURCE_ADDR_OFFSET (14) |
Defines the offset of the source address. More... | |
#define | FCS_LEN (2) |
Length (in octets) of FCS. More... | |
#define | INVALID_SHORT_ADDRESS (0xFFFF) |
Invalid short address. More... | |
#define | INVERSE_CHANNEL_MASK (~VALID_CHANNEL_MASK) |
Inverse channel masks for scanning. More... | |
#define | LENGTH_FIELD_LEN (1) |
Size of the length parameter. More... | |
#define | LQI_LEN (1) |
Length of the LQI number field. More... | |
#define | MAC_NO_SHORT_ADDR_VALUE (0xFFFE) |
MAC is using long address (by now). More... | |
#define | macAckWaitDuration (0x40) |
The maximum number of symbols to wait for an acknowledgment frame to arrive following a transmitted data frame. More... | |
#define | macAssociatedPANCoord (0x56) |
Indication of whether the device is associated to the PAN through the PAN coordinator. More... | |
#define | macAssociatedPANCoord_def (false) |
Default value for PIB macAssociatedPANCoord. More... | |
#define | macAssociationPermit (0x41) |
Indication of whether a coordinator is currently allowing association. More... | |
#define | macAssociationPermit_def (false) |
Default value for PIB macAssociationPermit. More... | |
#define | macAutoRequest (0x42) |
Indication of whether a device automatically sends a data request command if its address is listed in the beacon frame. More... | |
#define | macAutoRequest_def (true) |
Default value for PIB macAutoRequest. More... | |
#define | macBattLifeExt (0x43) |
Indication of whether battery life extension, by reduction of coordinator receiver operation time during the CAP, is enabled. More... | |
#define | macBattLifeExt_def (false) |
Default value for PIB macBattLifeExt. More... | |
#define | macBattLifeExtPeriods (0x44) |
The number of backoff periods during which the receiver is enabled following a beacon in battery life extension mode. More... | |
#define | macBattLifeExtPeriods_def (6) |
Default value for PIB macBattLifeExtPeriods. More... | |
#define | macBeaconOrder (0x47) |
Specification of how often the coordinator transmits a beacon. More... | |
#define | macBeaconOrder_def (15) |
Default value for PIB macBeaconOrder. More... | |
#define | macBeaconPayload (0x45) |
The contents of the beacon payload. More... | |
#define | macBeaconPayloadLength (0x46) |
The length, in octets, of the beacon payload. More... | |
#define | macBeaconPayloadLength_def (0) |
Default value for PIB macBeaconPayloadLength. More... | |
#define | macBeaconTxTime (0x48) |
The time that the device transmitted its last beacon frame, in symbol periods. More... | |
#define | macBeaconTxTime_def (0x000000) |
Default value for PIB macBeaconTxTime. More... | |
#define | macBSN (0x49) |
The sequence number added to the transmitted beacon frame. More... | |
#define | macCoordExtendedAddress (0x4A) |
The 64 bit address of the coordinator with which the device is associated. More... | |
#define | macCoordShortAddress (0x4B) |
The 16 bit short address assigned to the coordinator with which the device is associated. More... | |
#define | macCoordShortAddress_def (0xFFFF) |
Default value for PIB macCoordShortAddress. More... | |
#define | macDSN (0x4C) |
The sequence number added to the transmitted data or MAC command frame. More... | |
#define | macGTSPermit (0x4D) |
macGTSPermit is true if the PAN coordinator is to accept GTS requests, false otherwise. More... | |
#define | macGTSPermit_def (true) |
Default value for PIB macGTSPermit. More... | |
#define | macIeeeAddress (0xF0) |
Private MAC PIB attribute to allow setting the MAC address in test mode. More... | |
#define | macMaxBE (0x57) |
The maximum value of the backoff exponent, BE, in the CSMA-CA algorithm. More... | |
#define | macMaxCSMABackoffs (0x4E) |
The maximum number of backoffs the CSMA-CA algorithm will attempt before declaring a channel access failure. More... | |
#define | macMaxCSMABackoffs_def (4) |
Default value for PIB macMaxCSMABackoffs. More... | |
#define | macMaxFrameRetries (0x59) |
The maximum number of retries allowed after a transmission failure. More... | |
#define | macMaxFrameTotalWaitTime (0x58) |
The maximum number of CAP symbols in a beaconenabled PAN, or symbols in a nonbeacon-enabled PAN, to wait either for a frame intended as a response to a data request frame or for a broadcast frame following a beacon with the Frame Pending subfield set to one. More... | |
#define | macMaxNumRxFramesDuringBackoff (0x7F) |
Private MAC PIB attribute to control the CSMA algorithm. More... | |
#define | macMinBE (0x4F) |
The minimum value of the backoff exponent in the CSMA-CA algorithm. More... | |
#define | macMinLIFSPeriod (0x5E) |
The minimum number of symbols forming a LIFS period. More... | |
#define | macMinLIFSPeriod_def (40) |
Default value for PIB macMinLIFSPeriod. More... | |
#define | macMinSIFSPeriod (0x5F) |
The minimum number of symbols forming a SIFS period. More... | |
#define | macMinSIFSPeriod_def (12) |
Default value for PIB macMinSIFSPeriod. More... | |
#define | macPANCoordExtendedAddress (0x7D) |
The 64-bit address of the PAN coordinator. More... | |
#define | macPANCoordShortAddress (0x7E) |
The 16-bit short address assinged to the PAN coordinator. More... | |
#define | macPANId (0x50) |
The 16 bit identifier of the PAN on which the device is operating. More... | |
#define | macPANId_def (0xFFFF) |
Default value for PIB macPANId. More... | |
#define | macPromiscuousMode (0x51) |
This indicates whether the MAC sublayer is in a promiscuous (receive all) mode. More... | |
#define | macResponseWaitTime (0x5A) |
The maximum time, in multiples of aBaseSuperframeDuration, a device shall wait for a response command frame to be available following a request command frame. More... | |
#define | macResponseWaitTime_def (32 * aBaseSuperframeDuration) |
Default value for PIB macResponseWaitTime. More... | |
#define | macRxOnWhenIdle (0x52) |
This indicates whether the MAC sublayer is to enable its receiver during idle periods. More... | |
#define | macRxOnWhenIdle_def (false) |
Default value for PIB macRxOnWhenIdle. More... | |
#define | macSecurityEnabled (0x5D) |
Indication of whether the MAC sublayer has security enabled. More... | |
#define | macSecurityEnabled_def (false) |
Default value for PIB macSecurityEnabled. More... | |
#define | macShortAddress (0x53) |
The 16 bit address that the device uses to communicate in the PAN. More... | |
#define | macShortAddress_def (0xFFFF) |
Default value for PIB macShortAddress. More... | |
#define | macSuperframeOrder (0x54) |
This specifies the length of the active portion of the superframe, including the beacon frame. More... | |
#define | macSuperframeOrder_def (15) |
Default value for PIB macSuperframeOrder. More... | |
#define | macSyncSymbolOffset (0x5B) |
The offset, measured in symbols, between the symbol boundary at which the MLME captures the timestamp of each transmitted or received frame, and the onset of the first symbol past the SFD, namely, the first symbol of the Length field. More... | |
#define | macTimestampSupported (0x5C) |
Indication of whether the MAC sublayer supports the optional timestamping feature for incoming and outgoing data frames. More... | |
#define | macTransactionPersistenceTime (0x55) |
The maximum time (in superframe periods) that a transaction is stored by a coordinator and indicated in its beacon. More... | |
#define | macTransactionPersistenceTime_def (0x01F4) |
Default value for PIB macTransactionPersistenceTime. More... | |
#define | MAX_KEY_ID_FIELD_LEN (9) |
Maximum length of the key id field. More... | |
#define | MAX_MGMT_FRAME_LENGTH (30) |
Maximum size of the management frame(Association Response frame) More... | |
#define | MIN_FRAME_LENGTH (8) |
Minimum size of a valid frame other than an Ack frame. More... | |
#define | MLME_SCAN_TYPE_ACTIVE (0x01) |
Active scan (see wpan_mlme_scan_req()) More... | |
#define | MLME_SCAN_TYPE_ED (0x00) |
Energy scan (see wpan_mlme_scan_req()) More... | |
#define | MLME_SCAN_TYPE_ORPHAN (0x03) |
Orphan scan (see wpan_mlme_scan_req()) More... | |
#define | MLME_SCAN_TYPE_PASSIVE (0x02) |
Passive scan (see wpan_mlme_scan_req()) More... | |
#define | NO_PIB_INDEX (0) |
#define | NON_BEACON_NWK (0x0F) |
BO value for nonbeacon-enabled network. More... | |
#define | NUM_LONG_PEND_ADDR(x) (((x) & 0x70) >> 4) |
Mask for the number of long addresses pending. More... | |
#define | NUM_SHORT_PEND_ADDR(x) ((x) & 0x07) |
Mask for the number of short addresses pending. More... | |
#define | PAN_ACCESS_DENIED (2) |
Association status code value (see wpan_mlme_associate_resp()). More... | |
#define | PAN_AT_CAPACITY (1) |
Association status code value (see wpan_mlme_associate_resp()). More... | |
#define | PAN_COORD_BIT_POS (14) |
PAN coordinator bit position. More... | |
#define | PAN_ID_LEN (2) |
Length (in octets) of PAN ID. More... | |
#define | PL_POS_DST_ADDR_START (6) |
Octet start position of Destination Address field within payload array of frame_info_t. More... | |
#define | PL_POS_DST_PAN_ID_START (4) |
Octet start position of Destination PAN-Id field within payload array of frame_info_t. More... | |
#define | PL_POS_FCF_1 (1) |
Octet position of FCF octet one within payload array of frame_info_t. More... | |
#define | PL_POS_FCF_2 (2) |
Octet position of FCF octet two within payload array of frame_info_t. More... | |
#define | PL_POS_SEQ_NUM (3) |
Octet position of Sequence Number octet within payload array of frame_info_t. More... | |
#define | SEQ_NUM_LEN (1) |
Length of the sequence number field. More... | |
#define | SHORT_ADDR_LEN (2) |
Length (in octets) of short address. More... | |
#define | WPAN_TXOPT_ACK (0x01) |
Value for TxOptions parameter in wpan_mcps_data_req(). More... | |
#define | WPAN_TXOPT_GTS (0x02) |
Value for TxOptions parameter in wpan_mcps_data_req(). More... | |
#define | WPAN_TXOPT_GTS_ACK (0x03) |
Value for TxOptions parameter in wpan_mcps_data_req(). More... | |
#define | WPAN_TXOPT_INDIRECT (0x04) |
Value for TxOptions parameter in wpan_mcps_data_req(). More... | |
#define | WPAN_TXOPT_INDIRECT_ACK (0x05) |
Value for TxOptions parameter in wpan_mcps_data_req(). More... | |
#define | WPAN_TXOPT_OFF (0x00) |
Value for TxOptions parameter in wpan_mcps_data_req(). More... | |
Typedefs | |
typedef enum cca_mode_tag | cca_mode_t |
CCA mode enumeration. More... | |
typedef enum ch_pg_tag | ch_pg_t |
typedef enum trx_cca_mode_tag | trx_cca_mode_t |
CCA Modes of the transceiver. More... | |
Enumerations | |
enum | cca_mode_tag { CCA_MODE_0_CS_OR_ED = 0, CCA_MODE_1_ED = 1, CCA_MODE_2_CS, CCA_MODE_3_CS_ED, CCA_MODE_4_ALOHA } |
CCA mode enumeration. More... | |
enum | ch_pg_tag { CH_PG_2003 = 0, CH_PG_2006 = 2, CH_PG_CHINA = 5, CH_PG_JAPAN = 6, CH_PG_MSK = 7, CH_PG_LRP_UWB = 8, CH_PG_SUN = 9, CH_PG_GENERIC_PHY = 10, CH_PG_16 = 16, CH_PG_18 = 18, CH_PG_INVALID = 0xFF } |
enum | trx_cca_mode_tag { TRX_CCA_MODE0 = 0, TRX_CCA_MODE1 = 1, TRX_CCA_MODE2 = 2, TRX_CCA_MODE3 = 3 } |
#define | phyCurrentChannel (0x00) |
The RF channel to use for all following transmissions and receptions. More... | |
#define | phyChannelsSupported (0x01) |
The 5 most significant bits (MSBs) (b27, ..., b31) of phyChannelsSupported shall be reserved and set to 0, and the 27 LSBs (b0, b1, ..., b26) shall indicate the status (1 = available, 0 = unavailable) for each of the 27 valid channels (bk shall indicate the status of channel k). More... | |
#define | phyTransmitPower (0x02) |
The 2 MSBs represent the tolerance on the transmit power: 00 = 1 dB 01 = 3 dB 10 = 6 dB The 6 LSBs represent a signed integer in twos-complement format, corresponding to the nominal transmit power of the device in decibels relative to 1 mW. More... | |
#define | phyCCAMode (0x03) |
The CCA mode. More... | |
#define | phyCurrentPage (0x04) |
This is the current PHY channel page. More... | |
#define | phyMaxFrameDuration (0x05) |
The maximum number of symbols in a frame: = phySHRDuration + ceiling([aMaxPHYPacketSize + 1] x phySymbolsPerOctet) More... | |
#define | phySHRDuration (0x06) |
The duration of the synchronization header (SHR) in symbols for the current PHY. More... | |
#define | phySymbolsPerOctet (0x07) |
The number of symbols per octet for the current PHY. More... | |
#define | PHY_OVERHEAD (5) |
Number of octets added by the PHY: 4 sync octets + SFD octet. More... | |
enum | phy_enum_tag { PHY_BUSY = (0x00), PHY_BUSY_RX = (0x01), PHY_BUSY_TX = (0x02), PHY_FORCE_TRX_OFF = (0x03), PHY_IDLE = (0x04), PHY_INVALID_PARAMETER = (0x05), PHY_RX_ON = (0x06), PHY_SUCCESS = (0x07), PHY_TRX_OFF = (0x08), PHY_TX_ON = (0x09), PHY_UNSUPPORTED_ATTRIBUTE = (0x0A), PHY_READ_ONLY = (0x0B) } |
typedef enum phy_enum_tag | phy_enum_t |
#define | PHY_SUCCESS_DATA_PENDING (0x10) |
PHY_SUCCESS in phyAutoCSMACA when received ACK frame had the pending bit set. More... | |
#define | ED_SAMPLE_DURATION_SYM (8) |
ED scan/sampling duration. More... | |
#define aBaseSlotDuration (60) |
The number of symbols forming a superframe slot when the superframe order is equal to 0.
#define aBaseSuperframeDuration |
The number of symbols forming a superframe when the superframe order is equal to 0.
Referenced by start_ed_scan().
#define ACK_PAYLOAD_LEN (0x03) |
Length (in octets) of ACK payload.
Referenced by process_incoming_frame(), and tx_done_handling().
#define aGTSDescPersistenceTime (4) |
The number of superframes in which a GTS descriptor exists in the beacon frame of a PAN coordinator.
#define aMaxBeaconOverhead (75) |
The maximum number of octets added by the MAC sublayer to the payload of its beacon frame.
#define aMaxBeaconPayloadLength (aMaxPHYPacketSize - aMaxBeaconOverhead) |
The maximum size, in octets, of a beacon payload.
#define aMaxLostBeacons (4) |
The number of consecutive lost beacons that will cause the MAC sublayer of a receiving device to declare a loss of synchronization.
#define aMaxMACPayloadSize (aMaxPHYPacketSize - aMinMPDUOverhead) |
The maximum number of octets that can be transmitted in the MAC Payload field.
#define aMaxMACSafePayloadSize |
The maximum number of octets that can be transmitted in the MAC Payload field of an unsecured MAC frame that will be guaranteed not to exceed aMaxPHYPacketSize.
#define aMaxMPDUUnsecuredOverhead (25) |
The maximum number of octets added by the MAC sublayer to the PSDU without security.
#define aMaxPHYPacketSize (127) |
Maximum size of PHY packet.
Referenced by set_phy_frame_length().
#define aMaxSIFSFrameSize (18) |
The maximum size of an MPDU, in octets, that can be followed by a SIFS period.
Referenced by send_frame().
#define aMinCAPLength (440) |
The minimum number of symbols forming the CAP.
This ensures that MAC commands can still be transferred to devices when GTSs are being used. An exception to this minimum shall be allowed for the accommodation of the temporary increase in the beacon frame length needed to perform GTS maintenance (see 7.2.2.1.3).
#define aMinMPDUOverhead (9) |
The minimum number of octets added by the MAC sublayer to the PSDU.
#define aNumSuperframeSlots (16) |
The number of slots contained in any superframe.
#define ASSOC_PERMIT_BIT_POS (15) |
Association permit bit position.
#define ASSOCIATION_RESERVED (3) |
Association status code value (see wpan_mlme_associate_resp()).
#define ASSOCIATION_SUCCESSFUL (0) |
Association status code value (see wpan_mlme_associate_resp()).
#define aTurnaroundTime (12) |
Maximum turnaround Time of the radio to switch from Rx to Tx or Tx to Rx in symbols.
Referenced by tx_done_handling().
#define aUnitBackoffPeriod (20) |
The number of symbols forming the basic time period used by the CSMA-CA algorithm.
Referenced by tal_tx_frame().
#define BATT_LIFE_EXT_BIT_POS (12) |
Battery life extention bit position.
#define BROADCAST (0xFFFF) |
Generic 16 bit broadcast address.
Referenced by send_peer_req().
#define CLEAR_ADDR_64 (0ULL) |
Unused EUI-64 address.
#define CONV_DBM_TO_phyTransmitPower | ( | dbm_value | ) |
Converts a dBm value to a phyTransmitPower value.
dbm_value | dBm value |
Referenced by limit_tx_pwr(), recover_all_settings(), set_default_tx_pwr(), set_paramter_on_recptor_node(), and set_tx_power().
#define CONV_phyTransmitPower_TO_DBM | ( | phyTransmitPower_value | ) |
Converts a phyTransmitPower value to a dBm value.
phyTransmitPower_value | phyTransmitPower value |
Referenced by config_per_test_parameters(), convert_phyTransmitPower_to_reg_value(), limit_tx_pwr(), perf_get_req(), set_channel(), set_channel_page(), set_default_tx_pwr(), and set_parameter_on_transmitter_node().
#define ED_SAMPLE_DURATION_SYM (8) |
ED scan/sampling duration.
Referenced by tal_ed_start(), and tfa_ed_sample().
#define ED_VAL_LEN (1) |
Length of the ED value parameter number field.
Referenced by handle_received_frame_irq(), per_mode_initiator_rx_cb(), per_mode_receptor_rx_cb(), and wait_for_event_rx_cb().
#define EXT_ADDR_LEN (8) |
Length (in octets) of extended address.
Referenced by transmit_frame(), and usr_perf_start_confirm().
#define FCF1_FV_2003 (0) |
The mask for a IEEE 802.15.4-2003 compatible frame in the frame version subfield fcf1.
#define FCF1_FV_2006 (1) |
The mask for a IEEE 802.15.4-2006 compatible frame in the frame version subfield fcf1.
#define FCF1_FV_2012 (2) |
The mask for a IEEE 802.15.4e-2012 compatible frame in the frame version subfield fcf1.
#define FCF1_FV_MASK (3 << FCF1_FV_SHIFT) |
The mask for the frame version subfield fcf1.
#define FCF1_FV_SHIFT (4) |
Shift value for the frame version subfield fcf1.
#define FCF_2_DEST_ADDR_OFFSET (2) |
Offset of Destination Addressing Mode of octet two of MHR.
#define FCF_2_SOURCE_ADDR_OFFSET (6) |
Offset of Source Addressing Mode of octet two of MHR.
Referenced by transmit_frame().
#define FCF_ACK_REQUEST (1 << 5) |
The mask for the ACK request bit of the FCF.
Referenced by configure_frame_sending(), configure_range_test_frame_sending(), process_incoming_frame(), transmit_frame(), and tx_done_handling().
#define FCF_DEST_ADDR_OFFSET (10) |
Defines the offset of the destination address.
#define FCF_FRAME_PENDING (1 << 4) |
The mask for the frame pending bit of the FCF.
#define FCF_FRAME_VERSION_2003 (0 << 12) |
The mask for a IEEE 802.15.4-2003 compatible frame in the frame version subfield.
#define FCF_FRAME_VERSION_2006 (1 << 12) |
The mask for a IEEE 802.15.4-2006 compatible frame in the frame version subfield.
#define FCF_FRAME_VERSION_2012 (2 << 12) |
The mask for a IEEE 802.15.4e-2012 compatible frame in the frame version subfield.
#define FCF_FRAMETYPE_ACK (0x02) |
Define the ACK frame type.
(Table 65 IEEE 802.15.4 Specification)
#define FCF_FRAMETYPE_BEACON (0x00) |
Defines the beacon frame type.
(Table 65 IEEE 802.15.4 Specification)
Referenced by process_incoming_frame().
#define FCF_FRAMETYPE_DATA (0x01) |
Define the data frame type.
(Table 65 IEEE 802.15.4 Specification)
Referenced by configure_frame_sending(), configure_range_test_frame_sending(), and transmit_frame().
#define FCF_FRAMETYPE_LLDN (0x04) |
Define the LLDN frame type.
See 802.15.4e-2012
#define FCF_FRAMETYPE_MAC_CMD (0x03) |
Define the command frame type.
(Table 65 IEEE 802.15.4 Specification)
#define FCF_FRAMETYPE_MASK (0x07) |
Defines a mask for the frame type.
(Table 65 IEEE 802.15.4 Specification)
Referenced by process_incoming_frame().
#define FCF_FRAMETYPE_MP (0x05) |
Define the multipurpose frame type.
See 802.15.4e-2012
#define FCF_GET_FRAMETYPE | ( | x | ) | ((x) & FCF_FRAMETYPE_MASK) |
Macro to get the frame type.
#define FCF_LEN (2) |
Length (in octets) of FCF.
Referenced by configure_frame_sending(), configure_pkt_stream_frames(), configure_range_test_frame_sending(), and transmit_frame().
#define FCF_LONG_ADDR (0x03) |
Address Mode: LONG.
Referenced by send_peer_req(), send_peer_rsp(), and transmit_frame().
#define FCF_NO_ADDR (0x00) |
Address Mode: NO ADDRESS.
#define FCF_PAN_ID_COMPRESSION (1 << 6) |
The mask for the PAN ID compression bit of the FCF.
Referenced by configure_frame_sending(), configure_pkt_stream_frames(), configure_range_test_frame_sending(), and transmit_frame().
#define FCF_RESERVED_ADDR (0x01) |
Address Mode: RESERVED.
#define FCF_SECURITY_ENABLED (1 << 3) |
The mask for the security enable bit of the FCF.
#define FCF_SET_DEST_ADDR_MODE | ( | x | ) |
Macro to set the destination address mode.
Referenced by configure_frame_sending(), configure_pkt_stream_frames(), configure_range_test_frame_sending(), and transmit_frame().
#define FCF_SET_FRAMETYPE | ( | x | ) | (x) |
A macro to set the frame type.
#define FCF_SET_SOURCE_ADDR_MODE | ( | x | ) |
Macro to set the source address mode.
Referenced by configure_frame_sending(), configure_pkt_stream_frames(), configure_range_test_frame_sending(), and transmit_frame().
#define FCF_SHORT_ADDR (0x02) |
Address Mode: SHORT.
Referenced by configure_frame_sending(), configure_pkt_stream_frames(), configure_range_test_frame_sending(), range_test_frame_tx(), send_crc_set_req(), send_crc_status_req(), send_crc_status_rsp(), send_disconnect_command(), send_diversity_set_req(), send_diversity_status_req(), send_diversity_status_rsp(), send_identify_command(), send_parameters_changed(), send_peer_conf(), send_peer_info_req(), send_peer_info_rsp(), send_peer_req(), send_peer_rsp(), send_per_test_start_cmd(), send_range_test_marker_cmd(), send_range_test_marker_rsp(), send_range_test_rsp(), send_range_test_start_cmd(), send_range_test_stop_cmd(), send_remote_cmd(), send_remote_reply_cmd(), send_result_req(), send_result_rsp(), send_set_default_config_command(), and transmit_frame().
#define FCF_SOURCE_ADDR_OFFSET (14) |
Defines the offset of the source address.
#define FCS_LEN (2) |
Length (in octets) of FCS.
Referenced by configure_frame_sending(), configure_pkt_stream_frames(), configure_range_test_frame_sending(), crc_check_ok(), peer_req_send_rx_cb(), per_mode_initiator_rx_cb(), per_mode_initiator_tx_done_cb(), per_mode_receptor_rx_cb(), process_incoming_frame(), range_test_rx_cb(), transmit_frame(), tx_done_handling(), usr_range_test_beacon_rsp(), usr_range_test_marker_ind(), and wait_for_event_rx_cb().
#define INVALID_SHORT_ADDRESS (0xFFFF) |
Invalid short address.
#define INVERSE_CHANNEL_MASK (~VALID_CHANNEL_MASK) |
Inverse channel masks for scanning.
#define LENGTH_FIELD_LEN (1) |
Size of the length parameter.
Referenced by handle_received_frame_irq(), peer_req_send_rx_cb(), per_mode_initiator_rx_cb(), per_mode_initiator_tx_done_cb(), per_mode_receptor_rx_cb(), process_incoming_frame(), range_test_rx_cb(), send_frame(), tx_done_handling(), usr_range_test_beacon_rsp(), usr_range_test_marker_ind(), and wait_for_event_rx_cb().
#define LQI_LEN (1) |
Length of the LQI number field.
Referenced by handle_received_frame_irq(), per_mode_initiator_rx_cb(), per_mode_receptor_rx_cb(), process_incoming_frame(), and wait_for_event_rx_cb().
#define MAC_NO_SHORT_ADDR_VALUE (0xFFFE) |
MAC is using long address (by now).
#define macAckWaitDuration (0x40) |
The maximum number of symbols to wait for an acknowledgment frame to arrive following a transmitted data frame.
This value is dependent on the currently selected logical channel. For 0 <= phyCurrentChannel <= 10, this value is equal to 120. For 11 <= phyCurrentChannel <= 26, this value is equal to 54.
Referenced by tal_pib_get(), and tal_pib_set().
#define macAssociatedPANCoord (0x56) |
Indication of whether the device is associated to the PAN through the PAN coordinator.
A value of TRUE indicates the device has associated through the PAN coordinator. Otherwise, the value is set to FALSE.
#define macAssociatedPANCoord_def (false) |
Default value for PIB macAssociatedPANCoord.
#define macAssociationPermit (0x41) |
Indication of whether a coordinator is currently allowing association.
A value of true indicates that association is permitted.
#define macAssociationPermit_def (false) |
Default value for PIB macAssociationPermit.
#define macAutoRequest (0x42) |
Indication of whether a device automatically sends a data request command if its address is listed in the beacon frame.
A value of true indicates that the data request command is automatically sent.
#define macAutoRequest_def (true) |
Default value for PIB macAutoRequest.
#define macBattLifeExt (0x43) |
Indication of whether battery life extension, by reduction of coordinator receiver operation time during the CAP, is enabled.
A value of true indicates that it is enabled.
Referenced by tal_pib_get(), and tal_pib_set().
#define macBattLifeExt_def (false) |
Default value for PIB macBattLifeExt.
#define macBattLifeExtPeriods (0x44) |
The number of backoff periods during which the receiver is enabled following a beacon in battery life extension mode.
This value is dependent on the currently selected logical channel. For 0 <= * phyCurrentChannel <= 10, this value is equal to 8. For 11 <= * phyCurrentChannel <= 26, this value is equal to 6.
#define macBattLifeExtPeriods_def (6) |
Default value for PIB macBattLifeExtPeriods.
#define macBeaconOrder (0x47) |
Specification of how often the coordinator transmits a beacon.
The macBeaconOrder, BO, and the beacon interval, BI, are related as follows: for 0 <= BO <= 14, BI = aBaseSuperframeDuration * 2^BO symbols. If BO = 15, the coordinator will not transmit a beacon.
Referenced by tal_pib_get(), and tal_pib_set().
#define macBeaconOrder_def (15) |
Default value for PIB macBeaconOrder.
#define macBeaconPayload (0x45) |
The contents of the beacon payload.
#define macBeaconPayloadLength (0x46) |
The length, in octets, of the beacon payload.
#define macBeaconPayloadLength_def (0) |
Default value for PIB macBeaconPayloadLength.
#define macBeaconTxTime (0x48) |
The time that the device transmitted its last beacon frame, in symbol periods.
The measurement shall be taken at the same symbol boundary within every transmitted beacon frame, the location of which is implementation specific. The precision of this value shall be a minimum of 20 bits, with the lowest four bits being the least significant.
Referenced by tal_pib_get(), and tal_pib_set().
#define macBeaconTxTime_def (0x000000) |
Default value for PIB macBeaconTxTime.
#define macBSN (0x49) |
The sequence number added to the transmitted beacon frame.
#define macCoordExtendedAddress (0x4A) |
The 64 bit address of the coordinator with which the device is associated.
#define macCoordShortAddress (0x4B) |
The 16 bit short address assigned to the coordinator with which the device is associated.
A value of 0xfffe indicates that the coordinator is only using its 64 bit extended address. A value of 0xffff indicates that this value is unknown.
#define macCoordShortAddress_def (0xFFFF) |
Default value for PIB macCoordShortAddress.
#define macDSN (0x4C) |
The sequence number added to the transmitted data or MAC command frame.
#define macGTSPermit (0x4D) |
macGTSPermit is true if the PAN coordinator is to accept GTS requests, false otherwise.
#define macGTSPermit_def (true) |
Default value for PIB macGTSPermit.
#define macIeeeAddress (0xF0) |
Private MAC PIB attribute to allow setting the MAC address in test mode.
Referenced by configure_pibs(), tal_pib_get(), and tal_pib_set().
#define macMaxBE (0x57) |
The maximum value of the backoff exponent, BE, in the CSMA-CA algorithm.
See 7.5.1.4 for a detailed explanation of the backoff exponent.
Referenced by tal_pib_get(), and tal_pib_set().
#define macMaxCSMABackoffs (0x4E) |
The maximum number of backoffs the CSMA-CA algorithm will attempt before declaring a channel access failure.
Referenced by tal_pib_get(), and tal_pib_set().
#define macMaxCSMABackoffs_def (4) |
Default value for PIB macMaxCSMABackoffs.
#define macMaxFrameRetries (0x59) |
The maximum number of retries allowed after a transmission failure.
Referenced by tal_pib_get(), and tal_pib_set().
#define macMaxFrameTotalWaitTime (0x58) |
The maximum number of CAP symbols in a beaconenabled PAN, or symbols in a nonbeacon-enabled PAN, to wait either for a frame intended as a response to a data request frame or for a broadcast frame following a beacon with the Frame Pending subfield set to one.
This attribute, which shall only be set by the next higher layer, is dependent upon macMinBE, macMaxBE, macMaxCSMABackoffs and the number of symbols per octet. See 7.4.2 for the formula relating the attributes.
#define macMaxNumRxFramesDuringBackoff (0x7F) |
Private MAC PIB attribute to control the CSMA algorithm.
Maximum number of frames that are allowed to be received during CSMA backoff periods for a tx transaction.
#define macMinBE (0x4F) |
The minimum value of the backoff exponent in the CSMA-CA algorithm.
Note that if this value is set to 0, collision avoidance is disabled during the first iteration of the algorithm. Also note that for the slotted version of the CSMACA algorithm with the battery life extension enabled, the minimum value of the backoff exponent will be the lesser of 2 and the value of macMinBE.
Referenced by tal_pib_get(), and tal_pib_set().
#define macMinLIFSPeriod (0x5E) |
The minimum number of symbols forming a LIFS period.
#define macMinLIFSPeriod_def (40) |
Default value for PIB macMinLIFSPeriod.
Referenced by send_frame().
#define macMinSIFSPeriod (0x5F) |
The minimum number of symbols forming a SIFS period.
#define macMinSIFSPeriod_def (12) |
Default value for PIB macMinSIFSPeriod.
Referenced by send_frame().
#define macPANCoordExtendedAddress (0x7D) |
The 64-bit address of the PAN coordinator.
#define macPANCoordShortAddress (0x7E) |
The 16-bit short address assinged to the PAN coordinator.
#define macPANId (0x50) |
The 16 bit identifier of the PAN on which the device is operating.
If this value is 0xffff, the device is not associated.
Referenced by configure_pibs(), tal_pib_get(), and tal_pib_set().
#define macPANId_def (0xFFFF) |
Default value for PIB macPANId.
#define macPromiscuousMode (0x51) |
This indicates whether the MAC sublayer is in a promiscuous (receive all) mode.
A value of true indicates that the MAC sublayer accepts all frames received from the PHY.
Referenced by tal_pib_get(), and tal_pib_set().
#define macResponseWaitTime (0x5A) |
The maximum time, in multiples of aBaseSuperframeDuration, a device shall wait for a response command frame to be available following a request command frame.
#define macResponseWaitTime_def (32 * aBaseSuperframeDuration) |
Default value for PIB macResponseWaitTime.
#define macRxOnWhenIdle (0x52) |
This indicates whether the MAC sublayer is to enable its receiver during idle periods.
#define macRxOnWhenIdle_def (false) |
Default value for PIB macRxOnWhenIdle.
#define macSecurityEnabled (0x5D) |
Indication of whether the MAC sublayer has security enabled.
A value of TRUE indicates that security is enabled, while a value of FALSE indicates that security is disabled.
#define macSecurityEnabled_def (false) |
Default value for PIB macSecurityEnabled.
#define macShortAddress (0x53) |
The 16 bit address that the device uses to communicate in the PAN.
If the device is a PAN coordinator, this value shall be chosen before a PAN is started. Otherwise, the address is allocated by a coordinator during association. A value of 0xfffe indicates that the device has associated but has not been allocated an address. A value of 0xffff indicates that the device does not have a short address.
Referenced by configure_pibs(), peer_rsp_rcvd_init(), peer_search_receptor_init(), per_mode_receptor_rx_cb(), tal_pib_get(), and tal_pib_set().
#define macShortAddress_def (0xFFFF) |
Default value for PIB macShortAddress.
#define macSuperframeOrder (0x54) |
This specifies the length of the active portion of the superframe, including the beacon frame.
The macSuperframeOrder, SO, and the superframe duration, SD, are related as follows: for 0 <= SO <= BO <= 14, SD = aBaseSuperframeDuration * 2SO symbols. If SO = 15, the superframe will not be active following the beacon.
Referenced by tal_pib_get(), and tal_pib_set().
#define macSuperframeOrder_def (15) |
Default value for PIB macSuperframeOrder.
#define macSyncSymbolOffset (0x5B) |
The offset, measured in symbols, between the symbol boundary at which the MLME captures the timestamp of each transmitted or received frame, and the onset of the first symbol past the SFD, namely, the first symbol of the Length field.
#define macTimestampSupported (0x5C) |
Indication of whether the MAC sublayer supports the optional timestamping feature for incoming and outgoing data frames.
#define macTransactionPersistenceTime (0x55) |
The maximum time (in superframe periods) that a transaction is stored by a coordinator and indicated in its beacon.
#define macTransactionPersistenceTime_def (0x01F4) |
Default value for PIB macTransactionPersistenceTime.
#define MAX_KEY_ID_FIELD_LEN (9) |
Maximum length of the key id field.
#define MAX_MGMT_FRAME_LENGTH (30) |
Maximum size of the management frame(Association Response frame)
#define MIN_FRAME_LENGTH (8) |
Minimum size of a valid frame other than an Ack frame.
#define MLME_SCAN_TYPE_ACTIVE (0x01) |
Active scan (see wpan_mlme_scan_req())
#define MLME_SCAN_TYPE_ED (0x00) |
Energy scan (see wpan_mlme_scan_req())
#define MLME_SCAN_TYPE_ORPHAN (0x03) |
Orphan scan (see wpan_mlme_scan_req())
#define MLME_SCAN_TYPE_PASSIVE (0x02) |
Passive scan (see wpan_mlme_scan_req())
#define NO_PIB_INDEX (0) |
#define NON_BEACON_NWK (0x0F) |
BO value for nonbeacon-enabled network.
Referenced by tal_tx_frame().
#define NUM_LONG_PEND_ADDR | ( | x | ) | (((x) & 0x70) >> 4) |
Mask for the number of long addresses pending.
#define NUM_SHORT_PEND_ADDR | ( | x | ) | ((x) & 0x07) |
Mask for the number of short addresses pending.
#define PAN_ACCESS_DENIED (2) |
Association status code value (see wpan_mlme_associate_resp()).
#define PAN_AT_CAPACITY (1) |
Association status code value (see wpan_mlme_associate_resp()).
#define PAN_COORD_BIT_POS (14) |
PAN coordinator bit position.
#define PAN_ID_LEN (2) |
Length (in octets) of PAN ID.
Referenced by configure_frame_sending(), configure_pkt_stream_frames(), configure_range_test_frame_sending(), and transmit_frame().
#define PHY_OVERHEAD (5) |
Number of octets added by the PHY: 4 sync octets + SFD octet.
Referenced by process_incoming_frame(), send_frame(), and tx_done_handling().
#define PHY_SUCCESS_DATA_PENDING (0x10) |
PHY_SUCCESS in phyAutoCSMACA when received ACK frame had the pending bit set.
#define phyCCAMode (0x03) |
The CCA mode.
Referenced by tal_pib_get(), and tal_pib_set().
#define phyChannelsSupported (0x01) |
The 5 most significant bits (MSBs) (b27, ..., b31) of phyChannelsSupported shall be reserved and set to 0, and the 27 LSBs (b0, b1, ..., b26) shall indicate the status (1 = available, 0 = unavailable) for each of the 27 valid channels (bk shall indicate the status of channel k).
Referenced by set_channel(), and tal_pib_get().
#define phyCurrentChannel (0x00) |
The RF channel to use for all following transmissions and receptions.
Referenced by config_per_test_parameters(), configure_pibs(), per_mode_initiator_ed_end_cb(), perf_get_req(), pulse_cw_transmission(), set_channel(), set_channel_page(), set_parameter_on_transmitter_node(), set_paramter_on_recptor_node(), start_ed_scan(), tal_pib_get(), and tal_pib_set().
#define phyCurrentPage (0x04) |
This is the current PHY channel page.
This is used in conjunction with phyCurrentChannel to uniquely identify the channel currently being used.
Referenced by config_per_test_parameters(), configure_pibs(), per_mode_initiator_ed_end_cb(), perf_get_req(), set_channel_page(), set_parameter_on_transmitter_node(), set_paramter_on_recptor_node(), tal_pib_get(), tal_pib_set(), and validate_tx_power().
#define phyMaxFrameDuration (0x05) |
The maximum number of symbols in a frame: = phySHRDuration + ceiling([aMaxPHYPacketSize + 1] x phySymbolsPerOctet)
Referenced by tal_pib_get().
#define phySHRDuration (0x06) |
The duration of the synchronization header (SHR) in symbols for the current PHY.
Referenced by tal_pib_get().
#define phySymbolsPerOctet (0x07) |
The number of symbols per octet for the current PHY.
Referenced by tal_pib_get().
#define phyTransmitPower (0x02) |
The 2 MSBs represent the tolerance on the transmit power: 00 = 1 dB 01 = 3 dB 10 = 6 dB The 6 LSBs represent a signed integer in twos-complement format, corresponding to the nominal transmit power of the device in decibels relative to 1 mW.
The lowest value of phyTransmitPower shall be interpreted as less than or equal to 32 dBm.
Referenced by config_per_test_parameters(), peer_rsp_rcvd_exit(), peer_search_initiator_init(), per_mode_initiator_ed_end_cb(), per_mode_initiator_init(), per_mode_receptor_init(), perf_get_req(), recover_all_settings(), set_channel(), set_channel_page(), set_parameter_on_transmitter_node(), set_paramter_on_recptor_node(), set_tx_power(), start_ed_scan(), tal_pib_get(), and tal_pib_set().
#define PL_POS_DST_ADDR_START (6) |
Octet start position of Destination Address field within payload array of frame_info_t.
Referenced by per_mode_receptor_rx_cb(), and transmit_frame().
#define PL_POS_DST_PAN_ID_START (4) |
Octet start position of Destination PAN-Id field within payload array of frame_info_t.
#define PL_POS_FCF_1 (1) |
Octet position of FCF octet one within payload array of frame_info_t.
Referenced by process_incoming_frame(), and tx_done_handling().
#define PL_POS_FCF_2 (2) |
Octet position of FCF octet two within payload array of frame_info_t.
#define PL_POS_SEQ_NUM (3) |
Octet position of Sequence Number octet within payload array of frame_info_t.
Referenced by per_mode_initiator_task(), and per_mode_receptor_rx_cb().
#define SEQ_NUM_LEN (1) |
Length of the sequence number field.
Referenced by per_mode_initiator_rx_cb(), per_mode_initiator_tx_done_cb(), and per_mode_receptor_rx_cb().
#define SHORT_ADDR_LEN (2) |
Length (in octets) of short address.
Referenced by configure_frame_sending(), configure_pkt_stream_frames(), configure_range_test_frame_sending(), per_mode_receptor_rx_cb(), and transmit_frame().
#define WPAN_TXOPT_ACK (0x01) |
Value for TxOptions parameter in wpan_mcps_data_req().
#define WPAN_TXOPT_GTS (0x02) |
Value for TxOptions parameter in wpan_mcps_data_req().
#define WPAN_TXOPT_GTS_ACK (0x03) |
Value for TxOptions parameter in wpan_mcps_data_req().
#define WPAN_TXOPT_INDIRECT (0x04) |
Value for TxOptions parameter in wpan_mcps_data_req().
#define WPAN_TXOPT_INDIRECT_ACK (0x05) |
Value for TxOptions parameter in wpan_mcps_data_req().
#define WPAN_TXOPT_OFF (0x00) |
Value for TxOptions parameter in wpan_mcps_data_req().
typedef enum cca_mode_tag cca_mode_t |
CCA mode enumeration.
typedef enum phy_enum_tag phy_enum_t |
typedef enum trx_cca_mode_tag trx_cca_mode_t |
CCA Modes of the transceiver.
enum cca_mode_tag |
enum ch_pg_tag |
enum phy_enum_tag |
enum trx_cca_mode_tag |