AT32UC3A3 RZ600 board LEDs support package.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
#include <avr32/io.h>
#include "preprocessor.h"
#include "compiler.h"
#include "rz600.h"
#include "led.h"
Data Structures | |
struct | tLED_DESCRIPTOR |
Structure describing LED hardware connections. More... | |
Macros | |
#define | INSERT_LED_DESCRIPTOR(LED_NO, unused) |
Functions | |
void | LED_Display (U32 leds) |
Sets the state of all LEDs. More... | |
void | LED_Display_Field (U32 field, U32 leds) |
Sets as a bit-field the state of the specified LEDs. More... | |
void | LED_Display_Mask (U32 mask, U32 leds) |
Sets the state of the specified LEDs. More... | |
void | LED_Off (U32 leds) |
Turns off the specified LEDs. More... | |
void | LED_On (U32 leds) |
Turns on the specified LEDs. More... | |
U32 | LED_Read_Display (void) |
Gets the last state of all LEDs set through the LED API. More... | |
U32 | LED_Read_Display_Field (U32 field) |
Gets as a bit-field the last state of the specified LEDs set through the LED API. More... | |
U32 | LED_Read_Display_Mask (U32 mask) |
Gets the last state of the specified LEDs set through the LED API. More... | |
bool | LED_Test (U32 leds) |
Tests the last state of the specified LEDs set through the LED API. More... | |
void | LED_Toggle (U32 leds) |
Toggles the specified LEDs. More... | |
Variables | |
static tLED_DESCRIPTOR | LED_DESCRIPTOR [LED_COUNT] |
Hardware descriptors of all LEDs. More... | |
static volatile U32 | LED_State = (1 << LED_COUNT) - 1 |
Saved state of all LEDs. More... | |
#define INSERT_LED_DESCRIPTOR | ( | LED_NO, | |
unused | |||
) |
void LED_Display | ( | U32 | leds | ) |
Sets the state of all LEDs.
leds | New state of all LEDs (1 bit per LED). |
References tLED_DESCRIPTOR::GPIO, LED_COUNT, LED_State, tLED_DESCRIPTOR::PIN_MASK, and tLED_DESCRIPTOR::PORT.
Sets as a bit-field the state of the specified LEDs.
field | LEDs of which to set the state (1 bit per LED). |
leds | New state of the specified LEDs (1 bit per LED, beginning with the first specified LED). |
References ctz, and LED_Display_Mask().
Sets the state of the specified LEDs.
mask | LEDs of which to set the state (1 bit per LED). |
leds | New state of the specified LEDs (1 bit per LED). |
References ctz, tLED_DESCRIPTOR::GPIO, LED_COUNT, LED_State, tLED_DESCRIPTOR::PIN_MASK, tLED_DESCRIPTOR::PORT, and Wr_bits.
Referenced by LED_Display_Field().
void LED_Off | ( | U32 | leds | ) |
Turns off the specified LEDs.
leds | LEDs to turn off (1 bit per LED). |
References Clr_bits, ctz, tLED_DESCRIPTOR::GPIO, LED_COUNT, LED_State, tLED_DESCRIPTOR::PIN_MASK, and tLED_DESCRIPTOR::PORT.
Referenced by app_led_event(), app_switch_off_rx_led_cb(), app_switch_off_tx_led_cb(), marker_rsp_timer_handler_cb(), and marker_tx_timer_handler_cb().
void LED_On | ( | U32 | leds | ) |
Turns on the specified LEDs.
leds | LEDs to turn on (1 bit per LED). |
References ctz, tLED_DESCRIPTOR::GPIO, LED_COUNT, LED_State, tLED_DESCRIPTOR::PIN_MASK, tLED_DESCRIPTOR::PORT, and Set_bits.
Referenced by app_led_event(), marker_rsp_timer_handler_cb(), and marker_tx_timer_handler_cb().
U32 LED_Read_Display | ( | void | ) |
Gets the last state of all LEDs set through the LED API.
References LED_State.
Gets as a bit-field the last state of the specified LEDs set through the LED API.
field | LEDs of which to get the state (1 bit per LED). |
References LED_State, and Rd_bitfield.
Tests the last state of the specified LEDs set through the LED API.
leds | LEDs of which to test the state (1 bit per LED). |
true
if at least one of the specified LEDs has a state on, else false
.void LED_Toggle | ( | U32 | leds | ) |
Toggles the specified LEDs.
leds | LEDs to toggle (1 bit per LED). |
References ctz, tLED_DESCRIPTOR::GPIO, LED_COUNT, LED_State, tLED_DESCRIPTOR::PIN_MASK, tLED_DESCRIPTOR::PORT, and Tgl_bits.
Referenced by app_alert().
|
static |
Hardware descriptors of all LEDs.
Saved state of all LEDs.
Referenced by LED_Display(), LED_Display_Mask(), LED_Off(), LED_On(), LED_Read_Display(), LED_Read_Display_Field(), LED_Read_Display_Mask(), LED_Test(), and LED_Toggle().