#include "pal.h"
#include "return_val.h"
#include "tal.h"
#include "tal_internal.h"
#include "ieee_const.h"
#include "tal_helper.h"
Functions | |
uint8_t | convert_phyTransmitPower_to_reg_value (uint8_t phyTransmitPower_value) |
Converts a phyTransmitPower value to a register value. More... | |
FLASH_EXTERN (int8_t tx_pwr_table[16]) | |
Support and FAQ: visit Atmel Support More... | |
retval_t | tal_ant_div_config (bool div_ctrl, uint8_t ant_ctrl) |
retval_t | tal_convert_reg_value_to_dBm (uint8_t reg_value, int8_t *dbm_value) |
retval_t | tal_dump_registers (uint16_t start_addr, uint16_t end_addr, uint8_t *value) |
retval_t | tal_ext_pa_ctrl (bool pa_ext_sw_ctrl) |
Enable/Disable the external RF front end control. More... | |
retval_t | tal_get_curr_trx_config (param_type parameter, uint8_t *param_value) |
int8_t | tal_get_rssi_base_val (void) |
tal_trx_status_t | tal_get_trx_status (void) |
retval_t | tal_rxaack_prom_mode_ctrl (bool prom_ctrl) |
retval_t | tal_rxsafe_mode_ctrl (bool safe_mode_ctrl) |
Enable/Disable the rx safe mode. More... | |
retval_t | tal_set_rx_sensitivity_level (uint8_t pdt_level) |
to set the frequency based on CC_BAND and CC_NUMBER Registers More... | |
retval_t | tal_set_tx_pwr (bool type, int8_t pwr_value) |
Enable/Disable the external RF front end control. More... | |
retval_t | tal_trx_reg_read (uint16_t reg_addr, uint8_t *data) |
retval_t | tal_trx_reg_write (uint16_t reg_addr, uint8_t value) |
FLASH_EXTERN | ( | int8_t | tx_pwr_table[16] | ) |
Support and FAQ: visit Atmel Support
References ANT_CTRL_0, ANT_CTRL_1, ANT_CTRL_2, ANT_CTRL_3, ANT_DIV_DISABLE, ANT_DIV_ENABLE, ANT_EXT_SW_DISABLE, ANT_EXT_SW_ENABLE, FAILURE, MAC_INVALID_PARAMETER, MAC_SUCCESS, SR_ANT_CTRL, SR_ANT_DIV_EN, SR_ANT_EXT_SW_EN, SR_PDT_THRES, THRES_ANT_DIV_DISABLE, THRES_ANT_DIV_ENABLE, trx_bit_read(), and trx_bit_write().
Referenced by config_per_test_parameters(), init_state_init(), per_mode_receptor_rx_cb(), recover_all_settings(), set_transceiver_state(), and start_cw_transmission().
retval_t tal_convert_reg_value_to_dBm | ( | uint8_t | reg_value, |
int8_t * | dbm_value | ||
) |
References FAILURE, MAC_SUCCESS, and PGM_READ_BYTE.
Referenced by set_paramter_on_recptor_node(), set_tx_power(), and tal_set_tx_pwr().
retval_t tal_dump_registers | ( | uint16_t | start_addr, |
uint16_t | end_addr, | ||
uint8_t * | value | ||
) |
References MAC_INVALID_PARAMETER, MAC_SUCCESS, MAX_REG_ADDR_VALUE, and trx_reg_read().
Referenced by dump_trx_register_values().
Enable/Disable the external RF front end control.
pa_ext_sw_ctrl | true if external rf front end control has to be enabled |
References FAILURE, MAC_SUCCESS, SR_PA_EXT_EN, trx_bit_read(), and trx_bit_write().
Referenced by peer_search_initiator_init(), peer_search_receptor_init(), and per_mode_initiator_init().
retval_t tal_get_curr_trx_config | ( | param_type | parameter, |
uint8_t * | param_value | ||
) |
References CC_BAND, CC_NUMBER, MAC_INVALID_PARAMETER, MAC_SUCCESS, SR_AACK_PROM_MODE, SR_ANT_CTRL, SR_ANT_DIV_EN, SR_ANT_SEL, SR_TX_PWR, trx_bit_read(), trx_reg_read(), and TX_PWR.
Referenced by config_per_test_parameters(), perf_get_req(), save_all_settings(), send_crc_status_rsp(), set_paramter_on_recptor_node(), and set_tx_power().
int8_t tal_get_rssi_base_val | ( | void | ) |
References RSSI_BASE_VAL_DBM, and tal_pib.
Referenced by per_mode_initiator_rx_cb(), and per_mode_receptor_rx_cb().
tal_trx_status_t tal_get_trx_status | ( | void | ) |
References SR_TRX_STATUS, and trx_bit_read().
Referenced by perf_get_req(), and set_transceiver_state().
References FAILURE, MAC_SUCCESS, SR_AACK_PROM_MODE, trx_bit_read(), and trx_bit_write().
Referenced by per_mode_receptor_rx_cb().
Enable/Disable the rx safe mode.
safe_mode_ctrl | true if rx safe mode has to be enabled |
References FAILURE, MAC_SUCCESS, SR_RX_SAFE_MODE, trx_bit_read(), and trx_bit_write().
retval_t tal_set_rx_sensitivity_level | ( | uint8_t | pdt_level | ) |
to set the frequency based on CC_BAND and CC_NUMBER Registers
cc_band | band to be selected in cc_band register bits |
cc_number | offset frequency to be selected in cc_number register bits |
References FAILURE, MAC_INVALID_PARAMETER, MAC_SUCCESS, MAX_PDT_LEVEL, SR_RX_PDT_LEVEL, trx_bit_read(), and trx_bit_write().
Referenced by config_per_test_parameters(), config_rx_desensitization(), and recover_all_settings().
Enable/Disable the external RF front end control.
pa_ext_sw_ctrl | true if external rf front end control has to be enabled |
References CONV_DBM_TO_phyTransmitPower, convert_phyTransmitPower_to_reg_value(), FAILURE, MAC_INVALID_PARAMETER, MAC_SUCCESS, phyTransmitPower, SR_TX_PWR, tal_convert_reg_value_to_dBm(), tal_pib, tal_pib_set(), trx_bit_read(), and trx_bit_write().
Referenced by peer_search_initiator_init(), peer_search_receptor_init(), recover_all_settings(), set_paramter_on_recptor_node(), and set_tx_power().
retval_t tal_trx_reg_read | ( | uint16_t | reg_addr, |
uint8_t * | data | ||
) |
References MAC_INVALID_PARAMETER, MAC_SUCCESS, MAX_REG_ADDR_VALUE, and trx_reg_read().
Referenced by read_trx_registers(), and set_paramter_on_recptor_node().
retval_t tal_trx_reg_write | ( | uint16_t | reg_addr, |
uint8_t | value | ||
) |
References MAC_INVALID_PARAMETER, MAC_SUCCESS, MAX_REG_ADDR_VALUE, trx_reg_read(), and trx_reg_write().
Referenced by config_per_test_parameters(), set_paramter_on_recptor_node(), and write_trx_registers().