API function protypes - Performance Analyzer application for AT86RF215.
Copyright (c) 2015-2018 Microchip Technology Inc. and its subsidiaries.
Functions | |
Functions for User Request Primitives | |
void | perf_set_req (trx_id_t trx, uint8_t set_param_type, param_value_t *param_value) |
void | perf_set_sun_page (trx_id_t trx, uint8_t *sun_page) |
void | perf_get_req (trx_id_t trx, uint8_t param_type) |
Function to get the various configuration parameters for PER Test. More... | |
void | initiate_per_test (trx_id_t trx) |
Initiates the test procedure. More... | |
void | start_ed_scan (trx_id_t trx, uint8_t scan_duration, uint32_t channel_sel_mask) |
Function to start the ED scan. More... | |
void | get_sensor_data (trx_id_t trx) |
Function to get the Sensor data like Battery volatge. More... | |
void | get_board_details (trx_id_t trx) |
prints the hardware details More... | |
void | identify_peer_node (trx_id_t trx) |
Identifying peer node. More... | |
void | read_trx_registers (trx_id_t trx, uint16_t reg_addr) |
Read transceiver register. More... | |
void | write_trx_registers (trx_id_t trx, uint16_t reg_addr, uint8_t reg_val) |
write Transceiver registers More... | |
void | dump_trx_register_values (trx_id_t trx, uint16_t start_reg_addr, uint16_t end_reg_addr) |
Read a set of registers. More... | |
void | disconnect_peer_node (trx_id_t trx) |
Function to request the peer to get disconnected from source node. More... | |
void | set_default_configuration (trx_id_t trx) |
Function to set the default values of. More... | |
void | get_current_configuration (trx_id_t trx) |
Function to get the current values of the all configurabel patameters. More... | |
uint8_t | check_error_conditions (trx_id_t trx) |
Function used to check the error conditions before. More... | |
uint8_t | get_param_length (uint8_t parameter_type) |
UART COMMUNICATION FRAMING | |
void | usr_perf_start_confirm (trx_id_t trx, uint8_t status, uint8_t start_mode, trx_config_params_t *trx_config_params, uint8_t peer_ic_type, char *peer_soc_mcu_name, char *peer_trx_name, char *peer_board_name, uint64_t peer_mac_address, float peer_fw_version, uint32_t peer_feature_mask) |
Function to generate Perf Start confirmation frame that must be sent to host application via serial interface. More... | |
void | usr_per_test_start_confirm (trx_id_t trx, uint8_t status) |
Function to generate Per Test Start confirmation frame that must be sent to host application via serial interface. More... | |
void | usr_per_test_end_indication (trx_id_t trx, uint8_t status, int8_t rssi_val, uint8_t aver_lqi, uint32_t frames_transmitted, uint32_t frames_received, uint32_t frames_failure, uint32_t frames_no_ack, uint32_t frames_channel_access_failure, uint32_t frames_with_wrong_crc, float test_duration_sec, float test_net_data_rate) |
Function to generate Per test End Indication frame that must be sent to host application via serial interface. More... | |
void | usr_ed_scan_start_confirm (trx_id_t trx, uint8_t status, uint8_t scan_time_min, float scan_time_sec) |
Function to generate ED scan confirm test End Indication frame that must be sent to host application via serial interface. More... | |
void | usr_ed_scan_end_indication (trx_id_t trx, uint8_t no_of_channels, ed_scan_result_t *ed_scan_result) |
Function to generate ED scan Indication frame that must be sent to host application via serial interface. More... | |
void | usr_sensor_data_get_confirm (trx_id_t trx, uint8_t status, float bat_voltage, float temperature) |
Function to generate Sensor data confirm frame that must be sent to host application via serial interface. More... | |
void | usr_identify_board_confirm (trx_id_t trx, uint8_t status, uint8_t ic_type, const char *mcu_soc_name, const char *trx_name, const char *board_name, uint64_t mac_address, float fw_version, uint32_t fw_feature_mask) |
Function to generate Identify Board confirm frame that must be sent to host application via serial interface. More... | |
void | usr_perf_set_confirm (trx_id_t trx, uint8_t status, uint8_t param_type, param_value_t *param_value) |
Function to generate Perf Set confirmation frame that must be sent to host application via serial interface. More... | |
void | usr_perf_get_confirm (trx_id_t trx, uint8_t status, uint8_t parameter_type, param_value_t *parame_value) |
Function to generate Perf Get confirmation frame that must be sent to host application via serial interface. More... | |
void | usr_identify_peer_node_confirm (trx_id_t trx, uint8_t status) |
Function to generate Identify_peer_cnode_confirm that must be sent to host application via serial interface. More... | |
void | usr_cont_pulse_tx_confirm (trx_id_t trx, uint8_t status) |
Function to generate cont_pulse_tx_confirm that must be sent to host application via serial interface. More... | |
void | usr_cont_wave_tx_confirm (trx_id_t trx, uint8_t status, bool start_stop_param, uint8_t tx_mode) |
Function to generate cont_wave_tx_confirm that must be sent to host application via serial interface. More... | |
void | usr_register_read_confirm (trx_id_t trx, uint8_t status, uint16_t reg_addr, uint8_t reg_val) |
Function to generate usr_register_read_confirm that must be sent to host application via serial interface. More... | |
void | usr_register_write_confirm (trx_id_t trx, uint8_t status, uint16_t reg_addr, uint8_t reg_val) |
Function to generate usr_register_write_confirm that must be sent to host application via serial interface. More... | |
void | usr_register_dump_confirm (trx_id_t trx, uint8_t status, uint16_t start_reg_addr, uint16_t end_reg_addr, uint8_t *reg_val) |
Function to generate usr_register_dump_confirm that must be sent to host application via serial interface. More... | |
void | usr_peer_disconnect_confirm (trx_id_t trx, uint8_t status) |
Function to generate Disconnect Confirm frame that must be sent to host application via serial interface. More... | |
void | usr_set_default_config_confirm (trx_id_t trx, uint8_t status, trx_config_params_t *default_trx_config_params) |
Function to generate Set default config Confirm frame that must be sent to host application via serial interface. More... | |
void | usr_get_current_config_confirm (trx_id_t trx, uint8_t status, trx_config_params_t *curr_trx_conf_params) |
Function to generate Get Current config Confirm frame that must be sent to host application via serial interface. More... | |
void | usr_range_test_beacon_rsp (trx_id_t trx, frame_info_t *frame, uint8_t lqi_h, int8_t ed_h, uint8_t lqi_r, int8_t ed_r) |
Function to send the Received Range Test Response frame to the Host application. More... | |
void | usr_range_test_marker_ind (trx_id_t trx, frame_info_t *frame, uint8_t lqi, int8_t ed_value) |
Function to send the Marker Indication frame to the Host application. More... | |
void | usr_range_test_start_confirm (trx_id_t trx, uint8_t status) |
Function to generate Range Test Start confirmation frame that must be sent to host application via serial interface. More... | |
void | usr_range_test_stop_confirm (trx_id_t trx, uint8_t status) |
Function to generate Range Test Stop confirmation frame that must be sent to host application via serial interface. More... | |
void | usr_range_test_beacon_tx (trx_id_t trx, frame_info_t *frame) |
Function to send the transmitted frame to the Host application. More... | |
Functions for User Confirm/Indication Messages generated in response | |
to the Request Primitives | |
void | initiate_range_test (trx_id_t trx) |
Initiates the Range test procedure. More... | |
void | stop_range_test (trx_id_t trx) |
Function to Stop the range Test in PER Mode. More... | |
float | reverse_float (const float float_val) |
The reverse_float is used for reversing a float variable for supporting BIG ENDIAN systems. More... | |