PER Measurement mode prototypes and defines -Performance Analyzer application for AT86RF215.
Copyright (c) 2015-2018 Microchip Technology Inc. and its subsidiaries.
Data Structures | |
struct | ed_scan_result_t |
ED scan result structure to hold the channel and its ED value. More... | |
struct | trx_config_params_t |
Structure to hold all configurable parameter values. More... | |
Macros | |
#define | CHANNEL (0) |
#define | CHANNEL_PAGE (1) |
#define | LED_TOGGLE_COUNT_FOR_PER (50) |
#define | MAX_ED_REG_VAL (0X53) |
#define | MAX_ED_VAL 4 |
#define | MAX_TX_PWR_REG_VAL (0x1f) |
#define | MIN_ED_REG_VAL (0X00) |
#define | MIN_ED_VAL -127 |
#define | TX_POWER_DBM (2) |
Packet Error rate Measurement Generic Macros | |
#define | SET_PARAM (0x01) |
#define | RESULT_REQ (0x02) |
#define | RESULT_RSP (0x03) |
#define | IDENTIFY_NODE (0x07) |
#define | PER_TEST_PKT (0x0B) |
#define | PEER_INFO_REQ (0x0C) |
#define | PEER_INFO_RSP (0x0D) |
#define | DISCONNECT_NODE (0x0E) |
#define | SET_DEFAULT_REQ (0x0F) |
#define | PER_TEST_START_PKT (0x10) |
#define | RANGE_TEST_START_PKT (0x11) |
#define | RANGE_TEST_PKT (0x12) |
#define | RANGE_TEST_RSP (0x13) |
#define | RANGE_TEST_STOP_PKT (0x14) |
#define | RANGE_TEST_MARKER_CMD (0x15) |
#define | RANGE_TEST_MARKER_RSP (0x16) |
#define | SET_SUN_PAGE (0X17) |
#define | RANGE_TEST_PAYLOAD_LENGTH (0X08) |
#define | LED_BLINK_RATE_IN_MICRO_SEC (50000) |
Functions | |
void | app_reset (trx_id_t trx) |
void | marker_rsp_timer_handler_cb (void *parameter) |
Timer Callback function if marker command is received on air This is used to blink the LED and thus identify that the marker frame is received. More... | |
void | marker_tx_timer_handler_cb (void *parameter) |
Timer Callback function if marker response command is transmitted on air This is used to blink the LED and thus identify that the transmission is done. More... | |
void | per_mode_initiator_ed_end_cb (trx_id_t trx, uint8_t energy_level) |
User call back function after ED Scan completion. More... | |
void | per_mode_initiator_init (trx_id_t trx, void *parameter) |
Initialize the application in PER Measurement mode as Initiator. More... | |
void | per_mode_initiator_rx_cb (trx_id_t trx, frame_info_t *frame) |
Callback that is called if data has been received by trx in the PER_FOUND_PER_INITIATOR state. More... | |
void | per_mode_initiator_task (trx_id_t trx) |
Application task for PER Measurement mode as initiator. More... | |
void | per_mode_initiator_tx_done_cb (trx_id_t trx, retval_t status, frame_info_t *frame) |
Callback that is called once tx is done in the PER_FOUND_PER_INITIATOR state . More... | |
void | per_mode_receptor_init (trx_id_t trx, void *parameter) |
Initialize the application in PER Measurement mode as Receptor. More... | |
void | per_mode_receptor_rx_cb (trx_id_t trx, frame_info_t *frame) |
Callback that is called if data has been received by trx in the PER_TEST_RECEPTOR state This call back is used when the node is operating as PER Measurement mode Receptor. More... | |
void | per_mode_receptor_task (trx_id_t trx) |
The application task when the node is in PER_TEST_RECEPTOR state i.e.PER Measurement mode as Receptor. More... | |
void | per_mode_receptor_tx_done_cb (trx_id_t trx, retval_t status, frame_info_t *frame) |
Callback that is called once tx is done in PER_TEST_RECEPTOR state This call back is used when the node is operating as PER Measurement mode Receptor. More... | |
uint8_t | scale_ed_to_reg_val (int8_t ed_val) |
int8_t | scale_reg_value_to_ed (uint8_t reg_val) |
Variables | |
trx_config_params_t | curr_trx_config_params [NUM_TRX] |
#define CHANNEL (0) |
Referenced by set_channel_app(), set_parameter_on_transmitter_node(), and set_paramter_on_recptor_node().
#define CHANNEL_PAGE (1) |
Referenced by set_channel_page(), set_parameter_on_transmitter_node(), and set_paramter_on_recptor_node().
#define LED_TOGGLE_COUNT_FOR_PER (50) |
Referenced by per_mode_initiator_tx_done_cb(), and per_mode_receptor_rx_cb().
#define MAX_ED_REG_VAL (0X53) |
Referenced by scale_ed_to_reg_val(), and scale_reg_value_to_ed().
#define MAX_ED_VAL 4 |
Referenced by scale_ed_to_reg_val(), and scale_reg_value_to_ed().
#define MAX_TX_PWR_REG_VAL (0x1f) |
Referenced by set_tx_power().
#define MIN_ED_REG_VAL (0X00) |
Referenced by scale_ed_to_reg_val(), and scale_reg_value_to_ed().
#define MIN_ED_VAL -127 |
Referenced by scale_ed_to_reg_val(), and scale_reg_value_to_ed().
#define TX_POWER_DBM (2) |
Referenced by set_parameter_on_transmitter_node(), set_paramter_on_recptor_node(), and set_tx_power().