![]() ![]() | These are application-specific resources which are used in the example application of the coordinator in addition to the underlaying stack |
![]() ![]() | File contains register and command defines specific for AT86RF231 |
![]() ![]() | Copyright (c) 2014-2018 Microchip Technology Inc |
![]() ![]() | This file implements the functions for initializing buffer module, allocating and freeing up buffers |
![]() ![]() | This file contains the Buffer Management Module definitions |
![]() ![]() | Standard board header file |
![]() ![]() | Copyright (c) 2014-2018 Microchip Technology Inc |
![]() ![]() | Copyright (c) 2013-2018 Microchip Technology Inc |
![]() ![]() | Copyright (c) 2013-2018 Microchip Technology Inc |
![]() ![]() | Commonly used includes, types and macros |
![]() ![]() | Example specific board configuration file |
![]() ![]() | Example specific clock configuration file |
![]() ![]() | USART Serial configuration |
![]() ![]() | USART Serial configuration |
![]() ![]() | Sleep manager configuration |
![]() ![]() | Spi Master configuration for spi example |
![]() ![]() | |
![]() ![]() | Common TRX Access Configuration |
![]() ![]() | USB configuration file for CDC application |
![]() ![]() | |
![]() ![]() | Common Delay Service |
![]() ![]() | FLASHC driver for AVR32 UC3 |
![]() ![]() | FLASHC driver for AVR32 UC3 |
![]() ![]() | Generic clock management |
![]() ![]() | Chip-specific generic clock management |
![]() ![]() | |
![]() ![]() | |
![]() ![]() | Copyright (c) 2014-2018 Microchip Technology Inc |
![]() ![]() | Copyright (c) 2014-2018 Microchip Technology Inc |
![]() ![]() | This header holds all IEEE 802.15.4g-2012 constants and attribute identifiers |
![]() ![]() | This header holds all IEEE 802.15.4-2006 constants and attribute identifiers |
![]() ![]() | RZ600 board init |
![]() ![]() | Global interrupt management for 8- and 32-bit AVR |
![]() ![]() | Global interrupt management for 32-bit AVR |
![]() ![]() | Common IOPORT service main header file for AVR, UC3 and ARM architectures |
![]() ![]() | UC3 architecture specific IOPORT service implementation header file |
![]() ![]() | AT32UC3A3 RZ600 board LEDs support package |
![]() ![]() | AT32UC3A3 RZ600 board LEDs support package |
![]() ![]() | Provides MAC API to access MAC Layer functionality |
![]() ![]() | MAC API for IEEE 802.15.4-2006 |
![]() ![]() | This header file declares macros for various build configurations |
![]() ![]() | These are all timer IDs which are used in MAC |
![]() ![]() | This file defines all message constants |
![]() ![]() | This file defines all message structures for the MAC |
![]() ![]() | This file defines all message structures for the MAC |
![]() ![]() | |
![]() ![]() | Oscillator management |
![]() ![]() | Chip-specific oscillator management functions |
![]() ![]() | |
![]() ![]() | PAL related APIs |
![]() ![]() | PAL Generic APIs |
![]() ![]() | Atmel part identification macros |
![]() ![]() | PLL management |
![]() ![]() | Chip-specific PLL definitions |
![]() ![]() | |
![]() ![]() | |
![]() ![]() | |
![]() ![]() | |
![]() ![]() | |
![]() ![]() | |
![]() ![]() | This file implements the functions for initializing the queues, appending a buffer into the queue, removing a buffer from the queue and reading a buffer from the queue as per the search criteria |
![]() ![]() | This file contains the Queue Management Module definitions |
![]() ![]() | System-specific implementation of the _read function used by the standard library |
![]() ![]() | Return values of APIs |
![]() ![]() | AT32UC3A3 RZ600 board header file |
![]() ![]() | Sleep mode access |
![]() ![]() | AVR UC3 Sleep manager implementation |
![]() ![]() | Sleep manager |
![]() ![]() | AVR UC3 Sleep manager implementation |
![]() ![]() | |
![]() ![]() | |
![]() ![]() | |
![]() ![]() | SPI Master Mode management |
![]() ![]() | |
![]() ![]() | Stack configuration parameters |
![]() ![]() | Status code definitions |
![]() ![]() | USB CDC Standard I/O Serial Management |
![]() ![]() | USB Standard I/O Serial Management |
![]() ![]() | |
![]() ![]() | Test suite core functionality |
![]() ![]() | Test suite core declarations |
![]() ![]() | Chip-specific system clock management functions |
![]() ![]() | System clock management |
![]() ![]() | Chip-specific system clock management functions |
![]() ![]() | This file implements the TAL state machine and provides general functionality used by the TAL |
![]() ![]() | This file contains TAL API function declarations |
![]() ![]() | This file contains TAL API function declarations |
![]() ![]() | File contains TAL configuration parameters |
![]() ![]() | This file contains constants used througthout the TAL |
![]() ![]() | This file implements ED Scan |
![]() ![]() | This file contains defines for TAL types |
![]() ![]() | |
![]() ![]() | This file contains TAL helper function declarations |
![]() ![]() | This file implements functions for initializing TAL |
![]() ![]() | This header file contains types and variable definition that are used within the TAL only |
![]() ![]() | This file handles the interrupts generated by the transceiver |
![]() ![]() | This header file contains the interrupt handling definitions |
![]() ![]() | This file handles the TAL PIB attributes, set/get and initialization |
![]() ![]() | This file contains the prototypes for TAL PIB functions |
![]() ![]() | This file implements TAL power management functionality of the transceiver |
![]() ![]() | This file implements the frame reception functions |
![]() ![]() | File contains macros and modules used while processing a received frame |
![]() ![]() | File provides functionality supporting RX-Enable feature |
![]() ![]() | This file implements slotted CSMA-CA functions |
![]() ![]() | File provides CSMA-CA states |
![]() ![]() | File contains TAL timer configuration parameters |
![]() ![]() | This file handles the frame transmission within the TAL |
![]() ![]() | File contains the TAL sub-state macros and functions that perform frame transmission |
![]() ![]() | This file contains defines for TAL types |
![]() ![]() | |
![]() ![]() | |
![]() ![]() | |
![]() ![]() | |
![]() ![]() | |
![]() ![]() | HAL related APIs for externally plugged transceivers |
![]() ![]() | Missing Toolchain Definition for UC3 D header files |
![]() ![]() | Missing Toolchain Definition for UC3 L3 and UC3 L4 header files |
![]() ![]() | USB Device Controller (UDC) |
![]() ![]() | Interface of the USB Device Controller (UDC) |
![]() ![]() | Common API for USB Device Interface |
![]() ![]() | Common API for USB Device Drivers (UDD) |
![]() ![]() | Common API for USB Device Interface |
![]() ![]() | USB Device Communication Device Class (CDC) interface |
![]() ![]() | USB Device Communication Device Class (CDC) interface definitions |
![]() ![]() | Default CDC configuration for a USB Device with a single interface |
![]() ![]() | Default descriptors for a USB Device with a single interface CDC |
![]() ![]() | AT86RFx Wireless Module Unit Test |
![]() ![]() | Main functions |
![]() ![]() | All USB VIDs and PIDs from Atmel USB applications |
![]() ![]() | USB protocol definitions |
![]() ![]() | USB Communication Device Class (CDC) protocol definitions |
![]() ![]() | USB Device driver Compliance with common driver UDD |
![]() ![]() | USBB Device Driver header file |
![]() ![]() | USBB OTG Driver header file |
![]() ![]() | System-specific implementation of the _write function used by the standard library |