![]() | See Quickstart guide for SAM FLASHCALW driver |
![]() | Receiver Transmitter (USART) |
![]() | Common standard I/O driver that implements the stdio read and write functions on AVR and SAM devices |
![]() ![]() | Common standard serial I/O management driver that implements a stdio serial interface on AVR and SAM devices |
![]() | This module is responsible for encoding and decoding the serial bytes to/from Host into corresponding RF4Control APIs |
![]() | The RF4Control stack is a ZigBeeRF4CE Certified Platform implementing the ZigBee RF4CE standard |
![]() ![]() | All Build configuration Macros are defined in this module |
![]() ![]() | All nwk layer configuration Macros are defined in this module |
![]() ![]() | This module defines all Nwk layer core apis |
![]() ![]() ![]() | This module defines all Nwk layer core apis |
![]() ![]() ![]() | This module defines all generic apis used by nwk layer |
![]() ![]() ![]() | This module defines all Nwk layer constants |
![]() ![]() | This module defines all ZRC layer core apis |
![]() ![]() ![]() | This module defines all the Push button pairing APIs |
![]() ![]() ![]() | This module defines all the ZRC core APIs |
![]() ![]() ![]() | This module defines all generic apis used by nwk layer |
![]() ![]() ![]() | This module defines all the Constatnts used by zrc layer |
![]() | All General Definitions used by the Wireless Stack applications are defined in this module |
![]() ![]() | Includes IEEE Constant Definitions |
![]() ![]() | All return Value Enumerations are defined in this module |
![]() ![]() | Includes Stack Definitions |
![]() | This module is responsible for encoding and decoding the serial bytes to/from NCP into NWK or ZRC APIs to provide seamless working for application similar to stack running in same processor or on NCP |
![]() | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's Timer Counter functionality |
![]() | |
![]() ![]() | A Digital Frequency Locked Loop can be used to generate a highly accurate frequency from a slower-running reference clock, in much the same way as a PLL |
![]() ![]() | Generic clocks are configurable clocks which run outside the system clock domain |
![]() ![]() | This group contains functions and definitions related to configuring and enabling/disabling on-chip oscillators |
![]() ![]() | This group contains functions and definitions related to configuring and enabling/disabling on-chip PLLs |
![]() ![]() | See Quick Start Guide for the System Clock Management service (SAM4L) |
![]() ![]() ![]() | |
![]() | Compiler abstraction layer and code utilities for AT91SAM |
![]() ![]() | |
![]() ![]() | |
![]() ![]() | |
![]() | This is a driver for global enabling and disabling of interrupts |
![]() ![]() | |
![]() | This collection of macros identify which series and families that the various Atmel parts belong to |
![]() ![]() | |
![]() ![]() | |
![]() ![]() | |
![]() ![]() | |
![]() | Driver for the BPM (Backup Power Manager) |
![]() | This module performs serial input/output functionalities via UART |
![]() | See Quick start guide for Serial Interface service |
![]() | Transmitter (USART) |
![]() | This module performs serial input/output functionalities via UART from and to the HOST |
![]() | This module provides simple loop-based delay routines for those applications requiring a brief wait during execution |
![]() | See Quick start guide for the common IOPORT service |
![]() | Driver for the WDT (Watchdog Timer) |
![]() | The generic board support module includes board-specific definitions and function prototypes, such as the board initialization function |
![]() ![]() | |
![]() ![]() ![]() | Symbols to use for configuring the board and its initialization |
![]() ![]() ![]() | Symbols that describe features and capabilities of the board |
![]() | |
![]() | |
![]() ![]() | Implements the software Algorithm for Timer Handling in the Stack |
![]() ![]() ![]() | Implements a common api interface for accessing timer drivers of all architectures |