This is the reference manual for ZID Terminal adaptor application.
Terminal Adaptor Example Application will act as adaptor for the RF4CE ZID Class device application. Terminal adaptor stack will respond for the user input via serial interface. The user options will be printed on the serial console. Where as the user will choose the options like cold start, warm start, reset(NIB will be reset to default values and stored in EEPROM), start network and push button pairing, print the pairing table,
options are user selectable via serial console, response will be printed on the serial console after processing the requests.
Push button pairing procedure can be triggered at target side either by using "All-in-one start" option or "Reset"->"Start"->"ZID Connecting" sequence and make sure that the PBP is triggered at the ZID class device side also. The status of the push button pairing procedure will be displayed on the terminal.Then it displays ZID reports received from the ZID Class device.
Terminal adaptor can be used with the ZID device application.
This software was written for the GNU GCC and IAR . Other compilers may or may not work.
1) IEEE Std 802.15.4-2006 Part 15.4: Wireless Medium Access Control (MAC) and Physical Layer (PHY) Specifications for Low-Rate Wireless Personal Area Networks (WPANs).
2) Atmel Design Support.
For further information,visit www.microchip.com.