Microchip® Advanced Software Framework

app_config.h File Reference

These are application-specific resources which are used in the example application of the coordinator in addition to the underlaying stack.

Author
Microchip Technology Inc: http://www.microchip.com
Support: https://www.microchip.com/support/
#include "stack_config.h"
#include "tal_timer_config.h"
#include "mac_config.h"
#include "node_config.h"
#include "rf4ce.h"
#include "zid.h"
#include "common_nvm.h"
#include "conf_nvm.h"

Macros

#define APP_CAPABILITIES
 
#define APP_USER_STRING
 
#define NUM_SUPPORTED_DEV_TYPES   (1)
 
#define NUM_SUPPORTED_PROFILES   (1)
 
#define NUMBER_OF_APP_TIMERS   (1)
 
#define NUMBER_OF_LARGE_APP_BUFS   (0)
 Defines the number of additional large buffers used by the application. More...
 
#define NUMBER_OF_SMALL_APP_BUFS   (0)
 Defines the number of additional small buffers used by the application. More...
 
#define SUPPORTED_DEV_TYPE_0   DEV_TYPE_TELEVISION
 
#define SUPPORTED_DEV_TYPE_1   DEV_TYPE_TELEVISION
 
#define SUPPORTED_DEV_TYPE_2   DEV_TYPE_TELEVISION
 
#define SUPPORTED_PROFILE_ID_0   PROFILE_ID_ZID
 
#define SUPPORTED_PROFILE_ID_1   PROFILE_ID_ZID
 
#define SUPPORTED_PROFILE_ID_2   PROFILE_ID_ZID
 
#define SUPPORTED_PROFILE_ID_3   PROFILE_ID_ZID
 
#define SUPPORTED_PROFILE_ID_4   PROFILE_ID_ZID
 
#define SUPPORTED_PROFILE_ID_5   PROFILE_ID_ZID
 
#define SUPPORTED_PROFILE_ID_6   PROFILE_ID_ZID
 
#define TOTAL_NUMBER_OF_BUFS
 
#define TOTAL_NUMBER_OF_LARGE_BUFS
 Defines the total number of large buffers used by the application and the layers below. More...
 
#define TOTAL_NUMBER_OF_SMALL_BUFS
 Defines the total number of small buffers used by the application and the layers below. More...
 
#define TOTAL_NUMBER_OF_TIMERS   (NUMBER_OF_APP_TIMERS + TOTAL_STACK_TIMERS)
 
#define USER_STRING_AVAILABLE   true
 

Functions

void main_kbd_disable (void)
 
bool main_kbd_enable (void)
 
void main_mouse_disable (void)
 
bool main_mouse_enable (void)
 
void main_remotewakeup_disable (void)
 
void main_remotewakeup_enable (void)
 
void main_resume_action (void)
 
void main_sof_action (void)
 
void main_suspend_action (void)
 

#define APP_CAPABILITIES
Value:
(0x01 | \
#define NUM_SUPPORTED_DEV_TYPES
Definition: app_config.h:77
#define NUM_SUPPORTED_PROFILES
Definition: app_config.h:78

Referenced by nlme_start_confirm().

#define APP_USER_STRING
Value:
"My Target " /* 15 characters !
**/
#define NUM_SUPPORTED_DEV_TYPES   (1)
#define NUM_SUPPORTED_PROFILES   (1)
#define NUMBER_OF_APP_TIMERS   (1)
#define NUMBER_OF_LARGE_APP_BUFS   (0)

Defines the number of additional large buffers used by the application.

#define NUMBER_OF_SMALL_APP_BUFS   (0)

Defines the number of additional small buffers used by the application.

#define SUPPORTED_DEV_TYPE_0   DEV_TYPE_TELEVISION

Referenced by nlme_start_confirm().

#define SUPPORTED_DEV_TYPE_1   DEV_TYPE_TELEVISION
#define SUPPORTED_DEV_TYPE_2   DEV_TYPE_TELEVISION
#define SUPPORTED_PROFILE_ID_0   PROFILE_ID_ZID

Referenced by nlme_start_confirm().

#define SUPPORTED_PROFILE_ID_1   PROFILE_ID_ZID
#define SUPPORTED_PROFILE_ID_2   PROFILE_ID_ZID
#define SUPPORTED_PROFILE_ID_3   PROFILE_ID_ZID
#define SUPPORTED_PROFILE_ID_4   PROFILE_ID_ZID
#define SUPPORTED_PROFILE_ID_5   PROFILE_ID_ZID
#define SUPPORTED_PROFILE_ID_6   PROFILE_ID_ZID
#define TOTAL_NUMBER_OF_BUFS
Value:
#define TOTAL_NUMBER_OF_LARGE_BUFS
Defines the total number of large buffers used by the application and the layers below.
Definition: app_config.h:52
#define TOTAL_NUMBER_OF_SMALL_BUFS
Defines the total number of small buffers used by the application and the layers below.
Definition: app_config.h:59
#define TOTAL_NUMBER_OF_LARGE_BUFS
Value:
#define NUMBER_OF_LARGE_STACK_BUFS
Definition: nwk_config.h:79
#define NUMBER_OF_LARGE_APP_BUFS
Defines the number of additional large buffers used by the application.
Definition: app_config.h:43

Defines the total number of large buffers used by the application and the layers below.

Referenced by bmm_buffer_init().

#define TOTAL_NUMBER_OF_SMALL_BUFS
Value:
#define NUMBER_OF_SMALL_STACK_BUFS
Definition: nwk_config.h:81
#define NUMBER_OF_SMALL_APP_BUFS
Defines the number of additional small buffers used by the application.
Definition: app_config.h:46

Defines the total number of small buffers used by the application and the layers below.

Referenced by bmm_buffer_init().

#define TOTAL_NUMBER_OF_TIMERS   (NUMBER_OF_APP_TIMERS + TOTAL_STACK_TIMERS)
#define USER_STRING_AVAILABLE   true

void main_kbd_disable ( void  )

References main_b_kbd_enable.

bool main_kbd_enable ( void  )

References main_b_kbd_enable.

void main_mouse_disable ( void  )

References main_b_mouse_enable.

bool main_mouse_enable ( void  )

References main_b_mouse_enable.

void main_remotewakeup_disable ( void  )
void main_remotewakeup_enable ( void  )
void main_resume_action ( void  )
void main_sof_action ( void  )
void main_suspend_action ( void  )