This is the reference manual for ZID application.
ZID HID Class Device Application will act as HID Device for the RF4CE ZID Class adaptor application. ZID HID Class Device stack will respond for the user input via button press events in key remote control board. Corresponds to button press event LED will toggle on the key remote controller board once the device is paired with adaptor. Where as the user will choose the options like cold start, warm start, reset(NIB will be reset to default values and stored in EEPROM),
options are user selectable via serial console, response will be printed on the serial console after processing the requests.
Terminal adaptor can be used with the ZID device application.
This software was written for the GNU GCC and IAR . Other compilers may or may not work.
1) IEEE Std 802.15.4-2006 Part 15.4: Wireless Medium Access Control (MAC) and Physical Layer (PHY) Specifications for Low-Rate Wireless Personal Area Networks (WPANs).
2) Atmel Design Support.
For further information,visit www.microchip.com.