This file contains the QTouch Libary API interface for AVR 8-bit, AVR 32-bit and Atmel ARM QMatrix and QTouch method Capacitive Touch acquisition.
- Compiler: IAR EWAVR/EWAVR32 and GNU GCC for AVR/AVR32 IAR Workbench and GNU GCC for Atmel ARM.
- Supported devices: Atmel AVR 8-bit, AVR 32-bit, Atmel ARM.
- Userguide: QTouch Library User Guide - doc8207.pdf.
- Support: https://www.microchip.com/support/
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
|
#define | BURST_FUNC_1 BURST_JOIN(burst_qm_, PORT_NUM_1) |
|
#define | BURST_FUNC_2 BURST_JOIN(burst_qm_, PORT_NUM_2) |
|
#define | BURST_JOIN(A, B) JOIN(A, B) |
|
#define | CONCAT(A, B, C) JOIN1( A, B, C ) |
|
#define | FILL_OUT_X_LINE_INFO(port_num, x_bit) |
| QTouch libraries are supplied built with a range of charge times. More...
|
|
#define | FILL_OUT_Y_LINE_INFO(bit) { bit, (TOUCH_DATA_T)(1u << bit) } |
| Info stored for each y line. More...
|
|
#define | FILL_OUT_YA_LINE_INFO(bit) { bit, (uint8_t)(1u << bit) } |
| Info stored for each ya line. More...
|
|
#define | FILL_OUT_YB_LINE_INFO(bit) { bit, (uint8_t)(1u << bit) } |
| Info stored for each yb line. More...
|
|
#define | JOIN(x, y) x ## y |
| Error Checking For the User Configuration Options ends here. More...
|
|
#define | JOIN1(A, B, C) A ## B ## C |
|
#define | qt_init_sensing() qt_init_sensing_with_burst() |
| initialise touch sensing. More...
|
|
#define | QT_NUM_SENSOR_STATE_BYTES ((QT_NUM_CHANNELS + 7u) / 8u) |
| The number of bytes required to report the maximum possible number of sensors. More...
|
|
#define | QTLIB_BURST_AGAIN (uint16_t)0x0100 |
|
#define | QTLIB_CHANNEL_REF_CHANGE (uint16_t)0x0008 |
|
#define | QTLIB_IN_DETECT (uint16_t)0x0001 |
|
#define | QTLIB_NO_ACTIVITY (uint16_t)0x0000 |
| Status flags used with debug. More...
|
|
#define | QTLIB_RESOLVE_CAL (uint16_t)0x0200 |
|
#define | QTLIB_RESOLVE_DI (uint16_t)0x0800 |
|
#define | QTLIB_RESOLVE_FILTERIN (uint16_t)0x0400 |
|
#define | QTLIB_RESOLVE_POS_RECAL (uint16_t)0x1000 |
|
#define | QTLIB_ROTOR_SLIDER_POS_CHANGE (uint16_t)0x0004 |
|
#define | QTLIB_STATUS_CHANGE (uint16_t)0x0002 |
|
#define | REG(REGISTER, SIDE) JOIN( REGISTER, SIDE ) |
| Macro to build register writes for controlling ports. More...
|
|
#define | TOUCH_DATA_T uint8_t |
| This part of the code below is used for library selection. More...
|
|
|
enum | tag_aks_group_t {
NO_AKS_GROUP,
AKS_GROUP_1,
AKS_GROUP_2,
AKS_GROUP_3,
AKS_GROUP_4,
AKS_GROUP_5,
AKS_GROUP_6,
AKS_GROUP_7
} |
| Which AKS group, if any, a sensor is in. More...
|
|
enum | tag_burst_mask_t {
BURST_MASK_YA,
BURST_MASK_YB,
BURST_MASK_X_PORT_1,
BURST_MASK_X_PORT_2,
BURST_MASK_X_PORT_3,
NUM_BURST_MASKS
} |
|
enum | tag_channel_t {
CHANNEL_0,
CHANNEL_1,
CHANNEL_2,
CHANNEL_3,
CHANNEL_4,
CHANNEL_5,
CHANNEL_6,
CHANNEL_7,
CHANNEL_8,
CHANNEL_9,
CHANNEL_10,
CHANNEL_11,
CHANNEL_12,
CHANNEL_13,
CHANNEL_14,
CHANNEL_15,
CHANNEL_16,
CHANNEL_17,
CHANNEL_18,
CHANNEL_19,
CHANNEL_20,
CHANNEL_21,
CHANNEL_22,
CHANNEL_23,
CHANNEL_24,
CHANNEL_25,
CHANNEL_26,
CHANNEL_27,
CHANNEL_28,
CHANNEL_29,
CHANNEL_30,
CHANNEL_31
} |
|
enum | tag_hysteresis_t {
HYST_50,
HYST_25,
HYST_12_5,
HYST_6_25
} |
| A sensor detection hysteresis value. More...
|
|
enum | tag_recal_threshold_t {
RECAL_100,
RECAL_50,
RECAL_25,
RECAL_12_5,
RECAL_6_25
} |
| A sensor recalibration threshold. More...
|
|
enum | tag_resolution_t {
RES_1_BIT,
RES_2_BIT,
RES_3_BIT,
RES_4_BIT,
RES_5_BIT,
RES_6_BIT,
RES_7_BIT,
RES_8_BIT
} |
| For rotors and sliders, the resolution of the reported angle or position. More...
|
|
enum | tag_sensor_type_t {
SENSOR_TYPE_UNASSIGNED,
SENSOR_TYPE_KEY,
SENSOR_TYPE_ROTOR,
SENSOR_TYPE_SLIDER
} |
|
|
void | BURST_FUNC_1 (uint8_t channel, TOUCH_DATA_T x_mask) |
|
void | BURST_FUNC_2 (uint8_t channel, TOUCH_DATA_T x_mask) |
|
void | qt_calibrate_sensing (void) |
| calibrate touch sensing. More...
|
|
void | qt_enable_key (channel_t channel, aks_group_t aks_group, threshold_t detect_threshold, hysteresis_t detect_hysteresis) |
| enable a key sensor. More...
|
|
void | qt_enable_rotor (channel_t from_channel, channel_t to_channel, aks_group_t aks_group, threshold_t detect_threshold, hysteresis_t detect_hysteresis, resolution_t angle_resolution, uint8_t angle_hysteresis) |
| enable a rotor sensor. More...
|
|
void | qt_enable_slider (channel_t from_channel, channel_t to_channel, aks_group_t aks_group, threshold_t detect_threshold, hysteresis_t detect_hysteresis, resolution_t position_resolution, uint8_t position_hysteresis) |
| enable a slider sensor. More...
|
|
void | qt_get_library_sig (qt_lib_siginfo_t *lib_sig_ptr) |
| Get the library signature. More...
|
|
int16_t | qt_get_sensor_delta (uint8_t sensor) |
| get the current delta on the specified sensor. More...
|
|
void | qt_init_sensing_with_burst () |
|
uint16_t | qt_measure_sensors (uint16_t current_time_ms) |
| measure touch sensors. More...
|
|
void | qt_reset_sensing (void) |
| reset touch sensing. More...
|
|