Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
Rf4CE-ZID Terminal Device application AT86RF231 - XMEGA-A3BU Xplained Documentation

Preface

This is the reference manual for ZID device demo application.

Application Files

Application Introduction

ZID Class device is the RF4CE demo application which can be used in the ZID adaptor - Class device setup This will support push button pairing procedure and zid reports i.e Sending the Standard HID reports(Keyboard,Mouse,Touch sensor etc...) to the remote terminal adaptor over the air.

Application supports cold reset and warm reset. While powering on the device, if the Select key is pressed then it does cold reset. Otherwise it does warm reset i.e retrieving the network information base from NVM.

If the Select key is pressed on power on, it does the push pairing procedure following the cold reset.

The Application will use the ZID reports to send hid reports to paired device.

Application Dependent Modules

Compilation Info

This software was written for the GNU GCC and IAR . Other compilers may or may not work.

References

1) IEEE Std 802.15.4-2006 Part 15.4: Wireless Medium Access Control (MAC) and Physical Layer (PHY) Specifications for Low-Rate Wireless Personal Area Networks (WPANs).

2) Atmel Design Support.

Contact Information

For further information,visit www.microchip.com.