Microchip® Advanced Software Framework

gdp.h File Reference

API for ZID profile.

Author
Microchip Technology Inc: http://www.microchip.com
Support: https://www.microchip.com/support/
#include "rf4ce.h"
#include "nwk_internal.h"
#include "gdp_config.h"

Data Structures

struct  gdp_conf_complete_req_ind_tag
 
struct  gdp_generic_response_req_ind_tag
 
struct  gdp_get_attr_req_ind_tag
 
struct  gdp_get_attrrsp_req_ind_tag
 
struct  gdp_msg_struct_tag
 
struct  gdp_push_attr_req_ind_tag
 

Macros

#define aplcMaxResponseWaitTime   200 /* ms as per GDP*/
 The maximum time a device shall wait for a response command frame following a request command frame. More...
 
#define aplcMaxResponseWaitTime_us   (aplcMaxResponseWaitTime * 1000UL)
 
#define aplcMaxRxOnWaitTime   100 /* ms as per GDP */
 
#define aplcMaxRxOnWaitTime_us   (aplcMaxRxOnWaitTime * 1000UL)
 
#define GDP_COMMAND_FRAME_BIT   0x40
 
#define GDP_CONF_TX_OPTIONS
 
#define GDP_PENDING_DATA_BIT   0x80
 
#define PROFILE_ID   PROFILE_ID_ZID
 

Typedefs

typedef enum
gdp_attribute_status_tag 
gdp_attribute_status_t
 
typedef enum gdp_cmd_code_tag gdp_cmd_code_t
 ZID command codes. More...
 
typedef struct
gdp_conf_complete_req_ind_tag 
gdp_conf_complete_req_ind_t
 
typedef struct
gdp_generic_response_req_ind_tag 
gdp_generic_response_req_ind_t
 
typedef struct
gdp_get_attr_req_ind_tag 
gdp_get_attr_req_ind_t
 
typedef struct
gdp_get_attrrsp_req_ind_tag 
gdp_get_attrrsp_req_ind_t
 
typedef void(* gdp_heartbeat_confirm_cb_t )(nwk_enum_t Status, uint8_t PairingRef)
 
typedef struct gdp_msg_struct_tag gdp_msg_struct_t
 
typedef struct
gdp_push_attr_req_ind_tag 
gdp_push_attr_req_ind_t
 
typedef enum gdp_response_code_tag gdp_response_code_t
 Handshake response code. More...
 
typedef enum gdp_state_tag gdp_state_t
 

Enumerations

enum  gdp_attribute_status_tag {
  GDP_ATTRIBUTE_SUCCESS = 0x00,
  GDP_UNSUPPORTED_ATTRIBUTE,
  GDP_ILLEGAL_REQUEST
}
 
enum  gdp_cmd_code_tag {
  GENERIC_RESPONSE = 0x00,
  CONFIGURATION_COMPLETE,
  HEART_BEAT,
  GET_ATTRIBUTES,
  GET_ATTRIBUTES_RESPONSE,
  PUSH_ATTRIBUTES
}
 ZID command codes. More...
 
enum  gdp_response_code_tag {
  GDP_SUCCESSFUL = 0x00,
  GDP_UNSUPPORTED_REQUEST,
  GDP_INVALID_PARAMETER,
  GDP_CONFIGURATION_FAILURE,
  ZID_INVALID_REPORT_ID = 0x40,
  ZID_MISSING_FRAGMENT = 0x41
}
 Handshake response code. More...
 
enum  gdp_state_tag {
  GDP_STATE_IDLE,
  GDP_SENDING_HEARTBEAT,
  GDP_SENDING_GET_ATTRIBUTES_RESPONSE,
  GDP_SENDING_GENERIC_RESPONSE,
  GDP_WAITING_FOR_ATTRIBUTE_RESPONSE,
  GDP_WAITING_FOR_GENERIC_RESPONSE
}
 

Functions

void gdp_confirm (uint8_t PairingRef, nwk_enum_t status)
 
void gdp_indication (gdp_msg_struct_t *gdp_msg, uint8_t rxlinkquality, uint8_t rxflags)
 
void gdp_init (void)
 struct for zrc indication callback. More...
 
bool gdp_request (gdp_msg_struct_t *gdp_msg)
 

#define aplcMaxResponseWaitTime   200 /* ms as per GDP*/

The maximum time a device shall wait for a response command frame following a request command frame.

#define aplcMaxResponseWaitTime_us   (aplcMaxResponseWaitTime * 1000UL)
#define aplcMaxRxOnWaitTime   100 /* ms as per GDP */
#define aplcMaxRxOnWaitTime_us   (aplcMaxRxOnWaitTime * 1000UL)
#define GDP_COMMAND_FRAME_BIT   0x40
#define GDP_CONF_TX_OPTIONS
Value:
#define TXO_VEND_NOT_SPEC
Tx option - no vendor-specific data.
Definition: rf4ce.h:170
#define TXO_DST_ADDR_IEEE
Tx option - destination address: long.
Definition: rf4ce.h:152
#define TXO_ACK_REQ
Tx option - ACK requested.
Definition: rf4ce.h:156
#define TXO_UNICAST
Tx option - unicast.
Definition: rf4ce.h:146
#define TXO_SEC_REQ
Tx option - security requested.
Definition: rf4ce.h:160
#define TXO_MULTI_CH
Tx option - multi-channel transmission.
Definition: rf4ce.h:162
#define TXO_CH_NOT_SPEC
Tx option - channel not specified.
Definition: rf4ce.h:166
#define GDP_PENDING_DATA_BIT   0x80
#define PROFILE_ID   PROFILE_ID_ZID

ZID command codes.

typedef void(* gdp_heartbeat_confirm_cb_t)(nwk_enum_t Status, uint8_t PairingRef)

Handshake response code.

typedef enum gdp_state_tag gdp_state_t

Enumerator
GDP_ATTRIBUTE_SUCCESS 
GDP_UNSUPPORTED_ATTRIBUTE 
GDP_ILLEGAL_REQUEST 

ZID command codes.

Enumerator
GENERIC_RESPONSE 
CONFIGURATION_COMPLETE 
HEART_BEAT 
GET_ATTRIBUTES 
GET_ATTRIBUTES_RESPONSE 
PUSH_ATTRIBUTES 

Handshake response code.

Enumerator
GDP_SUCCESSFUL 
GDP_UNSUPPORTED_REQUEST 
GDP_INVALID_PARAMETER 
GDP_CONFIGURATION_FAILURE 
ZID_INVALID_REPORT_ID 
ZID_MISSING_FRAGMENT 
Enumerator
GDP_STATE_IDLE 
GDP_SENDING_HEARTBEAT 
GDP_SENDING_GET_ATTRIBUTES_RESPONSE 
GDP_SENDING_GENERIC_RESPONSE 
GDP_WAITING_FOR_ATTRIBUTE_RESPONSE 
GDP_WAITING_FOR_GENERIC_RESPONSE 

void gdp_confirm ( uint8_t  PairingRef,
nwk_enum_t  status 
)
void gdp_indication ( gdp_msg_struct_t gdp_msg,
uint8_t  rxlinkquality,
uint8_t  rxflags 
)
void gdp_init ( void  )

struct for zrc indication callback.

App should use this struct to register indication callback functions

bool gdp_request ( gdp_msg_struct_t gdp_msg)