RF4CE Serial Interface Implementation.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
#include <string.h>
#include <stdint.h>
#include <stdbool.h>
#include <stdio.h>
#include "compiler.h"
#include "app_config.h"
#include "nwk_msg_code.h"
#include "serial_api.h"
#include "sio2host.h"
#include "rf4ce.h"
#include "pb_pairing.h"
#include "zid.h"
#include "zid_adaptor.h"
#include "vendor_data.h"
Macros | |
#define | EOT (4) |
The end of transmission delimiter. More... | |
#define | SIO_BUF_COUNT (2) |
#define | SIO_RX_BUF_SIZE (250) |
#define | SIO_TX_BUF_SIZE SIO_RX_BUF_SIZE |
#define | SOT (1) |
The start of transmission delimiter. More... | |
#define | UART_RX_PROTOCOL_ID (3) |
A UART state that expects the protocol id to be received as the next character. More... | |
#define | UART_RX_STATE_DATA (4) |
A UART state that expects the next data character to be received. More... | |
#define | UART_RX_STATE_EOT (5) |
A UART state that expects a EOT to be received as the next character. More... | |
#define | UART_RX_STATE_LENGTH (2) |
A UART state that expects the length to be received as the next character. More... | |
#define | UART_RX_STATE_SOT (1) |
A UART state that expects a SOT to be received as the next character. More... | |
Functions | |
static uint8_t * | get_next_tx_buffer (void) |
static void | handle_incoming_msg (void) |
static void | nlde_data_confirm (nwk_enum_t Status, uint8_t PairingRef, profile_id_t OrgProfile, uint8_t Handle) |
void | nlde_data_indication (uint8_t PairingRef, profile_id_t ProfileId, uint16_t VendorId, uint8_t nsduLength, uint8_t *nsdu, uint8_t RxLinkQuality, uint8_t RxFlags) |
static void | nlme_get_confirm (nwk_enum_t Status, nib_attribute_t NIBAttribute, uint8_t NIBAttributeIndex, void *NIBAttributeValue) |
static void | nlme_reset_confirm (nwk_enum_t Status) |
static void | nlme_rx_enable_confirm (nwk_enum_t Status) |
static void | nlme_set_confirm (nwk_enum_t Status, nib_attribute_t NIBAttribute, uint8_t NIBAttributeIndex) |
static void | nlme_start_confirm (nwk_enum_t Status) |
static void | nlme_unpair_confirm (uint8_t Status, uint8_t PairingRef) |
static void | nlme_unpair_indication (uint8_t PairingRef) |
static void | nlme_update_key_confirm (nwk_enum_t Status, uint8_t PairingRef) |
static void | nwk_ch_agility_confirm (nwk_enum_t Status, bool ChannelChanged, uint8_t LogicalChannel) |
void | nwk_ch_agility_indication (uint8_t LogicalChannel) |
static void | pbp_rec_pair_confirm (nwk_enum_t Status, uint8_t PairingRef) |
static void | process_incoming_sio_data (void) |
void | serial_data_handler (void) |
Function to handle the state machine serial data exchange. More... | |
void | serial_interface_init (void) |
This function does the initialization of the SIO or UART. More... | |
static void | vendor_data_confirm (nwk_enum_t Status, uint8_t PairingRef, profile_id_t ProfileId, uint8_t Handle) |
static void | vendor_data_ind (uint8_t PairingRef, uint16_t VendorId, uint8_t nsduLength, uint8_t *nsdu, uint8_t RxLinkQuality, uint8_t RxFlags) |
static void | zid_connect_confirm (nwk_enum_t Status, uint8_t PairingRef) |
static void | zid_get_attribute_confirm (nwk_enum_t Status, uint8_t PairingRef, zid_attribute_t ZIDAttribute, uint8_t ZIDAttributeIndex, uint8_t AttributeSize, uint8_t *ZIDAttributeValue) |
static void | zid_get_report_confirm (nwk_enum_t Status, uint8_t PairingRef) |
static void | zid_heartbeat_indication (uint8_t PairingRef) |
void | zid_indication_callback_init (void) |
This function does the initialization of the zid indication functions. More... | |
static void | zid_report_data_confirm (nwk_enum_t Status, uint8_t PairingRef) |
static void | zid_report_data_indication (uint8_t PairingRef, uint8_t num_report_records, zid_report_data_record_t *zid_report_data_record_ptr, uint8_t RxLinkQuality, uint8_t RxFlags) |
static void | zid_set_attribute_confirm (nwk_enum_t Status, uint8_t PairingRef, zid_attribute_t ZIDAttribute, uint8_t ZIDAttributeIndex) |
static void | zid_set_report_confirm (nwk_enum_t Status, uint8_t PairingRef) |
static void | zid_standby_confirm (nwk_enum_t Status, bool StdbyEnabled) |
static void | zid_standby_leave_indication (void) |
Variables | |
static uint8_t | buf_count = 0 |
static uint8_t | data [SIO_RX_BUF_SIZE] |
This is the length of the message should be transmitted. More... | |
static uint8_t | data_length = 0 |
static uint8_t | head = 0 |
static nwk_indication_callback_t | nwk_ind |
static uint8_t | protocol_id |
static uint8_t | rx_index = 0 |
static uint8_t | sio_rx_buf [SIO_RX_BUF_SIZE] |
This is the receive buffer of the UART. More... | |
static uint8_t | sio_rx_length |
This is the length of the message should be received. More... | |
static uint8_t * | sio_rx_ptr |
This pointer points to the next free element inside the receive buffer of the UART. More... | |
static volatile uint8_t | sio_rx_state |
This is the receiver state of the UART. More... | |
static uint8_t | sio_tx_buf [SIO_BUF_COUNT][SIO_TX_BUF_SIZE] |
This is the transmit buffer of the UART. More... | |
static zid_indication_callback_t | zid_ind |
#define EOT (4) |
The end of transmission delimiter.
Referenced by nlde_data_confirm(), nlde_data_indication(), nlme_get_confirm(), nlme_reset_confirm(), nlme_rx_enable_confirm(), nlme_set_confirm(), nlme_start_confirm(), nlme_unpair_confirm(), nlme_unpair_indication(), nlme_update_key_confirm(), nwk_ch_agility_confirm(), nwk_ch_agility_indication(), pbp_rec_pair_confirm(), process_incoming_sio_data(), vendor_data_confirm(), vendor_data_ind(), zid_connect_confirm(), zid_get_attribute_confirm(), zid_get_report_confirm(), zid_heartbeat_indication(), zid_report_data_confirm(), zid_report_data_indication(), zid_set_attribute_confirm(), zid_set_report_confirm(), zid_standby_confirm(), and zid_standby_leave_indication().
#define SIO_BUF_COUNT (2) |
Referenced by get_next_tx_buffer(), and serial_data_handler().
#define SIO_RX_BUF_SIZE (250) |
Referenced by serial_data_handler().
#define SIO_TX_BUF_SIZE SIO_RX_BUF_SIZE |
#define SOT (1) |
The start of transmission delimiter.
Referenced by get_next_tx_buffer(), and process_incoming_sio_data().
#define UART_RX_PROTOCOL_ID (3) |
A UART state that expects the protocol id to be received as the next character.
Referenced by process_incoming_sio_data().
#define UART_RX_STATE_DATA (4) |
A UART state that expects the next data character to be received.
Referenced by process_incoming_sio_data().
#define UART_RX_STATE_EOT (5) |
A UART state that expects a EOT to be received as the next character.
Referenced by process_incoming_sio_data().
#define UART_RX_STATE_LENGTH (2) |
A UART state that expects the length to be received as the next character.
Referenced by process_incoming_sio_data().
#define UART_RX_STATE_SOT (1) |
A UART state that expects a SOT to be received as the next character.
Referenced by process_incoming_sio_data(), and serial_interface_init().
|
static |
References buf_count, head, SIO_BUF_COUNT, sio_tx_buf, and SOT.
Referenced by nlde_data_confirm(), nlde_data_indication(), nlme_get_confirm(), nlme_reset_confirm(), nlme_rx_enable_confirm(), nlme_set_confirm(), nlme_start_confirm(), nlme_unpair_confirm(), nlme_unpair_indication(), nlme_update_key_confirm(), nwk_ch_agility_confirm(), nwk_ch_agility_indication(), pbp_rec_pair_confirm(), vendor_data_confirm(), vendor_data_ind(), zid_connect_confirm(), zid_get_attribute_confirm(), zid_get_report_confirm(), zid_heartbeat_indication(), zid_report_data_confirm(), zid_report_data_indication(), zid_set_attribute_confirm(), zid_set_report_confirm(), zid_standby_confirm(), and zid_standby_leave_indication().
|
inlinestatic |
References Assert, mouse_desc_tag::button0, mouse_desc_tag::button1, mouse_desc_tag::button2, keyboard_output_desc_tag::caps_lock, pinch_gesture_report_tag::center_x, pinch_gesture_report_tag::center_y, keyboard_output_desc_tag::compose, sync_report_tag::contact_count, CONTACT_DATA, contact_data_report_tag::contact_index, contact_data_report_tag::contact_state, contact_data_report_tag::contact_type, DEVICE_TYPE_LIST_SIZE, scroll_gesture_report_tag::direction, pinch_gesture_report_tag::direction, rotation_gesture_report_tag::direction, scroll_gesture_report_tag::distance, pinch_gesture_report_tag::distance, tap_support_properties_tag::double_tap, tap_gesture_report_tag::finger_count, scroll_gesture_report_tag::finger_count, pinch_gesture_report_tag::finger_present, rotation_gesture_report_tag::finger_present, FUNC_PTR, sync_report_tag::gesture, touch_sensor_properties_tag::gestures, INPUT, keyboard_output_desc_tag::kana, keyboard_input_desc_tag::key_code, KEYBOARD, contact_data_report_tag::location_x, tap_gesture_report_tag::location_x, contact_data_report_tag::location_y, tap_gesture_report_tag::location_y, tap_support_properties_tag::long_tap, rotation_gesture_report_tag::magnitude, contact_data_report_tag::major_axis_length, contact_data_report_tag::major_axis_orientation, touch_sensor_properties_tag::max_coordinate_x, touch_sensor_properties_tag::max_coordinate_y, MEMCPY_ENDIAN, contact_data_report_tag::minor_axis_length, keyboard_input_desc_tag::modifier_keys, MOUSE, nlde_data_confirm(), NLDE_DATA_REQUEST, nlde_data_request(), nlme_get_confirm(), NLME_GET_REQUEST, nlme_get_request(), nlme_reset_confirm(), NLME_RESET_REQUEST, nlme_reset_request(), nlme_rx_enable_confirm(), NLME_RX_ENABLE_REQUEST, nlme_rx_enable_request(), nlme_set_confirm(), NLME_SET_REQUEST, nlme_set_request(), nlme_start_confirm(), NLME_START_REQUEST, nlme_start_request(), nlme_unpair_confirm(), NLME_UNPAIR_REQUEST, nlme_unpair_request(), NLME_UNPAIR_RESPONSE, nlme_unpair_response(), nlme_update_key_confirm(), NLME_UPDATE_KEY_REQUEST, nlme_update_key_request(), keyboard_output_desc_tag::num_lock, nwk_ch_agility_confirm(), NWK_CH_AGILITY_REQUEST, nwk_ch_agility_request(), NWK_SUCCESS, touch_sensor_properties_tag::origin, OUTPUT, pbp_rec_pair_confirm(), pbp_rec_pair_request(), PBP_REC_PAIR_REQUEST, PINCH_GESTURE, contact_data_report_tag::pressure, PROFILE_ID_LIST_SIZE, PROFILE_ID_ZID, touch_sensor_properties_tag::reliable_index, zid_report_data_record_tag::report_data, zid_report_data_record_tag::report_desc_identifier, zid_report_data_record_tag::report_type, touch_sensor_properties_tag::resolution_x, touch_sensor_properties_tag::resolution_y, ROTATE_GESTURE, SCROLL_GESTURE, keyboard_output_desc_tag::scroll_lock, touch_sensor_properties_tag::shape, tap_support_properties_tag::single_tap, sio_rx_buf, SYNC, tap_support_properties_tag::tap_and_a_half, TAP_GESTURE, TAP_SUPPORT_PROPERTIES, TOUCH_SENSOR_PROPERTIES, tap_gesture_report_tag::type, scroll_gesture_report_tag::type, vendor_data_confirm(), VENDOR_DATA_REQUEST, mouse_desc_tag::x_coordinate, mouse_desc_tag::y_coordinate, zid_connect_confirm(), zid_get_attribute_confirm(), ZID_GET_ATTRIBUTE_REQUEST, zid_get_attribute_request(), zid_get_report_confirm(), zid_get_report_data_request(), ZID_GET_REPORT_REQUEST, ZID_HEARTBEAT_REQUEST, ZID_ORG_CONNECT_REQUEST, ZID_REC_CONNECT_REQUEST, zid_rec_connect_request(), zid_report_data_confirm(), ZID_REPORT_DATA_REQUEST, zid_report_data_request(), zid_set_attribute_confirm(), ZID_SET_ATTRIBUTE_REQUEST, zid_set_attribute_request(), ZID_SET_NULL_REPORT_REQUEST, zid_set_report_confirm(), ZID_SET_REPORT_REQUEST, zid_set_report_request(), zid_standby_confirm(), ZID_STANDBY_REQUEST, and zid_standby_request().
Referenced by process_incoming_sio_data().
|
static |
References EOT, get_next_tx_buffer(), NLDE_DATA_CONF_LEN, NLDE_DATA_CONFIRM, RF4CONTROL_PID, and RF4CONTROL_PID_LEN.
Referenced by handle_incoming_msg().
void nlde_data_indication | ( | uint8_t | PairingRef, |
profile_id_t | ProfileId, | ||
uint16_t | VendorId, | ||
uint8_t | nsduLength, | ||
uint8_t * | nsdu, | ||
uint8_t | RxLinkQuality, | ||
uint8_t | RxFlags | ||
) |
References EOT, get_next_tx_buffer(), NLDE_DATA_IND_LEN, NLDE_DATA_INDICATION, RF4CONTROL_PID, and RF4CONTROL_PID_LEN.
|
static |
References EOT, get_next_tx_buffer(), NLME_GET_CONF_LEN, NLME_GET_CONFIRM, nwk_get_nib_attribute_size(), RF4CONTROL_PID, and RF4CONTROL_PID_LEN.
Referenced by handle_incoming_msg().
|
static |
References EOT, get_next_tx_buffer(), NLME_RESET_CONF_LEN, NLME_RESET_CONFIRM, RF4CONTROL_PID, and RF4CONTROL_PID_LEN.
Referenced by handle_incoming_msg().
|
static |
References EOT, get_next_tx_buffer(), NLME_RX_ENABLE_CONF_LEN, NLME_RX_ENABLE_CONFIRM, RF4CONTROL_PID, and RF4CONTROL_PID_LEN.
Referenced by handle_incoming_msg().
|
static |
References EOT, get_next_tx_buffer(), NLME_SET_CONFIRM, and RF4CONTROL_PID.
Referenced by handle_incoming_msg().
|
static |
References EOT, get_next_tx_buffer(), NLME_START_CONF_LEN, NLME_START_CONFIRM, RF4CONTROL_PID, and RF4CONTROL_PID_LEN.
Referenced by handle_incoming_msg().
|
static |
References EOT, get_next_tx_buffer(), NLME_UNPAIR_CONF_LEN, NLME_UNPAIR_CONFIRM, RF4CONTROL_PID, and RF4CONTROL_PID_LEN.
Referenced by handle_incoming_msg().
|
static |
References EOT, get_next_tx_buffer(), NLME_UNPAIR_IND_LEN, NLME_UNPAIR_INDICATION, RF4CONTROL_PID, and RF4CONTROL_PID_LEN.
Referenced by zid_indication_callback_init().
|
static |
References EOT, get_next_tx_buffer(), NLME_UPDATE_KEY_CONF_LEN, NLME_UPDATE_KEY_CONFIRM, RF4CONTROL_PID, and RF4CONTROL_PID_LEN.
Referenced by handle_incoming_msg().
|
static |
References EOT, get_next_tx_buffer(), NWK_CH_AGILITY_CONF_LEN, NWK_CH_AGILITY_CONFIRM, RF4CONTROL_PID, and RF4CONTROL_PID_LEN.
Referenced by handle_incoming_msg().
void nwk_ch_agility_indication | ( | uint8_t | LogicalChannel | ) |
References EOT, get_next_tx_buffer(), NWK_CH_AGILITY_IND_LEN, NWK_CH_AGILITY_INDICATION, RF4CONTROL_PID, and RF4CONTROL_PID_LEN.
|
static |
References EOT, get_next_tx_buffer(), PBP_REC_PAIR_CONFIRM, RF4CONTROL_PID, and RF4CONTROL_PID_LEN.
Referenced by handle_incoming_msg().
|
inlinestatic |
References data, EOT, handle_incoming_msg(), protocol_id, RF4CONTROL_PID, rx_index, sio_rx_buf, sio_rx_length, sio_rx_ptr, sio_rx_state, SOT, UART_RX_PROTOCOL_ID, UART_RX_STATE_DATA, UART_RX_STATE_EOT, UART_RX_STATE_LENGTH, and UART_RX_STATE_SOT.
Referenced by serial_data_handler().
void serial_data_handler | ( | void | ) |
Function to handle the state machine serial data exchange.
References buf_count, data, data_length, head, process_incoming_sio_data(), rx_index, sio2host_rx(), sio2host_tx(), SIO_BUF_COUNT, SIO_RX_BUF_SIZE, and sio_tx_buf.
Referenced by main().
void serial_interface_init | ( | void | ) |
This function does the initialization of the SIO or UART.
References sio2host_init(), sio_rx_state, and UART_RX_STATE_SOT.
Referenced by main().
|
static |
References EOT, get_next_tx_buffer(), RF4CONTROL_PID, RF4CONTROL_PID_LEN, and VENDOR_DATA_CONFIRM.
Referenced by handle_incoming_msg().
|
static |
References EOT, get_next_tx_buffer(), PROFILE_ID_ZID, RF4CONTROL_PID, RF4CONTROL_PID_LEN, and VENDOR_DATA_INDICATION.
Referenced by zid_indication_callback_init().
|
static |
References EOT, get_next_tx_buffer(), RF4CONTROL_PID, RF4CONTROL_PID_LEN, and ZID_CONNECT_CONFIRM.
Referenced by handle_incoming_msg().
|
static |
References EOT, get_next_tx_buffer(), RF4CONTROL_PID, RF4CONTROL_PID_LEN, and ZID_GET_ATTRIBUTE_CONFIRM.
Referenced by handle_incoming_msg().
|
static |
References EOT, get_next_tx_buffer(), RF4CONTROL_PID, RF4CONTROL_PID_LEN, and ZID_GET_REPORT_CONFIRM.
Referenced by handle_incoming_msg().
|
static |
References EOT, get_next_tx_buffer(), RF4CONTROL_PID, RF4CONTROL_PID_LEN, and ZID_HEARTBEAT_INDICATION.
Referenced by zid_indication_callback_init().
void zid_indication_callback_init | ( | void | ) |
This function does the initialization of the zid indication functions.
References nlme_unpair_indication(), nwk_indication_callback_tag::nlme_unpair_indication_cb, register_nwk_indication_callback(), register_zid_indication_callback(), vendor_data_ind(), zid_indication_callback_tag::vendor_data_ind_cb, zid_heartbeat_indication(), zid_indication_callback_tag::zid_heartbeat_indication_cb, zid_report_data_indication(), zid_indication_callback_tag::zid_report_data_indication_cb, zid_standby_leave_indication(), and zid_indication_callback_tag::zid_standby_leave_indication_cb.
Referenced by main().
|
static |
References EOT, get_next_tx_buffer(), RF4CONTROL_PID, RF4CONTROL_PID_LEN, and ZID_REPORT_DATA_CONFIRM.
Referenced by handle_incoming_msg().
|
static |
References mouse_desc_tag::button0, mouse_desc_tag::button1, mouse_desc_tag::button2, keyboard_output_desc_tag::caps_lock, pinch_gesture_report_tag::center_x, pinch_gesture_report_tag::center_y, keyboard_output_desc_tag::compose, sync_report_tag::contact_count, CONTACT_DATA, contact_data_report_tag::contact_index, contact_data_report_tag::contact_state, contact_data_report_tag::contact_type, scroll_gesture_report_tag::direction, pinch_gesture_report_tag::direction, rotation_gesture_report_tag::direction, scroll_gesture_report_tag::distance, pinch_gesture_report_tag::distance, tap_support_properties_tag::double_tap, EOT, tap_gesture_report_tag::finger_count, scroll_gesture_report_tag::finger_count, pinch_gesture_report_tag::finger_present, rotation_gesture_report_tag::finger_present, sync_report_tag::gesture, touch_sensor_properties_tag::gestures, get_next_tx_buffer(), INPUT, keyboard_output_desc_tag::kana, keyboard_input_desc_tag::key_code, KEYBOARD, contact_data_report_tag::location_x, tap_gesture_report_tag::location_x, contact_data_report_tag::location_y, tap_gesture_report_tag::location_y, tap_support_properties_tag::long_tap, rotation_gesture_report_tag::magnitude, contact_data_report_tag::major_axis_length, contact_data_report_tag::major_axis_orientation, touch_sensor_properties_tag::max_coordinate_x, touch_sensor_properties_tag::max_coordinate_y, contact_data_report_tag::minor_axis_length, keyboard_input_desc_tag::modifier_keys, MOUSE, keyboard_output_desc_tag::num_lock, touch_sensor_properties_tag::origin, PINCH_GESTURE, contact_data_report_tag::pressure, touch_sensor_properties_tag::reliable_index, zid_report_data_record_tag::report_desc_identifier, zid_report_data_record_tag::report_type, touch_sensor_properties_tag::resolution_x, touch_sensor_properties_tag::resolution_y, RF4CONTROL_PID, ROTATE_GESTURE, SCROLL_GESTURE, keyboard_output_desc_tag::scroll_lock, touch_sensor_properties_tag::shape, tap_support_properties_tag::single_tap, SYNC, tap_support_properties_tag::tap_and_a_half, TAP_GESTURE, TAP_SUPPORT_PROPERTIES, TOUCH_SENSOR_PROPERTIES, tap_gesture_report_tag::type, scroll_gesture_report_tag::type, mouse_desc_tag::x_coordinate, mouse_desc_tag::y_coordinate, and ZID_REPORT_DATA_INDICATION.
Referenced by zid_indication_callback_init().
|
static |
References EOT, get_next_tx_buffer(), RF4CONTROL_PID, RF4CONTROL_PID_LEN, and ZID_SET_ATTRIBUTE_CONFIRM.
Referenced by handle_incoming_msg().
|
static |
References EOT, get_next_tx_buffer(), RF4CONTROL_PID, RF4CONTROL_PID_LEN, and ZID_SET_REPORT_CONFIRM.
Referenced by handle_incoming_msg().
|
static |
References EOT, get_next_tx_buffer(), RF4CONTROL_PID, RF4CONTROL_PID_LEN, and ZID_STANDBY_CONFIRM.
Referenced by handle_incoming_msg().
|
static |
References EOT, get_next_tx_buffer(), RF4CONTROL_PID, RF4CONTROL_PID_LEN, and ZID_STANDBY_LEAVE_INDICATION.
Referenced by zid_indication_callback_init().
|
static |
Referenced by get_next_tx_buffer(), and serial_data_handler().
|
static |
This is the length of the message should be transmitted.
Referenced by nvm_eeprom_read_byte(), process_incoming_sio_data(), serial_data_handler(), and spi_put().
|
static |
Referenced by serial_data_handler().
|
static |
Referenced by get_next_tx_buffer(), and serial_data_handler().
|
static |
|
static |
Referenced by process_incoming_sio_data().
|
static |
Referenced by process_incoming_sio_data(), and serial_data_handler().
|
static |
This is the receive buffer of the UART.
Referenced by handle_incoming_msg(), and process_incoming_sio_data().
|
static |
This is the length of the message should be received.
Referenced by process_incoming_sio_data().
|
static |
This pointer points to the next free element inside the receive buffer of the UART.
Referenced by process_incoming_sio_data().
|
static |
This is the receiver state of the UART.
(UART_RX_STATE_SOT, UART_RX_STATE_LENGTH, UART_RX_STATE_DATA, or UART_RX_STATE_EOT)
Referenced by process_incoming_sio_data(), and serial_interface_init().
|
static |
This is the transmit buffer of the UART.
Referenced by get_next_tx_buffer(), and serial_data_handler().
|
static |