![]() | See Quickstart guide for SAM FLASHCALW driver |
![]() | See Quickstart guide for SAM SPI driver |
![]() | Receiver Transmitter (USART) |
![]() | Common standard I/O driver that implements the stdio read and write functions on AVR and SAM devices |
![]() ![]() | Common standard serial I/O management driver that implements a stdio serial interface on AVR and SAM devices |
![]() | This module is responsible for encoding and decoding the serial bytes to/from Host into corresponding RF4Control APIs |
![]() | The RF4Control stack is a ZigBeeRF4CE Certified Platform implementing the ZigBee RF4CE standard |
![]() ![]() | All Build configuration Macros are defined in this module |
![]() ![]() | All nwk layer configuration Macros are defined in this module |
![]() ![]() | This module defines all Nwk layer core apis |
![]() ![]() ![]() | This module defines all Nwk layer core apis |
![]() ![]() ![]() | This module defines all generic apis used by nwk layer |
![]() ![]() ![]() | This module defines all Nwk layer constants |
![]() ![]() | This module defines all ZRC layer core apis |
![]() ![]() ![]() | This module defines all the Push button pairing APIs |
![]() ![]() ![]() | This module defines all the ZRC core APIs |
![]() ![]() ![]() | This module defines all generic apis used by nwk layer |
![]() ![]() ![]() | This module defines all the Constatnts used by zrc layer |
![]() | All General Definitions used by the Wireless Stack applications are defined in this module |
![]() ![]() | Includes IEEE Constant Definitions |
![]() ![]() | All return Value Enumerations are defined in this module |
![]() ![]() | Includes Stack Definitions |
![]() | This module acts as a wrapper layer between the Wireless stack and the ASF drivers All hardwar level acess to the ASF drivers from the stack happens through this module |
![]() ![]() | Implements the software Algorithm for Timer Handling in the Stack |
![]() ![]() ![]() | Implements a common api interface for accessing timer drivers of all architectures |
![]() | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's Timer Counter functionality |
![]() | |
![]() ![]() | A Digital Frequency Locked Loop can be used to generate a highly accurate frequency from a slower-running reference clock, in much the same way as a PLL |
![]() ![]() | Generic clocks are configurable clocks which run outside the system clock domain |
![]() ![]() | This group contains functions and definitions related to configuring and enabling/disabling on-chip oscillators |
![]() ![]() | This group contains functions and definitions related to configuring and enabling/disabling on-chip PLLs |
![]() ![]() | See Quick Start Guide for the System Clock Management service (SAM4L) |
![]() ![]() ![]() | |
![]() | Compiler abstraction layer and code utilities for AT91SAM |
![]() ![]() | |
![]() ![]() | |
![]() ![]() | |
![]() | This is a driver for global enabling and disabling of interrupts |
![]() ![]() | |
![]() | This collection of macros identify which series and families that the various Atmel parts belong to |
![]() ![]() | |
![]() ![]() | |
![]() ![]() | |
![]() ![]() | |
![]() | Driver for the BPM (Backup Power Manager) |
![]() | This module includes api's and defenitions required for Devices with externally plugged transceivers(Non Soc's) |
![]() | This module provides simple loop-based delay routines for those applications requiring a brief wait during execution |
![]() | This is the common API for SPI interface |
![]() | See Quick start guide for the common IOPORT service |
![]() | This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the on-chip General-Purpose Input/Output (GPIO) controller with both interrupt and event support |
![]() | The Transceiver Abstraction Layer (TAL) implements the transceiver specific functionalities and provides interfaces to the upper layers (like IEEE 802.15.4 MAC )and uses the services of PAL |
![]() ![]() | The AT86RF212B is a low-power ,low voltage 700/800/900 MHz radio transceiver designed for industrial and consumer ZigBee/IEEE 802.15.4, 6LoWPAN, RF4CE and high data rate sub 1GHz ISM band applications |
![]() ![]() ![]() | The different operating states of the Transceiver are controlled by the TAL state machine |
![]() ![]() ![]() | Performs initialization and reset functionalities of the transceiver |
![]() ![]() ![]() | Performs the ED scan functionalities |
![]() ![]() ![]() | Handles Transceiver related Interrupts |
![]() ![]() ![]() | The PIB(Pan Information Base) attributes related to the TAL are Stored and handled by the TAL PIB storage |
![]() ![]() ![]() | The Frame Transmission Unit generates and transmits the frames using PAL |
![]() ![]() ![]() | The Frame Reception Unit reads/uploads the incoming frames |
![]() | The Resource Management provides access to resources to the stack or the application |
![]() ![]() | Buffer Management (large and small buffers): provides services for dynamically allocating and freeing memory buffers |
![]() ![]() | Queue Management: provides services for creating and maintaining the queues |
![]() | The IEEE standard 802.15.4 MAC Layer defines the protocol and compatible interconnection for data communication devices using low data rate, low power and low complexity, short-range radio frequency (RF) transmissions in a wireless personal area network (WPAN) |
![]() ![]() | The MAC Core Layer (MCL) abstracts and implements IEEE 802.15.4-2006 compliant behavior for non-beacon enabled and beacon-enabled network support |
![]() ![]() | Defines MAC Build Configuration Used |
![]() ![]() | This module defines all the MAC Data Structures |
![]() ![]() ![]() | The MAC Core Layer (MCL) abstracts and implements IEEE 802.15.4-2006 compliant behavior for non-beacon enabled and beacon-enabled network support |
![]() ![]() ![]() | All Definitions used by the MAC Layer is described here |
![]() ![]() ![]() ![]() | This module defines all the MAC Data Structures |
![]() ![]() | All Definitions used by the MAC Layer is described here |
![]() ![]() ![]() | This module defines all the MAC Data Structures |
![]() ![]() ![]() ![]() | The MAC Core Layer (MCL) abstracts and implements IEEE 802.15.4-2006 compliant behavior for non-beacon enabled and beacon-enabled network support |
![]() ![]() ![]() ![]() | All Definitions used by the MAC Layer is described here |
![]() ![]() | All MAC Prototypes are described in this module |
![]() ![]() ![]() | This module describes all Mac Core Layer(MCL) API's |
![]() ![]() ![]() ![]() | This module describes all MCL Request API's |
![]() ![]() ![]() ![]() | This module describes all MCL General API's |
![]() ![]() ![]() ![]() | This module describes all MCL Confirmation API's |
![]() ![]() ![]() ![]() | This module describes all MCL Indication API's |
![]() ![]() ![]() ![]() | This module describes all MCL Response API's |
![]() ![]() ![]() | This module describes all MAC Callback's |
![]() ![]() ![]() ![]() | This module describes all MAC Confirmation Callback's |
![]() ![]() ![]() ![]() | This module describes all MAC Indication Callback's |
![]() | The STB (Security Toolbox) is a high level security abstraction layer providing an easy- to-use crypto API for direct application access.It is placed on top of the SAL and abstracts and implements transceiver or MCU dependent functionality that encrypts or decrypts frames usimg CCM according to 802.15.4/Zigbee |
![]() ![]() | SAL Security abstraction layer The SAL (Security Abstraction Layer) provides an API that allows access to low level AES engine functions abstraction to encrypt and decrypt frames |
![]() | This module performs serial input/output functionalities via UART |
![]() | See Quick start guide for Serial Interface service |
![]() | Transmitter (USART) |
![]() | See Quick Start quide for common NVM driver |
![]() | Driver for the WDT (Watchdog Timer) |
![]() | The generic board support module includes board-specific definitions and function prototypes, such as the board initialization function |
![]() ![]() | |
![]() ![]() ![]() | Symbols to use for configuring the board and its initialization |
![]() ![]() ![]() | Symbols that describe features and capabilities of the board |
![]() | |
![]() | |
![]() | |
![]() ![]() | Performs channel access mechanism for frame transmission For Detailed information refer CSMA-CA algorithm section of IEEE Std 802.15.4-2006 |