Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
RF4CE - ZRC Terminal target application AT86RF233 (ATREB233-XPRO) - SAM4L Xplained Pro Documentation

Preface

This is the reference manual for ZRC Terminal target application.

Application Files

Application Introduction

Terminal Target Example Application will act as target for the RF4CE ZRC button controller application. Terminal Target stack will respond for the user input via serial interface. The user options will be printed on the serial console. Where as the user will choose the options like cold start, warm start, reset(NIB will be reset to default values and stored in EEPROM), start network and push button pairing, channel agility, vendor data support, unpair, print the pairing table, setting the base channel on the target device, toggle the standby mode on the target device.

options are user selectable via serial console, response will be printed on the serial console after processing the requests.

Push button pairing procedure can be triggered at target side either by using "All-in-one start" option or "Reset"->"Start"->"Pairing" sequence and make sure that the PBP is triggered at the controller side also. The status of the push button pairing proceure will be displayed on the terminal.Then it displays ZRC commands received from the controller.

Terminal target can be used with the single button controller node and button controller nodes.

Application Dependent Modules

Compilation Info

This software was written for the GNU GCC and IAR . Other compilers may or may not work.

References

1) IEEE Std 802.15.4-2006 Part 15.4: Wireless Medium Access Control (MAC) and Physical Layer (PHY) Specifications for Low-Rate Wireless Personal Area Networks (WPANs).

2) Atmel Design Support.

Contact Information

For further information,visit www.microchip.com.