#include "compiler.h"
#include "sysclk.h"
#include "status_codes.h"
#include "spi.h"
#include "conf_spi_master.h"
Data Structures | |
struct | spi_device |
Polled SPI device definition. More... | |
Macros | |
Spi Master Management Configuration | |
#define | CONFIG_SPI_MASTER_DELAY_BCS 0 |
Default Config Spi Master Delay BCS. More... | |
#define | CONFIG_SPI_MASTER_BITS_PER_TRANSFER 8 |
Default Config Spi Master Bits per Transfer Definition. More... | |
#define | CONFIG_SPI_MASTER_DELAY_BCT 0 |
Default Config Spi Master Delay BCT. More... | |
#define | CONFIG_SPI_MASTER_DELAY_BS 0 |
Default Config Spi Master Delay BS. More... | |
#define | CONFIG_SPI_MASTER_DUMMY 0xFF |
Default Config Spi Master Dummy Field. More... | |
Typedefs | |
typedef uint8_t | board_spi_select_id_t |
Board Spi Select Id Definition. More... | |
typedef uint8_t | spi_flags_t |
Spi Flags definition. More... | |
Functions | |
static void | spi_deselect_device (volatile avr32_spi_t *spi, struct spi_device *device) |
Deselect given device on the SPI bus. More... | |
void | spi_disable (volatile avr32_spi_t *spi) |
Disables the SPI. More... | |
void | spi_enable (volatile avr32_spi_t *spi) |
Enables the SPI. More... | |
bool | spi_is_enabled (volatile avr32_spi_t *spi) |
Tests if the SPI is enabled. More... | |
bool | spi_is_rx_full (volatile avr32_spi_t *spi) |
Check if the SPI contains a received character. More... | |
bool | spi_is_rx_ready (volatile avr32_spi_t *spi) |
Checks if all reception is ready. More... | |
bool | spi_is_tx_empty (volatile avr32_spi_t *spi) |
Checks if all transmissions are complete. More... | |
bool | spi_is_tx_ready (volatile avr32_spi_t *spi) |
Checks if all transmissions is ready. More... | |
static void | spi_master_init (volatile avr32_spi_t *spi) |
Initializes the SPI in master mode. More... | |
void | spi_master_setup_device (volatile avr32_spi_t *spi, struct spi_device *device, spi_flags_t flags, uint32_t baud_rate, board_spi_select_id_t sel_id) |
Setup a SPI device. More... | |
status_code_t | spi_read_packet (volatile avr32_spi_t *spi, uint8_t *data, size_t len) |
Receive a sequence of bytes from a SPI device. More... | |
static void | spi_read_single (volatile avr32_spi_t *spi, uint8_t *data) |
Receive one byte from a SPI device. More... | |
static void | spi_select_device (volatile avr32_spi_t *spi, struct spi_device *device) |
Select given device on the SPI bus. More... | |
status_code_t | spi_write_packet (volatile avr32_spi_t *spi, const uint8_t *data, size_t len) |
Send a sequence of bytes to a SPI device. More... | |
static void | spi_write_single (volatile avr32_spi_t *spi, uint8_t data) |
Write one byte to a SPI device. More... | |
#define CONFIG_SPI_MASTER_BITS_PER_TRANSFER 8 |
Default Config Spi Master Bits per Transfer Definition.
Referenced by spi_master_setup_device().
#define CONFIG_SPI_MASTER_DELAY_BCS 0 |
Default Config Spi Master Delay BCS.
Referenced by spi_master_init().
#define CONFIG_SPI_MASTER_DELAY_BCT 0 |
Default Config Spi Master Delay BCT.
Referenced by spi_master_setup_device().
#define CONFIG_SPI_MASTER_DELAY_BS 0 |
Default Config Spi Master Delay BS.
Referenced by spi_master_setup_device().
#define CONFIG_SPI_MASTER_DUMMY 0xFF |
Default Config Spi Master Dummy Field.
Referenced by spi_read_packet().
typedef uint8_t board_spi_select_id_t |
Board Spi Select Id Definition.
typedef uint8_t spi_flags_t |
Spi Flags definition.
|
inlinestatic |
Deselect given device on the SPI bus.
Calls board chip deselect.
spi | Base address of the SPI instance. |
device | SPI device |
References spi_device::id, and spi_unselectChip().
Referenced by trx_aes_wrrd(), trx_frame_read(), trx_frame_write(), trx_reg_read(), trx_reg_write(), trx_sram_read(), and trx_sram_write().
void spi_disable | ( | volatile avr32_spi_t * | spi | ) |
Disables the SPI.
Ensures that nothing is transferred while setting up buffers.
spi | Base address of the SPI instance. |
void spi_enable | ( | volatile avr32_spi_t * | spi | ) |
Enables the SPI.
spi | Base address of the SPI instance. |
bool spi_is_enabled | ( | volatile avr32_spi_t * | spi | ) |
Tests if the SPI is enabled.
spi | Base address of the SPI instance. |
true
if the SPI is enabled, otherwise false
. bool spi_is_rx_full | ( | volatile avr32_spi_t * | spi | ) |
Check if the SPI contains a received character.
spi | Base address of the SPI instance. |
1
if the SPI Receive Holding Register is full, otherwise 0
. bool spi_is_rx_ready | ( | volatile avr32_spi_t * | spi | ) |
Checks if all reception is ready.
spi | Base address of the SPI instance. |
1
if the SPI Receiver is ready, otherwise 0
. Referenced by spi_read_packet().
bool spi_is_tx_empty | ( | volatile avr32_spi_t * | spi | ) |
Checks if all transmissions are complete.
spi | Base address of the SPI instance. |
1 | All transmissions complete. |
0 | Transmissions not complete. |
Referenced by trx_aes_wrrd(), trx_sram_read(), and trx_sram_write().
bool spi_is_tx_ready | ( | volatile avr32_spi_t * | spi | ) |
Checks if all transmissions is ready.
spi | Base address of the SPI instance. |
1 | All transmissions complete. |
0 | Transmissions not complete. |
Referenced by spi_read_packet(), and spi_write_packet().
|
inlinestatic |
Initializes the SPI in master mode.
spi | Base address of the SPI instance. |
References CONFIG_SPI_MASTER_DELAY_BCS, spi_disable_chipselect_decoding(), spi_disable_loopback(), spi_disable_modfault(), spi_disable_variable_chipselect(), spi_reset(), spi_set_chipselect(), spi_set_delay(), spi_set_master_mode(), sysclk_enable_pba_module(), SYSCLK_SPI0, and SYSCLK_SPI1.
Referenced by trx_spi_init().
void spi_master_setup_device | ( | volatile avr32_spi_t * | spi, |
struct spi_device * | device, | ||
spi_flags_t | flags, | ||
uint32_t | baud_rate, | ||
board_spi_select_id_t | sel_id | ||
) |
Setup a SPI device.
The returned device descriptor structure must be passed to the driver whenever that device should be used as current slave device.
spi | Base address of the SPI instance. |
device | Pointer to SPI device struct that should be initialized. |
flags | SPI configuration flags. Common flags for all implementations are the SPI modes SPI_MODE_0 ... SPI_MODE_3. |
baud_rate | Baud rate for communication with slave device in Hz. |
sel_id | Board specific select id |
References CONFIG_SPI_MASTER_BITS_PER_TRANSFER, CONFIG_SPI_MASTER_DELAY_BCT, CONFIG_SPI_MASTER_DELAY_BS, getBaudDiv(), spi_device::id, spi_enable_active_mode(), spi_set_baudrate_register(), spi_set_bits_per_transfer(), spi_set_chipselect_delay_bct(), spi_set_chipselect_delay_bs(), spi_set_mode(), and sysclk_get_peripheral_bus_hz().
Referenced by trx_spi_init().
status_code_t spi_read_packet | ( | volatile avr32_spi_t * | spi, |
uint8_t * | data, | ||
size_t | len | ||
) |
Receive a sequence of bytes from a SPI device.
All bytes sent out on SPI bus are sent as value 0.
spi | Base address of the SPI instance. |
data | Data buffer to read |
len | Length of data |
References CONFIG_SPI_MASTER_DUMMY, ERR_TIMEOUT, spi_is_rx_ready(), spi_is_tx_ready(), spi_read_single(), SPI_TIMEOUT, spi_write_single(), and STATUS_OK.
Referenced by trx_aes_wrrd(), trx_frame_read(), trx_reg_read(), and trx_sram_read().
|
inlinestatic |
Receive one byte from a SPI device.
spi | Base address of the SPI instance. |
data | Data to read |
References spi_get().
Referenced by spi_read_packet(), and trx_aes_wrrd().
|
inlinestatic |
Select given device on the SPI bus.
Set device specific setting and calls board chip select.
spi | Base address of the SPI instance. |
device | SPI device |
References spi_device::id, and spi_selectChip().
Referenced by trx_aes_wrrd(), trx_frame_read(), trx_frame_write(), trx_reg_read(), trx_reg_write(), trx_sram_read(), and trx_sram_write().
status_code_t spi_write_packet | ( | volatile avr32_spi_t * | spi, |
const uint8_t * | data, | ||
size_t | len | ||
) |
Send a sequence of bytes to a SPI device.
Received bytes on the SPI bus are discarded.
spi | Base address of the SPI instance. |
data | Data buffer to write |
len | Length of data |
References ERR_TIMEOUT, spi_is_tx_ready(), SPI_TIMEOUT, spi_write_single(), and STATUS_OK.
Referenced by trx_aes_wrrd(), trx_frame_read(), trx_frame_write(), trx_reg_read(), trx_reg_write(), trx_sram_read(), and trx_sram_write().
|
inlinestatic |
Write one byte to a SPI device.
spi | Base address of the SPI instance. |
data | Data to write |
References spi_put().
Referenced by spi_read_packet(), and spi_write_packet().